RAIL_ChannelConfigEntry_t Struct Reference
A channel configuration entry structure, which defines a channel range and parameters across which a corresponding radio configuration is valid.
#include <
rail_types.h
>
Data Fields |
|
| const uint32_t * | phyConfigDeltaAdd |
|
The minimum radio configuration to apply to the base configuration for this channel set.
|
|
| uint32_t | baseFrequency |
|
A base frequency in Hz of this channel set.
|
|
| uint32_t | channelSpacing |
|
A channel spacing in Hz of this channel set.
|
|
| uint16_t | physicalChannelOffset |
|
The offset to subtract from the logical channel to align them with the zero based physical channels which are relative to baseFrequency.
|
|
| uint16_t | channelNumberStart |
|
The first valid RAIL channel number for this channel set.
|
|
| uint16_t | channelNumberEnd |
|
The last valid RAIL channel number for this channel set.
|
|
| RAIL_TxPower_t | maxPower |
|
The maximum power allowed in this channel set.
|
|
| RAIL_ChannelConfigEntryAttr_t * | attr |
|
A pointer to a structure containing attributes specific to this channel set.
|
|
| RAIL_ChannelConfigEntryType_t | entryType |
|
Indicates channel config type.
|
|
| uint8_t | reserved [3] |
|
to align to 32-bit boundary.
|
|
A channel configuration entry structure, which defines a channel range and parameters across which a corresponding radio configuration is valid.
operating frequency = baseFrequency
- channelSpacing * (channel - physicalChannelOffset);
Definition at line
1399
of file
rail_types.h
.
Field Documentation
◆ attr
| RAIL_ChannelConfigEntryAttr_t * RAIL_ChannelConfigEntry_t::attr |
A pointer to a structure containing attributes specific to this channel set.
Definition at line
1415
of file
rail_types.h
.
◆ baseFrequency
| uint32_t RAIL_ChannelConfigEntry_t::baseFrequency |
A base frequency in Hz of this channel set.
Definition at line
1402
of file
rail_types.h
.
◆ channelNumberEnd
| uint16_t RAIL_ChannelConfigEntry_t::channelNumberEnd |
The last valid RAIL channel number for this channel set.
Definition at line
1412
of file
rail_types.h
.
◆ channelNumberStart
| uint16_t RAIL_ChannelConfigEntry_t::channelNumberStart |
The first valid RAIL channel number for this channel set.
Definition at line
1410
of file
rail_types.h
.
◆ channelSpacing
| uint32_t RAIL_ChannelConfigEntry_t::channelSpacing |
A channel spacing in Hz of this channel set.
Definition at line
1403
of file
rail_types.h
.
◆ entryType
| RAIL_ChannelConfigEntryType_t RAIL_ChannelConfigEntry_t::entryType |
Indicates channel config type.
Definition at line
1418
of file
rail_types.h
.
◆ maxPower
| RAIL_TxPower_t RAIL_ChannelConfigEntry_t::maxPower |
The maximum power allowed in this channel set.
Definition at line
1414
of file
rail_types.h
.
◆ phyConfigDeltaAdd
| const uint32_t* RAIL_ChannelConfigEntry_t::phyConfigDeltaAdd |
The minimum radio configuration to apply to the base configuration for this channel set.
Definition at line
1400
of file
rail_types.h
.
◆ physicalChannelOffset
| uint16_t RAIL_ChannelConfigEntry_t::physicalChannelOffset |
The offset to subtract from the logical channel to align them with the zero based physical channels which are relative to baseFrequency.
(i.e., By default ch 0 = base freq, but if offset = 11, ch 11 = base freq.)
Definition at line
1404
of file
rail_types.h
.
◆ reserved
| uint8_t RAIL_ChannelConfigEntry_t::reserved[3] |
to align to 32-bit boundary.
Definition at line
1419
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h