RAIL_BLE_TxChannelHoppingConfigEntry_t Struct Reference
Structure that represents one of the channels that is part of a RAIL_BLE_TxChannelHoppingConfig_t sequence of channels used in channel hopping.
#include <
rail_ble.h
>
Data Fields |
|
| uint32_t | delay |
|
Idle time in microseconds to wait before hopping into the channel indicated by this entry.
|
|
| RAIL_BLE_Phy_t | phy |
|
The BLE PHY to use for this hop's transmit.
|
|
| uint8_t | logicalChannel |
|
The logical channel to use for this hop's transmit.
|
|
| uint8_t | railChannel |
|
The channel number to be used for this hop's transmit.
|
|
| bool | disableWhitening |
|
This can turn off the whitening engine and is useful for sending BLE test mode packets that don't have this turned on.
|
|
| uint32_t | crcInit |
|
The value to use for CRC initialization.
|
|
| uint32_t | accessAddress |
|
The access address to use for the connection.
|
|
Structure that represents one of the channels that is part of a RAIL_BLE_TxChannelHoppingConfig_t sequence of channels used in channel hopping.
Definition at line
685
of file
rail_ble.h
.
Field Documentation
◆ logicalChannel
| uint8_t RAIL_BLE_TxChannelHoppingConfigEntry_t::logicalChannel |
The logical channel to use for this hop's transmit.
The whitener will be reinitialized if used.
Definition at line
699
of file
rail_ble.h
.
◆ railChannel
| uint8_t RAIL_BLE_TxChannelHoppingConfigEntry_t::railChannel |
The channel number to be used for this hop's transmit.
If this is an invalid channel for the chosen PHY, the call to RAIL_SetNextTxRepeat() will fail.
Definition at line
705
of file
rail_ble.h
.
The documentation for this struct was generated from the following file:
-
protocol/ble/
rail_ble.h