RAIL_ZWAVE_LrAckData_t Struct Reference
Configuration structure for Z-Wave Long Range ACK.
#include <
rail_zwave.h
>
Data Fields | |
int8_t | noiseFloorDbm |
Radio noise level measured on the channel the frame is transmitted on. | |
int8_t | txPowerDbm |
Transmit power used to transmit the ongoing Z-Wave Long Range ACK. | |
int8_t | receiveRssiDbm |
Signal strength measured while receiving the Z-Wave Long Range frame. |
Configuration structure for Z-Wave Long Range ACK.
Definition at line 349
of file rail_zwave.h
.
The documentation for this struct was generated from the following file:
- protocol/zwave/
rail_zwave.h