RX Channel Hopping
Hardware accelerated hopping between channels while waiting for a packet in receive.
Data Structures |
|
| struct | RAIL_RxChannelHoppingConfigEntry_t |
|
Structure that represents one of the channels that is part of a sequence of channels used in channel hopping.
|
|
| struct | RAIL_RxChannelHoppingConfig_t |
|
Wrapper struct that will contain the sequence of
RAIL_RxChannelHoppingConfig_t
that represent the channel sequence to use during RX Channel Hopping.
|
|
Enumerations |
|
| enum |
RAIL_RxChannelHoppingMode_t
{
RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL , RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT , RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE , RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE } |
|
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
|
|
| enum | RAIL_RxChannelHoppingDelayMode_t { RAIL_RX_CHANNEL_HOPPING_DELAY_MODE_STATIC } |
|
Modes by which
RAIL_RxChannelHoppingConfigEntry_t::delay
timing can be applied to the time gap between channels.
|
|
Functions |
|
| RAIL_Status_t | RAIL_ConfigRxChannelHopping ( RAIL_Handle_t railHandle, RAIL_RxChannelHoppingConfig_t *config) |
|
Configure RX Channel Hopping.
|
|
| RAIL_Status_t | RAIL_EnableRxChannelHopping ( RAIL_Handle_t railHandle, bool enable, bool reset) |
|
Enable RX Channel Hopping.
|
|
Detailed Description
Hardware accelerated hopping between channels while waiting for a packet in receive.
Channel hopping provides a hardware accelerated method for scanning across multiple channels quickly, as part of a receive protocol. While it is possible to call RAIL_StartRx on different channels, back to back, and listen on many channels sequentially in that way, the time it takes to switch channels with that method may be too long for some protocols. This API pre-computes necessary channel change operations for a given list of channels, so that the radio can move from channel to channel much faster. Additionally, it leads to more succinct code as channel changes will be done implicitly, without requiring numerous calls to RAIL_StartRx . Currently, while this feature is enabled, the radio will hop channels in the given sequence each time it enters RX.
The following code gives an example of how to use the RX Channel Hopping API.
Enumeration Type Documentation
Modes by which RAIL_RxChannelHoppingConfigEntry_t::delay timing can be applied to the time gap between channels.
Definition at line
2304
of file
rail_types.h
.
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
Definition at line
2270
of file
rail_types.h
.
Function Documentation
| RAIL_Status_t RAIL_ConfigRxChannelHopping | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxChannelHoppingConfig_t * |
config
|
||
| ) |
Configure RX Channel Hopping.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] configConfiguration parameters for RX Channel Hopping.
- Returns
- Status code indicating success of the function call.
Configure Channel Hopping channels, conditions, and parameters. This API must be called before RAIL_EnableChannelHopping. This API must never be called while Channel Hopping is enabled.
- Note
- This feature/API is not supported on the EFR32XG1 family of chips.
- This feature/API is currently not supported in multiprotocol.
| RAIL_Status_t RAIL_EnableRxChannelHopping | ( | RAIL_Handle_t |
railHandle,
|
| bool |
enable,
|
||
| bool |
reset
|
||
| ) |
Enable RX Channel Hopping.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] enableEnable (true) or disable (false) RX Channel Hopping. [in] resetStart from the first channel of the channel hopping sequence (true) or from wherever hopping left off last time the code left RX.
- Returns
- Status code indicating success of the function call.
Enable or disable Channel Hopping. Additionally, specify whether hopping should be reset to start from the channel at index zero, or continue from the channel last hopped to. The radio should not be in receive when this API is called. RAIL_ConfigChannelHopping must be called before this API is called.
- Note
- This feature/API is not supported on the EFR32XG1 family of chips.
- This feature/API is currently not supported in multiprotocol.
- RX Channel Hopping may not be enabled while Auto Acking is enabled.