Configures the scheduled RX algorithm.
#include <
rail_types.h
>
Data Fields |
|
| RAIL_Time_t | start |
|
The time to start receive.
|
|
| RAIL_TimeMode_t | startMode |
|
How to interpret the time value specified in the start parameter.
|
|
| RAIL_Time_t | end |
|
The time to end receive.
|
|
| RAIL_TimeMode_t | endMode |
|
How to interpret the time value specified in the end parameter.
|
|
| uint8_t | rxTransitionEndSchedule |
|
While in scheduled RX, you can still control the radio state via state transitions.
|
|
| uint8_t | hardWindowEnd |
|
If set to 0, this will allow any packets, which are received when the window end event occurs, to complete.
|
|
Configures the scheduled RX algorithm.
Defines the start and end times of the receive window created for a scheduled receive. If either start or end times are disabled, they will be ignored.
Definition at line
1861
of file
rail_types.h
.
Field Documentation
| RAIL_Time_t RAIL_ScheduleRxConfig_t::end |
The time to end receive.
See endMode for more information about the types of end times you can specify.
Definition at line
1879
of file
rail_types.h
.
| RAIL_TimeMode_t RAIL_ScheduleRxConfig_t::endMode |
How to interpret the time value specified in the end parameter.
See the RAIL_TimeMode_t documentation for more information. Note that, in this API, if you specify a RAIL_TIME_DELAY , it is relative to the start time if given and relative to now if none is specified. Also, using RAIL_TIME_DISABLED means that this window will not end unless you explicitly call RAIL_RfIdle() or add an end event through a future update to this configuration.
Definition at line
1889
of file
rail_types.h
.
| uint8_t RAIL_ScheduleRxConfig_t::hardWindowEnd |
If set to 0, this will allow any packets, which are received when the window end event occurs, to complete.
If set to anything else, an abort of any packets received when the window end occurs is forced.
Definition at line
1904
of file
rail_types.h
.
| uint8_t RAIL_ScheduleRxConfig_t::rxTransitionEndSchedule |
While in scheduled RX, you can still control the radio state via state transitions.
This option configures whether a transition to RX goes back to scheduled RX or to the normal RX state. Once in the normal RX state, you will effectively end the scheduled RX window and can continue to receive indefinitely depending on the state transitions. Set to 1 to transition to normal RX and 0 to stay in the scheduled RX.
Definition at line
1898
of file
rail_types.h
.
| RAIL_Time_t RAIL_ScheduleRxConfig_t::start |
The time to start receive.
See startMode for more information about the types of start times that you can specify.
Definition at line
1866
of file
rail_types.h
.
| RAIL_TimeMode_t RAIL_ScheduleRxConfig_t::startMode |
How to interpret the time value specified in the start parameter.
See the RAIL_TimeMode_t documentation for more information. Use RAIL_TIME_ABSOLUTE for absolute times, RAIL_TIME_DELAY for times relative to the current time and RAIL_TIME_DISABLED to ignore the start time.
Definition at line
1874
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h