RAIL_PtiConfig_t Struct Reference
A configuration for PTI.
#include <
rail_chip_specific.h
>
Data Fields |
|
| RAIL_PtiMode_t | mode |
|
Packet Trace mode (UART or SPI)
|
|
| uint32_t | baud |
|
Output baudrate for PTI in Hz.
|
|
| uint8_t | doutLoc |
|
Data output (DOUT) location for pin/port.
|
|
| GPIO_Port_TypeDef | doutPort |
|
Data output (DOUT) GPIO port.
|
|
| uint8_t | doutPin |
|
Data output (DOUT) GPIO pin.
|
|
| uint8_t | dclkLoc |
|
Data clock (DCLK) location for pin/port.
|
|
| GPIO_Port_TypeDef | dclkPort |
|
Data clock (DCLK) GPIO port.
|
|
| uint8_t | dclkPin |
|
Data clock (DCLK) GPIO pin.
|
|
| uint8_t | dframeLoc |
|
Data frame (DFRAME) location for pin/port.
|
|
| GPIO_Port_TypeDef | dframePort |
|
Data frame (DFRAME) GPIO port.
|
|
| uint8_t | dframePin |
|
Data frame (DFRAME) GPIO pin.
|
|
A configuration for PTI.
Definition at line
545
of file
rail_chip_specific.h
.
Field Documentation
| uint8_t RAIL_PtiConfig_t::dclkLoc |
Data clock (DCLK) location for pin/port.
Only used in SPI mode
Definition at line
557
of file
rail_chip_specific.h
.
| uint8_t RAIL_PtiConfig_t::dclkPin |
Data clock (DCLK) GPIO pin.
Only used in SPI mode
Definition at line
561
of file
rail_chip_specific.h
.
| GPIO_Port_TypeDef RAIL_PtiConfig_t::dclkPort |
Data clock (DCLK) GPIO port.
Only used in SPI mode
Definition at line
559
of file
rail_chip_specific.h
.
The documentation for this struct was generated from the following file:
-
chip/efr32/efr32xg1x/
rail_chip_specific.h