Received packet details obtained via RAIL_GetRxPacketDetails() or RAIL_GetRxPacketDetailsAlt() .
      
       #include <
       
     
        rail_types.h
       
       >
      
         Data Fields | 
       |
| RAIL_PacketTimeStamp_t | timeReceived | 
| 
         The timestamp of the received packet in the RAIL timebase.
          | 
       |
| bool | crcPassed | 
| 
         Indicates whether the CRC passed or failed for the received packet.
          | 
       |
| bool | isAck | 
| 
         Indicates whether the received packet is an ACK.
          | 
       |
| int8_t | rssi | 
| 
         RSSI of the received packet in integer dBm.
          | 
       |
| uint8_t | lqi | 
| 
         The link quality indicator of the received packet.
          | 
       |
| uint8_t | syncWordId | 
| 
         For radios and PHY configurations that support multiple sync words, this number is the ID of the sync word that was used for this packet.
          | 
       |
| uint8_t | subPhyId | 
| 
         In configurations where the radio has the option of receiving a given packet in multiple ways, indicates which of the sub-PHY options was used to receive the packet.
          | 
       |
| uint8_t | antennaId | 
| 
         For configurations where the device has multiple antennas, indicates which antenna received the packets.
          | 
       |
| uint8_t | channelHoppingChannelIndex | 
| 
         When channel hopping is enabled, this field will contain the index of the channel in
         
          RAIL_RxChannelHoppingConfig_t::entries
         
         on which this packet was received.
          | 
       |
Received packet details obtained via RAIL_GetRxPacketDetails() or RAIL_GetRxPacketDetailsAlt() .
- Note
 - Certain details are always available, while others are only available if the RAIL_RxOptions_t RAIL_RX_OPTION_REMOVE_APPENDED_INFO option is not in effect and the received packet's RAIL_RxPacketStatus_t is among the RAIL_RX_PACKET_READY_ set. Each detail's description indicates its availability.
 
       Definition at line
       
        1992
       
       of file
       
        rail_types.h
       
       .
      
Field Documentation
| uint8_t RAIL_RxPacketDetails_t::antennaId | 
For configurations where the device has multiple antennas, indicates which antenna received the packets.
For hardware configurations with only one antenna, this will be set to the default of 0. It is always available.
        Definition at line
        
         2045
        
        of file
        
         rail_types.h
        
        .
       
| uint8_t RAIL_RxPacketDetails_t::channelHoppingChannelIndex | 
When channel hopping is enabled, this field will contain the index of the channel in RAIL_RxChannelHoppingConfig_t::entries on which this packet was received.
It is always available.
        Definition at line
        
         2052
        
        of file
        
         rail_types.h
        
        .
       
| bool RAIL_RxPacketDetails_t::crcPassed | 
Indicates whether the CRC passed or failed for the received packet.
It is true for RAIL_RX_PACKET_READY_SUCCESS packets and false for all others. It is always available.
        Definition at line
        
         2004
        
        of file
        
         rail_types.h
        
        .
       
| bool RAIL_RxPacketDetails_t::isAck | 
Indicates whether the received packet is an ACK.
An 'ACK' is defined as a packet received during the RX ACK window when auto ACK is enabled. Set to 0 if not an ACK, and 1 for an ACK. It is always 0 if auto ACK is not enabled. It is always available.
        Definition at line
        
         2012
        
        of file
        
         rail_types.h
        
        .
       
| uint8_t RAIL_RxPacketDetails_t::lqi | 
The link quality indicator of the received packet.
It is calculated as the average correlation for the first 8 symbols in a frame. When not available it will be 0.
        Definition at line
        
         2024
        
        of file
        
         rail_types.h
        
        .
       
| int8_t RAIL_RxPacketDetails_t::rssi | 
RSSI of the received packet in integer dBm.
It is latched when the sync word is detected for the packet. When not available it will be RAIL_RSSI_INVALID_DBM .
        Definition at line
        
         2018
        
        of file
        
         rail_types.h
        
        .
       
| uint8_t RAIL_RxPacketDetails_t::subPhyId | 
In configurations where the radio has the option of receiving a given packet in multiple ways, indicates which of the sub-PHY options was used to receive the packet.
Most radio configurations do not have this ability and the subPhy is set to 0. It is always available.
        Definition at line
        
         2038
        
        of file
        
         rail_types.h
        
        .
       
| uint8_t RAIL_RxPacketDetails_t::syncWordId | 
For radios and PHY configurations that support multiple sync words, this number is the ID of the sync word that was used for this packet.
It is always available.
        Definition at line
        
         2030
        
        of file
        
         rail_types.h
        
        .
       
| RAIL_PacketTimeStamp_t RAIL_RxPacketDetails_t::timeReceived | 
The timestamp of the received packet in the RAIL timebase.
When not available it will be RAIL_PACKET_TIME_INVALID .
        Definition at line
        
         1997
        
        of file
        
         rail_types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       common/
       
rail_types.h