A configuration structure for a scheduled transmit.
      
       #include <
       
     
        rail_types.h
       
       >
      
         Data Fields | 
       |
| RAIL_Time_t | when | 
| 
         The time when to transmit this packet.
          | 
       |
| RAIL_TimeMode_t | mode | 
| 
         The type of delay.
          | 
       |
| RAIL_ScheduledTxDuringRx_t | txDuringRx | 
| 
         Indicates which action to take with a scheduled TX if it occurs during RX.
          | 
       |
A configuration structure for a scheduled transmit.
       Definition at line
       
        1570
       
       of file
       
        rail_types.h
       
       .
      
Field Documentation
| RAIL_TimeMode_t RAIL_ScheduleTxConfig_t::mode | 
The type of delay.
See the RAIL_TimeMode_t documentation for more information. Be sure to use RAIL_TIME_ABSOLUTE delays for time-critical protocols.
        Definition at line
        
         1581
        
        of file
        
         rail_types.h
        
        .
       
| RAIL_ScheduledTxDuringRx_t RAIL_ScheduleTxConfig_t::txDuringRx | 
Indicates which action to take with a scheduled TX if it occurs during RX.
See RAIL_ScheduledTxDuringRx_t structure for more information on potential options.
        Definition at line
        
         1587
        
        of file
        
         rail_types.h
        
        .
       
| RAIL_Time_t RAIL_ScheduleTxConfig_t::when | 
The time when to transmit this packet.
The exact interpretation of this value depends on the mode specified below.
        Definition at line
        
         1575
        
        of file
        
         rail_types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       common/
       
rail_types.h