RAIL_DataConfig_t Struct Reference
RAIL data configuration structure.
#include <
rail_types.h
>
Data Fields | |
RAIL_TxDataSource_t | txSource |
Source of TX Data. | |
RAIL_RxDataSource_t | rxSource |
Source of RX Data. | |
RAIL_DataMethod_t | txMethod |
Method of providing transmit data. | |
RAIL_DataMethod_t | rxMethod |
Method of retrieving receive data. |
RAIL data configuration structure.
Selects the transmit/receive data sources and the method the application uses to provide/retrieve data from RAIL.
Definition at line 1314
of file rail_types.h
.
Field Documentation
RAIL_DataMethod_t RAIL_DataConfig_t::rxMethod |
Method of retrieving receive data.
Definition at line 1318
of file rail_types.h
.
RAIL_RxDataSource_t RAIL_DataConfig_t::rxSource |
Source of RX Data.
Definition at line 1316
of file rail_types.h
.
RAIL_DataMethod_t RAIL_DataConfig_t::txMethod |
Method of providing transmit data.
Definition at line 1317
of file rail_types.h
.
RAIL_TxDataSource_t RAIL_DataConfig_t::txSource |
Source of TX Data.
Definition at line 1315
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h