RAIL_VerifyConfig_t Struct Reference
The configuration array provided to RAIL for use by the radio state verification feature.
#include <
rail_types.h
>
Data Fields | |
RAIL_Handle_t | correspondingHandle |
Internal verification tracking information. | |
uint32_t | nextIndexToVerify |
Internal verification tracking information. | |
const uint32_t * | override |
Internal verification tracking information. | |
RAIL_VerifyCallbackPtr_t | cb |
Internal verification tracking information. |
The configuration array provided to RAIL for use by the radio state verification feature.
This structure will be populated with appropriate values by calling RAIL_ConfigVerification(). The application should not set or alter any of these structure elements.
Definition at line 2447
of file rail_types.h
.
Field Documentation
RAIL_VerifyCallbackPtr_t RAIL_VerifyConfig_t::cb |
Internal verification tracking information.
Definition at line 2455
of file rail_types.h
.
RAIL_Handle_t RAIL_VerifyConfig_t::correspondingHandle |
Internal verification tracking information.
Definition at line 2449
of file rail_types.h
.
uint32_t RAIL_VerifyConfig_t::nextIndexToVerify |
Internal verification tracking information.
Definition at line 2451
of file rail_types.h
.
const uint32_t* RAIL_VerifyConfig_t::override |
Internal verification tracking information.
Definition at line 2453
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h