Transmit
APIs related to transmitting data packets.
Modules |
|
| Power Amplifier (PA) | |
|
APIs for interacting with one of the on chip PAs.
|
|
Data Structures |
|
| struct | RAIL_TxPacketDetails_t |
|
Detailed information requested and about the packet that was just transmitted.
|
|
| struct | RAIL_ScheduleTxConfig_t |
|
A configuration structure for a scheduled transmit.
|
|
| struct | RAIL_CsmaConfig_t |
|
A configuration structure for the CSMA transmit algorithm.
|
|
| struct | RAIL_LbtConfig_t |
|
A configuration structure for the LBT transmit algorithm.
|
|
Macros |
|
| #define | RAIL_STOP_MODES_NONE (0U) |
|
Do not stop any radio operations.
|
|
| #define | RAIL_STOP_MODE_ACTIVE (1U << RAIL_STOP_MODE_ACTIVE_SHIFT) |
|
Stop active radio operations only.
|
|
| #define | RAIL_STOP_MODE_PENDING (1U << RAIL_STOP_MODE_PENDING_SHIFT) |
|
Stop pending radio operations.
|
|
| #define | RAIL_STOP_MODES_ALL (0xFFU) |
|
Stop all radio operations.
|
|
| #define | RAIL_TX_OPTIONS_NONE 0UL |
|
A value representing no options enabled.
|
|
| #define | RAIL_TX_OPTIONS_DEFAULT RAIL_TX_OPTIONS_NONE |
|
All options disabled by default .
|
|
| #define | RAIL_TX_OPTION_WAIT_FOR_ACK (1UL << RAIL_TX_OPTION_WAIT_FOR_ACK_SHIFT) |
|
An option to configure whether or not the TXing node will listen for an ACK.
|
|
| #define | RAIL_TX_OPTION_REMOVE_CRC (1UL << RAIL_TX_OPTION_REMOVE_CRC_SHIFT) |
|
An option to remove CRC bytes from TX packets.
|
|
| #define | RAIL_TX_OPTION_SYNC_WORD_ID (1UL << RAIL_TX_OPTION_SYNC_WORD_ID_SHIFT) |
|
An option to select which sync word to send (0 or 1).
|
|
| #define | RAIL_TX_OPTION_ANTENNA0 (1UL << RAIL_TX_OPTION_ANTENNA0_SHIFT) |
|
An option to select the antenna 0 for transmission.
|
|
| #define | RAIL_TX_OPTION_ANTENNA1 (1UL << RAIL_TX_OPTION_ANTENNA1_SHIFT) |
|
An option to select the antenna 1 for transmission.
|
|
| #define | RAIL_TX_OPTION_ALT_PREAMBLE_LEN (1UL << RAIL_TX_OPTION_ALT_PREAMBLE_LEN_SHIFT) |
|
An option to dynamically set an alternate preamble length for the transmission.
|
|
| #define | RAIL_TX_OPTION_CCA_PEAK_RSSI (1UL << RAIL_TX_OPTION_CCA_PEAK_RSSI_SHIFT) |
|
An option to use peak rather than average RSSI energy detected during CSMA's
RAIL_CsmaConfig_t::ccaDuration
or LBT's
RAIL_LbtConfig_t::lbtDuration
to determine whether the channel is clear or busy.
|
|
| #define | RAIL_TX_OPTIONS_ALL 0xFFFFFFFFUL |
|
A value representing all possible options.
|
|
| #define | RAIL_MAX_LBT_TRIES 15 |
|
The maximum number of LBT/CSMA retries supported.
|
|
| #define | RAIL_CSMA_CONFIG_802_15_4_2003_2p4_GHz_OQPSK_CSMA |
|
RAIL_CsmaConfig_t
initializer configuring CSMA per IEEE 802.15.4-2003 on 2.4 GHz OSPSK, commonly used by ZigBee.
|
|
| #define | RAIL_CSMA_CONFIG_SINGLE_CCA |
|
RAIL_CsmaConfig_t
initializer configuring a single CCA prior to TX.
|
|
| #define | RAIL_LBT_CONFIG_ETSI_EN_300_220_1_V2_4_1 |
|
RAIL_LbtConfig_t
initializer configuring LBT per ETSI 300 220-1 V2.4.1 for a typical Sub-GHz band.
|
|
Enumerations |
|
| enum |
RAIL_StopMode_t
{
RAIL_STOP_MODE_ACTIVE_SHIFT = 0, RAIL_STOP_MODE_PENDING_SHIFT = 1 } |
|
Stop radio operation options bit mask.
|
|
| enum |
RAIL_TxOptions_t
{
RAIL_TX_OPTION_WAIT_FOR_ACK_SHIFT = 0, RAIL_TX_OPTION_REMOVE_CRC_SHIFT , RAIL_TX_OPTION_SYNC_WORD_ID_SHIFT , RAIL_TX_OPTION_ANTENNA0_SHIFT , RAIL_TX_OPTION_ANTENNA1_SHIFT , RAIL_TX_OPTION_ALT_PREAMBLE_LEN_SHIFT , RAIL_TX_OPTION_CCA_PEAK_RSSI_SHIFT } |
|
Transmit options, in reality a bitmask.
|
|
| enum |
RAIL_ScheduledTxDuringRx_t
{
RAIL_SCHEDULED_TX_DURING_RX_POSTPONE_TX , RAIL_SCHEDULED_TX_DURING_RX_ABORT_TX } |
|
Enumerates the possible outcomes of what will occur if a scheduled TX ends up firing during RX.
|
|
Functions |
|
| RAIL_Status_t | RAIL_SetTxPowerDbm ( RAIL_Handle_t railHandle, RAIL_TxPower_t power) |
|
Sets the TX power in terms of deci-dBm instead of raw power level.
|
|
| RAIL_TxPower_t | RAIL_GetTxPowerDbm ( RAIL_Handle_t railHandle) |
|
Gets the TX power in terms of deci-dBm instead of raw power level.
|
|
| RAIL_Status_t | RAIL_StartTx ( RAIL_Handle_t railHandle, uint16_t channel, RAIL_TxOptions_t options, const RAIL_SchedulerInfo_t *schedulerInfo) |
|
Starts a non-blocking transmit.
|
|
| RAIL_Status_t | RAIL_StopTx ( RAIL_Handle_t railHandle, RAIL_StopMode_t mode) |
|
Stops an active or pending transmit.
|
|
| RAIL_Status_t | RAIL_StartScheduledTx ( RAIL_Handle_t railHandle, uint16_t channel, RAIL_TxOptions_t options, const RAIL_ScheduleTxConfig_t *config, const RAIL_SchedulerInfo_t *schedulerInfo) |
|
Schedules sending a packet.
|
|
| RAIL_Status_t | RAIL_StartCcaCsmaTx ( RAIL_Handle_t railHandle, uint16_t channel, RAIL_TxOptions_t options, const RAIL_CsmaConfig_t *csmaConfig, const RAIL_SchedulerInfo_t *schedulerInfo) |
|
Starts a non-blocking Transmit using CSMA.
|
|
| RAIL_Status_t | RAIL_StartCcaLbtTx ( RAIL_Handle_t railHandle, uint16_t channel, RAIL_TxOptions_t options, const RAIL_LbtConfig_t *lbtConfig, const RAIL_SchedulerInfo_t *schedulerInfo) |
|
Starts a non-blocking Transmit using LBT.
|
|
| RAIL_Status_t | RAIL_SetCcaThreshold ( RAIL_Handle_t railHandle, int8_t ccaThresholdDbm) |
|
Sets the CCA threshold in dBm.
|
|
| RAIL_Status_t | RAIL_GetTxPacketDetails ( RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t *pPacketDetails) |
|
Gets detailed information about the last packet transmitted.
|
|
| RAIL_Status_t | RAIL_GetTxPacketDetailsAlt ( RAIL_Handle_t railHandle, bool isAck, RAIL_Time_t *pPacketTime) |
|
Gets detailed information about the last packet transmitted.
|
|
| RAIL_Status_t | RAIL_GetTxTimePreambleStart ( RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) |
|
Adjust a RAIL TX timestamp to refer to the start of the preamble.
|
|
| RAIL_Status_t | RAIL_GetTxTimeSyncWordEnd ( RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) |
|
Adjust a RAIL TX timestamp to refer to the end of the sync word.
|
|
| RAIL_Status_t | RAIL_GetTxTimeFrameEnd ( RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) |
|
Adjust a RAIL TX timestamp to refer to the end of frame.
|
|
| void | RAIL_EnableTxHoldOff ( RAIL_Handle_t railHandle, bool enable) |
|
Prevent the radio from starting a transmit.
|
|
| bool | RAIL_IsTxHoldOffEnabled ( RAIL_Handle_t railHandle) |
|
Check whether or not TX hold off is enabled.
|
|
| RAIL_Status_t | RAIL_SetTxAltPreambleLength ( RAIL_Handle_t railHandle, uint16_t length) |
|
Sets an alternate transmitter preamble length.
|
|
Detailed Description
APIs related to transmitting data packets.
Macro Definition Documentation
| #define RAIL_CSMA_CONFIG_802_15_4_2003_2p4_GHz_OQPSK_CSMA |
RAIL_CsmaConfig_t initializer configuring CSMA per IEEE 802.15.4-2003 on 2.4 GHz OSPSK, commonly used by ZigBee.
Definition at line
1645
of file
rail_types.h
.
| #define RAIL_CSMA_CONFIG_SINGLE_CCA |
RAIL_CsmaConfig_t initializer configuring a single CCA prior to TX.
It can be used to as a basis for implementing other channel access schemes with custom backoff delays. Users can override ccaBackoff with a fixed delay on each use.
Definition at line
1663
of file
rail_types.h
.
| #define RAIL_LBT_CONFIG_ETSI_EN_300_220_1_V2_4_1 |
rail_types.h:1594
RAIL_LbtConfig_t initializer configuring LBT per ETSI 300 220-1 V2.4.1 for a typical Sub-GHz band.
To be practical, users should override lbtTries and/or lbtTimeout so channel access failure will be reported in a reasonable time frame rather than the unbounded time frame ETSI defined.
Definition at line
1727
of file
rail_types.h
.
| #define RAIL_TX_OPTION_ALT_PREAMBLE_LEN (1UL << RAIL_TX_OPTION_ALT_PREAMBLE_LEN_SHIFT) |
An option to dynamically set an alternate preamble length for the transmission.
If this option is not set, the pre-configured channel preamble length will be used.
Definition at line
1513
of file
rail_types.h
.
| #define RAIL_TX_OPTION_ANTENNA0 (1UL << RAIL_TX_OPTION_ANTENNA0_SHIFT) |
An option to select the antenna 0 for transmission.
If the antenna selection option is not set or if both antenna options are set, then the TX will take place in either antenna depending on the last RX or TX configuration. This option is only valid on platforms that support antenna selection.
Definition at line
1499
of file
rail_types.h
.
| #define RAIL_TX_OPTION_ANTENNA1 (1UL << RAIL_TX_OPTION_ANTENNA1_SHIFT) |
An option to select the antenna 1 for transmission.
If the antenna selection option is not set or if both antenna options are set, then the TX will take place in either antenna depending on the last RX or TX configuration. This option is only valid on platforms that support antenna selection.
Definition at line
1507
of file
rail_types.h
.
| #define RAIL_TX_OPTION_CCA_PEAK_RSSI (1UL << RAIL_TX_OPTION_CCA_PEAK_RSSI_SHIFT) |
An option to use peak rather than average RSSI energy detected during CSMA's RAIL_CsmaConfig_t::ccaDuration or LBT's RAIL_LbtConfig_t::lbtDuration to determine whether the channel is clear or busy.
- Note
- This option does nothing on platforms like EFR32XG1 that lack support for capturing peak RSSI energy.
Definition at line
1522
of file
rail_types.h
.
| #define RAIL_TX_OPTION_REMOVE_CRC (1UL << RAIL_TX_OPTION_REMOVE_CRC_SHIFT) |
An option to remove CRC bytes from TX packets.
To receive packets when the sender has this option set true, set RAIL_RX_OPTION_IGNORE_CRC_ERRORS on the receive side.
Definition at line
1485
of file
rail_types.h
.
| #define RAIL_TX_OPTION_SYNC_WORD_ID (1UL << RAIL_TX_OPTION_SYNC_WORD_ID_SHIFT) |
An option to select which sync word to send (0 or 1).
Note that this does not set the actual sync words, it just picks which of the two will be sent with the packet.
Definition at line
1491
of file
rail_types.h
.
| #define RAIL_TX_OPTION_WAIT_FOR_ACK (1UL << RAIL_TX_OPTION_WAIT_FOR_ACK_SHIFT) |
An option to configure whether or not the TXing node will listen for an ACK.
If this is false, the isAck flag in RAIL_RxPacketDetails_t of a received packet will always be false.
Definition at line
1479
of file
rail_types.h
.
| #define RAIL_TX_OPTIONS_ALL 0xFFFFFFFFUL |
A value representing all possible options.
Definition at line
1525
of file
rail_types.h
.
| #define RAIL_TX_OPTIONS_DEFAULT RAIL_TX_OPTIONS_NONE |
All options disabled by default .
Definition at line
1473
of file
rail_types.h
.
| #define RAIL_TX_OPTIONS_NONE 0UL |
A value representing no options enabled.
Definition at line
1471
of file
rail_types.h
.
Enumeration Type Documentation
Enumerates the possible outcomes of what will occur if a scheduled TX ends up firing during RX.
Because RX and TX can't happen at the same time, it is up to the user how the TX should be handled. This enumeration is passed into RAIL_StartScheduledTx() as part of RAIL_ScheduleTxConfig_t .
Definition at line
1555
of file
rail_types.h
.
| enum RAIL_StopMode_t |
Stop radio operation options bit mask.
| Enumerator | |
|---|---|
| RAIL_STOP_MODE_ACTIVE_SHIFT |
Shift position of RAIL_STOP_MODE_ACTIVE bit. |
| RAIL_STOP_MODE_PENDING_SHIFT |
Shift position of RAIL_STOP_MODE_PENDING bit. |
Definition at line
1433
of file
rail_types.h
.
| enum RAIL_TxOptions_t |
Transmit options, in reality a bitmask.
| Enumerator | |
|---|---|
| RAIL_TX_OPTION_WAIT_FOR_ACK_SHIFT |
Shift position of RAIL_TX_OPTION_WAIT_FOR_ACK bit. |
| RAIL_TX_OPTION_REMOVE_CRC_SHIFT |
Shift position of RAIL_TX_OPTION_REMOVE_CRC bit. |
| RAIL_TX_OPTION_SYNC_WORD_ID_SHIFT |
Shift position of RAIL_TX_OPTION_SYNC_WORD_ID bit. |
| RAIL_TX_OPTION_ANTENNA0_SHIFT |
Shift position of RAIL_TX_OPTION_ANTENNA0 bit. |
| RAIL_TX_OPTION_ANTENNA1_SHIFT |
Shift position of RAIL_TX_OPTION_ANTENNA1 bit. |
| RAIL_TX_OPTION_ALT_PREAMBLE_LEN_SHIFT |
Shift position of RAIL_TX_OPTION_ALT_PREAMBLE_LEN bit. |
| RAIL_TX_OPTION_CCA_PEAK_RSSI_SHIFT |
Shift position of RAIL_TX_OPTION_CCA_PEAK_RSSI bit. |
Definition at line
1453
of file
rail_types.h
.
Function Documentation
| void RAIL_EnableTxHoldOff | ( | RAIL_Handle_t |
railHandle,
|
| bool |
enable
|
||
| ) |
Prevent the radio from starting a transmit.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] enableEnable/Disable TX hold off.
- Returns
- void.
Enable TX hold off to prevent the radio from starting any transmits. Disable TX hold off to allow the radio to transmit again. Attempting to transmit with the TX hold off enabled will result in RAIL_EVENT_TX_BLOCKED and/or RAIL_EVENT_TXACK_BLOCKED events.
- Note
- This function does not affect a transmit that has already started. To stop an already-started transmission, use RAIL_Idle() with RAIL_IDLE_ABORT .
| RAIL_Status_t RAIL_GetTxPacketDetails | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_TxPacketDetails_t * |
pPacketDetails
|
||
| ) |
Gets detailed information about the last packet transmitted.
- Parameters
-
[in] railHandleA RAIL instance handle. [in,out] pPacketDetailsAn application-provided pointer to store RAIL_TxPacketDetails_t corresponding to the transmit event. The isAck and timeSent fields totalPacketBytes and timePosition must be initialized prior to each call: - isAck true to obtain details about the most recent ACK transmit, false to obtain details about the most recent app-initiated transmit.
- totalPacketBytes with the total number of bytes of the transmitted packet for RAIL to use when calculating the specified timestamp. This should account for all bytes sent over the air after the Preamble and Sync word(s), including CRC bytes.
- timePosition with a RAIL_PacketTimePosition_t value specifying the packet position to put in the timeSent field on return. This field will also be updated with the actual position corresponding to the timeSent value filled in.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketDetails was filled in, or an appropriate error code otherwise.
- Note
- Consider using RAIL_GetTxPacketDetailsAlt for smaller code size.
This function can only be called from callback context for either RAIL_EVENT_TX_PACKET_SENT or RAIL_EVENT_TXACK_PACKET_SENT events.
| RAIL_Status_t RAIL_GetTxPacketDetailsAlt | ( | RAIL_Handle_t |
railHandle,
|
| bool |
isAck,
|
||
| RAIL_Time_t * |
pPacketTime
|
||
| ) |
Gets detailed information about the last packet transmitted.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] isAckTrue to obtain details about the most recent ACK transmit. False to obtain details about the most recent app-initiated transmit. [out] pPacketTimeAn application-provided non-NULL pointer to store a RAIL_Time_t corresponding to the transmit event. This will be populated with a timestamp corresponding to an arbitrary location in the packet. Call RAIL_GetTxTimePreambleStart , RAIL_GetTxTimeSyncWordEnd , or RAIL_GetTxTimeFrameEnd to adjust the timestamp for different locations in the packet.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketTime was filled in, or an appropriate error code otherwise.
This function can only be called from callback context for either RAIL_EVENT_TX_PACKET_SENT or RAIL_EVENT_TXACK_PACKET_SENT events.
| RAIL_TxPower_t RAIL_GetTxPowerDbm | ( | RAIL_Handle_t |
railHandle
|
) |
Gets the TX power in terms of deci-dBm instead of raw power level.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- The current output power in deci-dBm.
This is a utility function for user convenience. Normally, to get TX power in dBm, the user would have to do the following:
This function wraps all those calls in a single function with power returned as the result.
| RAIL_Status_t RAIL_GetTxTimeFrameEnd | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
totalPacketBytes,
|
||
| RAIL_Time_t * |
pPacketTime
|
||
| ) |
Adjust a RAIL TX timestamp to refer to the end of frame.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] totalPacketBytesThe total number of bytes of the transmitted packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes. [in,out] pPacketTimeThe time that was returned in a RAIL_Time_t from a previous call to RAIL_GetTxPacketDetailsAlt for this same packet. After this function, the time at that location will be updated with the time that this packet finished on air. Must be non-NULL.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.
This timestamp adjustment API should be called in the same interrupt context as RAIL_GetTxPacketDetailsAlt in order to get the timestamp for the end of the frame.
| RAIL_Status_t RAIL_GetTxTimePreambleStart | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
totalPacketBytes,
|
||
| RAIL_Time_t * |
pPacketTime
|
||
| ) |
Adjust a RAIL TX timestamp to refer to the start of the preamble.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] totalPacketBytesThe total number of bytes of the transmitted packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes. [in,out] pPacketTimeThe time that was returned in a RAIL_Time_t from a previous call to RAIL_GetTxPacketDetailsAlt for this same packet. After this function, the time at that location will be updated with the time that the preamble for this packet started on air. Must be non-NULL.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.
This timestamp adjustment API should be called in the same interrupt context as RAIL_GetTxPacketDetailsAlt in order to get the timestamp for the beginning of the preamble.
| RAIL_Status_t RAIL_GetTxTimeSyncWordEnd | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
totalPacketBytes,
|
||
| RAIL_Time_t * |
pPacketTime
|
||
| ) |
Adjust a RAIL TX timestamp to refer to the end of the sync word.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] totalPacketBytesThe total number of bytes of the transmitted packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes. [in,out] pPacketTimeThe time that was returned in a RAIL_Time_t from a previous call to RAIL_GetTxPacketDetailsAlt for this same packet. After this function, the time at that location will be updated with the time that the sync word for this packet finished on air. Must be non-NULL.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.
This timestamp adjustment API should be called in the same interrupt context as RAIL_GetTxPacketDetailsAlt in order to get the timestamp for the end of the sync word.
| bool RAIL_IsTxHoldOffEnabled | ( | RAIL_Handle_t |
railHandle
|
) |
Check whether or not TX hold off is enabled.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- Returns true if TX hold off is enabled, false otherwise.
TX hold off can be enabled/disabled using RAIL_EnableTxHoldOff . Attempting to transmit with the TX hold off enabled will block the transmission and result in RAIL_EVENT_TX_BLOCKED and/or RAIL_EVENT_TXACK_BLOCKED events.
| RAIL_Status_t RAIL_SetCcaThreshold | ( | RAIL_Handle_t |
railHandle,
|
| int8_t |
ccaThresholdDbm
|
||
| ) |
Sets the CCA threshold in dBm.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] ccaThresholdDbmThe CCA threshold in dBm.
- Returns
- Status code indicating success of the function call.
Unlike RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx() , which can cause a transmit, this function only modifies the CCA threshold. A possible use case for this function involves setting the CCA threshold to invalid RSSI of -128 which blocks transmission by preventing clear channel assessments from succeeding.
| RAIL_Status_t RAIL_SetTxAltPreambleLength | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
length
|
||
| ) |
Sets an alternate transmitter preamble length.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] lengthThe desired preamble length, in bits.
- Returns
- Status code indicating success of the function call.
- Note
- Attempting to set a preamble length of 0xFFFF bits will result in RAIL_STATUS_INVALID_PARAMETER .
| RAIL_Status_t RAIL_SetTxPowerDbm | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_TxPower_t |
power
|
||
| ) |
Sets the TX power in terms of deci-dBm instead of raw power level.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] powerA desired deci-dBm power to be set.
- Returns
- RAIL Status variable indicate whether setting the power was successful.
This is a utility function for user convenience. Normally, to set TX power in dBm, the user would have to do the following:
This function wraps all those calls in a single function with power passed in as a parameter.
| RAIL_Status_t RAIL_StartCcaCsmaTx | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
channel,
|
||
| RAIL_TxOptions_t |
options,
|
||
| const RAIL_CsmaConfig_t * |
csmaConfig,
|
||
| const RAIL_SchedulerInfo_t * |
schedulerInfo
|
||
| ) |
Starts a non-blocking Transmit using CSMA.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelDefine the channel to transmit on. [in] optionsTX options to be applied to this transmit only. [in] csmaConfigA pointer to the RAIL_CsmaConfig_t structure describing the CSMA parameters to use for this transmit. [in] schedulerInfoInformation to allow the radio scheduler to place this transmit appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.
- Returns
- Status code indicating success of the function call. If successfully initiated, a transmit completion or failure will be reported by a later RAIL_Config_t::eventsCallback with the appropriate RAIL_Events_t .
Performs the Carrier Sense Multiple Access (CSMA) algorithm and, if the channel is deemed clear (RSSI below the specified threshold), it will commence transmission of the payload previously loaded via RAIL_WriteTxFifo() . Packets can be received during CSMA backoff periods if receive is active throughout the CSMA process. This will happen either by starting the CSMA process while receive is already active, or if the csmaBackoff time in the RAIL_CsmaConfig_t is less than the idleToRx time (set by RAIL_SetStateTiming() ). If the csmaBackoff time is greater than the idleToRx time, receive will only be active during CSMA's clear channel assessments.
If the CSMA algorithm deems the channel busy, the RAIL_Config_t::eventsCallback occurs with RAIL_EVENT_TX_CHANNEL_BUSY , and the contents of the transmit FIFO remain intact.
Returns an error if a previous transmit is still in progress. If changing channels, any ongoing packet reception is aborted.
In multiprotocol, ensure that the radio is properly yielded after this operation completes. See Yielding the radio for more details.
| RAIL_Status_t RAIL_StartCcaLbtTx | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
channel,
|
||
| RAIL_TxOptions_t |
options,
|
||
| const RAIL_LbtConfig_t * |
lbtConfig,
|
||
| const RAIL_SchedulerInfo_t * |
schedulerInfo
|
||
| ) |
Starts a non-blocking Transmit using LBT.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelDefine the channel to transmit on. [in] optionsTX options to be applied to this transmit only. [in] lbtConfigA pointer to the RAIL_LbtConfig_t structure describing the LBT parameters to use for this transmit. [in] schedulerInfoInformation to allow the radio scheduler to place this transmit appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.
- Returns
- Status code indicating success of the function call. If successfully initiated, a transmit completion or failure will be reported by a later RAIL_Config_t::eventsCallback with the appropriate RAIL_Events_t .
Performs the Listen Before Talk (LBT) algorithm and, if the channel is deemed clear (RSSI below the specified threshold), it will commence transmission of the payload previously loaded via RAIL_WriteTxFifo() . Packets can be received during LBT backoff periods if receive is active throughout the LBT process. This will happen either by starting the LBT process while receive is already active, or if the lbtBackoff time in the RAIL_LbtConfig_t is less than the idleToRx time (set by RAIL_SetStateTiming() ). If the lbtBackoff time is greater than the idleToRx time, receive will only be active during LBT's clear channel assessments.
If the LBT algorithm deems the channel busy, the RAIL_Config_t::eventsCallback occurs with RAIL_EVENT_TX_CHANNEL_BUSY , and the contents of the transmit FIFO remain intact.
Returns an error if a previous transmit is still in progress. If changing channels, any ongoing packet reception is aborted.
In multiprotocol, ensure that the radio is properly yielded after this operation completes. See Yielding the radio for more details.
| RAIL_Status_t RAIL_StartScheduledTx | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
channel,
|
||
| RAIL_TxOptions_t |
options,
|
||
| const RAIL_ScheduleTxConfig_t * |
config,
|
||
| const RAIL_SchedulerInfo_t * |
schedulerInfo
|
||
| ) |
Schedules sending a packet.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelDefine the channel to transmit on. [in] optionsTX options to be applied to this transmit only. [in] configA pointer to the RAIL_ScheduleTxConfig_t structure containing when the transmit should occur. [in] schedulerInfoInformation to allow the radio scheduler to place this transmit appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.
- Returns
- Status code indicating success of the function call. If successfully initiated, a transmit completion or failure will be reported by a later RAIL_Config_t::eventsCallback with the appropriate RAIL_Events_t .
Will begin transmission of the payload previously loaded via RAIL_WriteTxFifo() at the scheduled time. The time (in microseconds) as well as whether that time is absolute or relative, is specified using the RAIL_ScheduleTxConfig_t structure. Also specified in this structure is what to do if a scheduled transmit fires in the midst of receiving a packet.
Returns an error if a previous transmit is still in progress. If changing channels, any ongoing packet reception is aborted.
In multiprotocol, ensure that the radio is properly yielded after this operation completes. See Yielding the radio for more details.
| RAIL_Status_t RAIL_StartTx | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
channel,
|
||
| RAIL_TxOptions_t |
options,
|
||
| const RAIL_SchedulerInfo_t * |
schedulerInfo
|
||
| ) |
Starts a non-blocking transmit.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelDefine the channel to transmit on. [in] optionsTX options to be applied to this transmit only. [in] schedulerInfoInformation to allow the radio scheduler to place this transmit appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.
- Returns
- Status code indicating success of the function call. If successfully initiated, transmit completion or failure will be reported by a later RAIL_Config_t::eventsCallback with the appropriate RAIL_Events_t .
Will begin transmission of the payload previously loaded via RAIL_WriteTxFifo() immediately, or right after a packet currently being received is completed.
Returns an error if a previous transmit is still in progress. If changing channels, any ongoing packet reception is aborted.
In multiprotocol, ensure that the radio is properly yielded after this operation completes. See Yielding the radio for more details.
| RAIL_Status_t RAIL_StopTx | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_StopMode_t |
mode
|
||
| ) |
Stops an active or pending transmit.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] modeConfigure the types of transmits to stop.
- Returns
- RAIL_STATUS_NO_ERROR if the transmit was successfully canceled. Returns RAIL_STATUS_INVALID_STATE if the requested transmit mode cannot be stopped.
- Note
- This function will stop autoAcks in active transmit.