New API Name | Return Value | Comment |
PRORTC_IRQHandler(void) | void | |
RAILCb_SetupRxFifo(RAIL_Handle_t railHandle) | RAIL_Status_t | |
RAIL_BLE_CalibrateIr(RAIL_Handle_t railHandle, uint32_t *imageRejection) | RAIL_Status_t | |
RAIL_GetChannel(RAIL_Handle_t railHandle, uint16_t *channel) | RAIL_Status_t | |
RAIL_GetRssiOffset(RAIL_Handle_t railHandle) | int8_t | |
RAIL_GetRxPacketDetailsAlt(RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle, RAIL_RxPacketDetails_t *pPacketDetails) | RAIL_Status_t | |
RAIL_GetRxTimeFrameEnd(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) | RAIL_Status_t | |
RAIL_GetRxTimePreambleStart(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) | RAIL_Status_t | |
RAIL_GetRxTimeSyncWordEnd(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) | RAIL_Status_t | |
RAIL_GetTxPacketDetailsAlt(RAIL_Handle_t railHandle, bool isAck, RAIL_Time_t *pPacketTime) | RAIL_Status_t | |
RAIL_GetTxTimeFrameEnd(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) | RAIL_Status_t | |
RAIL_GetTxTimePreambleStart(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) | RAIL_Status_t | |
RAIL_GetTxTimeSyncWordEnd(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) | RAIL_Status_t | |
RAIL_IEEE802154_CalibrateIr2p4Ghz(RAIL_Handle_t railHandle, uint32_t *imageRejection) | RAIL_Status_t | |
RAIL_IEEE802154_CalibrateIrSubGhz(RAIL_Handle_t railHandle, uint32_t *imageRejection) | RAIL_Status_t | |
RAIL_IEEE802154_ConfigGB863MHzRadio(RAIL_Handle_t railHandle) | RAIL_Status_t | |
RAIL_IEEE802154_ConfigGB915MHzRadio(RAIL_Handle_t railHandle) | RAIL_Status_t | |
RAIL_PrepareChannel(RAIL_Handle_t railHandle, uint16_t channel) | RAIL_Status_t | |
RAIL_SetRssiOffset(RAIL_Handle_t railHandle, int8_t rssiOffset) | RAIL_Status_t | |
RAIL_SetRxFifo(RAIL_Handle_t railHandle, uint8_t *addr, uint16_t *size) | RAIL_Status_t | |
RAIL_SetTaskPriority(RAIL_Handle_t railHandle, uint8_t priority, RAIL_TaskType_t taskType) | RAIL_Status_t | |
RAIL_StopTx(RAIL_Handle_t railHandle, RAIL_StopMode_t mode) | RAIL_Status_t | |