Detailed information requested about the packet that was just, or is currently being, transmitted.
#include <
rail_types.h
>
Data Fields |
|
RAIL_PacketTimeStamp_t | timeSent |
The timestamp of the transmitted packet in the RAIL timebase, filled in by
RAIL_GetTxPacketDetails()
.
|
|
bool | isAck |
Indicate whether the transmitted packet was an automatic ACK.
|
Detailed information requested about the packet that was just, or is currently being, transmitted.
Definition at line
1910
of file
rail_types.h
.
Field Documentation
◆ isAck
bool RAIL_TxPacketDetails_t::isAck |
Indicate whether the transmitted packet was an automatic ACK.
In a generic sense, an automatic ACK is defined as a packet sent in response to a received ACK-requesting frame when auto-ACK is enabled. In a protocol specific sense this definition may be more or less restrictive to match the specification and you should refer to that protocol's documentation.
Definition at line
1923
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h