Packet Trace (PTI)
Basic APIs to set up and interact with PTI settings.
Modules |
|
| EFR32 | |
|
EFR32 PTI functionalityThese enumerations and structures are used with RAIL PTI API.
|
|
Enumerations |
|
| enum |
RAIL_PtiProtocol_t
{
RAIL_PTI_PROTOCOL_CUSTOM = 0, RAIL_PTI_PROTOCOL_THREAD = 2, RAIL_PTI_PROTOCOL_BLE = 3, RAIL_PTI_PROTOCOL_CONNECT = 4, RAIL_PTI_PROTOCOL_ZIGBEE = 5, RAIL_PTI_PROTOCOL_ZWAVE = 6 } |
|
The protocol that RAIL outputs via the Packet Trace Interface (PTI).
|
|
Functions |
|
| RAIL_Status_t | RAIL_ConfigPti ( RAIL_Handle_t railHandle, const RAIL_PtiConfig_t *ptiConfig) |
|
Configure PTI pin locations, serial protocols, and baud rates.
|
|
| RAIL_Status_t | RAIL_GetPtiConfig ( RAIL_Handle_t railHandle, RAIL_PtiConfig_t *ptiConfig) |
|
Get the currently active PTI configuration.
|
|
| RAIL_Status_t | RAIL_EnablePti ( RAIL_Handle_t railHandle, bool enable) |
|
Enable Packet Trace Interface (PTI) output of packet data.
|
|
| RAIL_Status_t | RAIL_SetPtiProtocol ( RAIL_Handle_t railHandle, RAIL_PtiProtocol_t protocol) |
|
Set a protocol that RAIL outputs on PTI.
|
|
Detailed Description
Basic APIs to set up and interact with PTI settings.
Enumeration Type Documentation
◆ RAIL_PtiProtocol_t
| enum RAIL_PtiProtocol_t |
The protocol that RAIL outputs via the Packet Trace Interface (PTI).
Definition at line
1539
of file
rail_types.h
.
Function Documentation
◆ RAIL_ConfigPti()
| RAIL_Status_t RAIL_ConfigPti | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_PtiConfig_t * |
ptiConfig
|
||
| ) |
Configure PTI pin locations, serial protocols, and baud rates.
- Parameters
-
[in] railHandleA RAIL instance handle (currently not used). [in] ptiConfigA configuration structure applied to the relevant PTI registers. A NULL ptiConfig will produce undefined behavior.
- Returns
- Status code indicating success of the function call.
This method must be called before RAIL_EnablePti() is called. Although a RAIL handle is included for potential future expansion of this function, it is currently not used. That is, there is only one PTI configuration that can be active on a chip, regardless of the number of protocols (unless the application updates the configuration upon a protocol switch), and the configuration is not saved in the RAIL instance. For optimal future compatibility, pass in a chip-specific handle, such as RAIL_EFR32_HANDLE .
◆ RAIL_EnablePti()
| RAIL_Status_t RAIL_EnablePti | ( | RAIL_Handle_t |
railHandle,
|
| bool |
enable
|
||
| ) |
Enable Packet Trace Interface (PTI) output of packet data.
- Parameters
-
[in] railHandleA RAIL instance handle (currently not used). [in] enablePTI is enabled if true; disable if false.
- Returns
- RAIL status indicating success of the function call.
Similar to having only one PTI configuration per chip, PTI can only be enabled or disabled for all protocols. It cannot be individually set to enabled and disabled per protocol (unless the application switches it when the protocol switches), and enable/disable is not saved as part of the RAIL instance. For optimal future compatibility, pass in a chip-specific handle, such as RAIL_EFR32_HANDLE .
◆ RAIL_GetPtiConfig()
| RAIL_Status_t RAIL_GetPtiConfig | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_PtiConfig_t * |
ptiConfig
|
||
| ) |
Get the currently active PTI configuration.
- Parameters
-
[in] railHandleA RAIL instance handle (currently not used). [out] ptiConfigA configuration structure filled with the active PTI configuration.
- Returns
- RAIL status indicating success of the function call.
Although most combinations of configurations can be set, it is safest to call this method after configuration to confirm which values were actually set. As in RAIL_ConfigPti, railHandle is not used. This function always returns the single active PTI configuration regardless of the active protocol. For optimal future compatibility, pass in a chip specific handle, such as RAIL_EFR32_HANDLE .
◆ RAIL_SetPtiProtocol()
| RAIL_Status_t RAIL_SetPtiProtocol | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_PtiProtocol_t |
protocol
|
||
| ) |
Set a protocol that RAIL outputs on PTI.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] protocolThe enumeration representing which protocol the node is using.
- Returns
- Status code indicating success of the function call.
The protocol is output via PTI for each packet. Before any protocol is set, the default value is RAIL_PTI_PROTOCOL_CUSTOM . Use one of the enumeration values so that the Network Analyzer can decode the packet.