RAIL_RxDutyCycleConfig_t Struct Reference
Structure to configure duty cycled receive mode.
#include <
rail_types.h
>
Data Fields |
|
| RAIL_RxChannelHoppingMode_t | mode |
|
The mode by which RAIL determines when to exit RX.
|
|
| uint32_t | parameter |
|
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode.
|
|
| uint32_t | delay |
|
Idle time in microseconds to wait before re-entering RX.
|
|
| RAIL_RxChannelHoppingDelayMode_t | delayMode |
|
Indicate how the timing specified in 'delay' should be applied.
|
|
Structure to configure duty cycled receive mode.
Definition at line
3175
of file
rail_types.h
.
Field Documentation
◆ mode
| RAIL_RxChannelHoppingMode_t RAIL_RxDutyCycleConfig_t::mode |
The mode by which RAIL determines when to exit RX.
Definition at line
3177
of file
rail_types.h
.
◆ parameter
| uint32_t RAIL_RxDutyCycleConfig_t::parameter |
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode.
See the comments on each value of RAIL_RxChannelHoppingMode_t to learn what to specify here.
Definition at line
3183
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h