Radio Configuration
Routines for setting up and querying radio configuration information.
Modules |
|
EFR32 | |
Types specific to the EFR32 for radio configuration.
|
Data Structures |
|
struct | RAIL_FrameType_t |
Configures if there is a frame type in your frame and the lengths of each frame.
|
|
struct | RAIL_ChannelConfigEntryAttr_t |
A channel configuration entry attribute structure.
|
|
struct | RAIL_ChannelConfigEntry_t |
A channel configuration entry structure, which defines a channel range and parameters across which a corresponding radio configuration is valid.
|
|
struct | RAIL_ChannelConfig_t |
A channel configuration structure, which defines the channel meaning when a channel number is passed into a RAIL function, e.g.,
RAIL_StartTx()
and
RAIL_StartRx()
.
|
|
struct | RAIL_ChannelMetadata_t |
Container for individual channel metadata.
|
Macros |
|
#define | RAIL_SETFIXEDLENGTH_INVALID (0xFFFFU) |
An invalid return value when calling
RAIL_SetFixedLength()
.
|
Typedefs |
|
typedef void(* | RAIL_RadioConfigChangedCallback_t ) ( RAIL_Handle_t railHandle, const RAIL_ChannelConfigEntry_t *entry) |
A pointer to a function called whenever a radio configuration change occurs.
|
Functions |
|
RAIL_Status_t | RAIL_ConfigRadio ( RAIL_Handle_t railHandle, RAIL_RadioConfig_t config) |
Load a static radio configuration.
|
|
uint16_t | RAIL_SetFixedLength ( RAIL_Handle_t railHandle, uint16_t length) |
Modify the currently configured fixed frame length in bytes.
|
|
uint16_t | RAIL_ConfigChannels ( RAIL_Handle_t railHandle, const RAIL_ChannelConfig_t *config, RAIL_RadioConfigChangedCallback_t cb) |
Configure the channels supported by this device.
|
|
RAIL_Status_t | RAIL_GetChannelMetadata ( RAIL_Handle_t railHandle, RAIL_ChannelMetadata_t *channelMetadata, uint16_t *length, uint16_t minChannel, uint16_t maxChannel) |
Get verbose listing of channel metadata for the current channel configuration.
|
|
RAIL_Status_t | RAIL_IsValidChannel ( RAIL_Handle_t railHandle, uint16_t channel) |
Check whether the channel exists in RAIL.
|
|
RAIL_Status_t | RAIL_PrepareChannel ( RAIL_Handle_t railHandle, uint16_t channel) |
Cause radio settings associated with a particular channel to be applied to hardware.
|
|
RAIL_Status_t | RAIL_GetChannel ( RAIL_Handle_t railHandle, uint16_t *channel) |
Return the current RAIL channel.
|
|
uint32_t | RAIL_GetSymbolRate ( RAIL_Handle_t railHandle) |
Return the symbol rate for the current PHY.
|
|
uint32_t | RAIL_GetBitRate ( RAIL_Handle_t railHandle) |
Return the bit rate for the current PHY.
|
|
RAIL_Status_t | RAIL_SetPaCTune ( RAIL_Handle_t railHandle, uint8_t txPaCtuneValue, uint8_t rxPaCtuneValue) |
Set the PA capacitor tune value for transmit and receive.
|
|
RAIL_Status_t | RAIL_GetSyncWords ( RAIL_Handle_t railHandle, RAIL_SyncWordConfig_t *syncWordConfig) |
Get the sync words and their length.
|
|
RAIL_Status_t | RAIL_ConfigSyncWords ( RAIL_Handle_t railHandle, const RAIL_SyncWordConfig_t *syncWordConfig) |
Set the selected sync words and their length.
|
Detailed Description
Routines for setting up and querying radio configuration information.
These routines allow for runtime flexibility in the radio configuration. Some of the parameters, however, are meant to be generated from the radio calculator in Simplicity Studio. The basic code to configure the radio from this calculator output looks like the example below.
For more information about the types of parameters that can be changed in the other functions and how to use them, see their individual documentation.
Macro Definition Documentation
◆ RAIL_SETFIXEDLENGTH_INVALID
#define RAIL_SETFIXEDLENGTH_INVALID (0xFFFFU) |
An invalid return value when calling RAIL_SetFixedLength() .
An invalid return value when calling RAIL_SetFixedLength() while the radio is not in fixed-length mode.
Definition at line
1247
of file
rail_types.h
.
Typedef Documentation
◆ RAIL_RadioConfigChangedCallback_t
RAIL_RadioConfigChangedCallback_t |
A pointer to a function called whenever a radio configuration change occurs.
- Parameters
-
[in] railHandle
A handle for RAIL instance. [in] entry
The radio configuration entry being changed to.
Definition at line
1523
of file
rail_types.h
.
Function Documentation
◆ RAIL_ConfigChannels()
uint16_t RAIL_ConfigChannels | ( | RAIL_Handle_t |
railHandle,
|
const RAIL_ChannelConfig_t * |
config,
|
||
RAIL_RadioConfigChangedCallback_t |
cb
|
||
) |
Configure the channels supported by this device.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] config
A pointer to the channel configuration for your device. This pointer will be cached in the library so it must exist for the runtime of the application. Typically, this should be what is stored in Flash by the configuration tool. [in] cb
Function called whenever a radio configuration change occurs.
- Returns
- Returns the first available channel in the configuration.
When configuring channels on EFR32, the radio tuner is reconfigured based on the frequency and channel spacing in the channel configuration.
- Note
- config can be NULL to simply register or unregister the cb callback function when using RAIL internal protocol-specific radio configuration APIs for BLE, IEEE 802.15.4, or Z-Wave, which lack callback specification. In this use case, 0 is returned.
◆ RAIL_ConfigRadio()
RAIL_Status_t RAIL_ConfigRadio | ( | RAIL_Handle_t |
railHandle,
|
RAIL_RadioConfig_t |
config
|
||
) |
Load a static radio configuration.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] config
A pointer to a radio configuration.
- Returns
- Status code indicating success of the function call.
The configuration passed into this function should be auto-generated and not manually created or edited. By default, this function should not be called in RAIL 2.x and later unless a non-default radio configuration needs to be applied. In RAIL 2.x and later, the RAIL_ConfigChannels function applies the default radio configuration automatically.
◆ RAIL_ConfigSyncWords()
RAIL_Status_t RAIL_ConfigSyncWords | ( | RAIL_Handle_t |
railHandle,
|
const RAIL_SyncWordConfig_t * |
syncWordConfig
|
||
) |
Set the selected sync words and their length.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] syncWordConfig
A non-NULL pointer to RAIL_SyncWordConfig_t specifying the sync words and their length. The desired length should be between 2 and 32 bits inclusive. Other values will result in RAIL_STATUS_INVALID_PARAMETER . The default syncWord continues to be valid.
- Returns
- Status code indicating success of the function call. When the custom sync word(s) applied by this API are no longer needed, or to revert to default sync word, calling RAIL_ConfigChannels() will re-establish the sync words specified in the radio configuration.
◆ RAIL_GetBitRate()
uint32_t RAIL_GetBitRate | ( | RAIL_Handle_t |
railHandle
|
) |
Return the bit rate for the current PHY.
- Parameters
-
[in] railHandle
A RAIL instance handle.
- Returns
- The bit rate in bits per second or 0.
The bit rate is the effective over-the-air data rate. It does not account for extra spreading for forward error correction, and so on, but accounts for modulation schemes, DSSS, and other configurations. For more information, see the modem calculator documentation. If the rate cannot be calculated, this function returns 0.
◆ RAIL_GetChannel()
RAIL_Status_t RAIL_GetChannel | ( | RAIL_Handle_t |
railHandle,
|
uint16_t * |
channel
|
||
) |
Return the current RAIL channel.
- Parameters
-
[in] railHandle
A RAIL instance handle. [out] channel
The channel for which RAIL is currently configured.
- Returns
- RAIL_STATUS_NO_ERROR on success or RAIL_STATUS_INVALID_CALL if the radio is not configured for any channel or RAIL_STATUS_INVALID_PARAMETER if channel parameter is NULL.
This function returns the channel configured for use corresponding to the specified RAIL handle whether or not the specified handle is the active one.
◆ RAIL_GetChannelMetadata()
RAIL_Status_t RAIL_GetChannelMetadata | ( | RAIL_Handle_t |
railHandle,
|
RAIL_ChannelMetadata_t * |
channelMetadata,
|
||
uint16_t * |
length,
|
||
uint16_t |
minChannel,
|
||
uint16_t |
maxChannel
|
||
) |
Get verbose listing of channel metadata for the current channel configuration.
- Parameters
-
[in] railHandle
A RAIL instance handle. [out] channelMetadata
Allocated array that will be populated with channel metadata. [in,out] length
Pointer to the length of the channelMetadata. [in] minChannel
Minimum channel number about which to collect data. [in] maxChannel
Maximum channel number about which to collect data. When execution completes, this value will be updated to the number of channels written to the array.
- Returns
- Status of the call. RAIL_STATUS_SUSPENDED means that, based on the currently active radio configuration, there are more channels to write than there is space provided in the allocated channelMetadata. However, the channel metadata that was written is valid. RAIL_STATUS_INVALID_STATE indicates that the channel configuration has not been configured.
◆ RAIL_GetSymbolRate()
uint32_t RAIL_GetSymbolRate | ( | RAIL_Handle_t |
railHandle
|
) |
Return the symbol rate for the current PHY.
- Parameters
-
[in] railHandle
A RAIL instance handle.
- Returns
- The symbol rate in symbols per second or 0.
The symbol rate is the rate of symbol changes over the air. For non-DSSS PHYs, this is the same as the baudrate. For DSSS PHYs, it is the baudrate divided by the length of a chipping sequence. For more information, see the modem calculator documentation. If the rate cannot be calculated, this function returns 0.
◆ RAIL_GetSyncWords()
RAIL_Status_t RAIL_GetSyncWords | ( | RAIL_Handle_t |
railHandle,
|
RAIL_SyncWordConfig_t * |
syncWordConfig
|
||
) |
Get the sync words and their length.
- Parameters
-
[in] railHandle
A RAIL instance handle. [out] syncWordConfig
An application-provided non-NULL pointer to store RAIL_SyncWordConfig_t sync word information.
- Returns
- Status code indicating success of the function call.
◆ RAIL_IsValidChannel()
RAIL_Status_t RAIL_IsValidChannel | ( | RAIL_Handle_t |
railHandle,
|
uint16_t |
channel
|
||
) |
Check whether the channel exists in RAIL.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] channel
A channel number to check.
- Returns
- Returns RAIL_STATUS_NO_ERROR if channel exists
Returns RAIL_STATUS_INVALID_PARAMETER if the given channel does not exist in the channel configuration currently used or RAIL_STATUS_NO_ERROR if the channel is valid.
◆ RAIL_PrepareChannel()
RAIL_Status_t RAIL_PrepareChannel | ( | RAIL_Handle_t |
railHandle,
|
uint16_t |
channel
|
||
) |
Cause radio settings associated with a particular channel to be applied to hardware.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] channel
The channel to prepare for use.
- Returns
- RAIL_STATUS_NO_ERROR on success or RAIL_STATUS_INVALID_PARAMETER if the given channel does not have an associated channel configuration entry or RAIL_STATUS_INVALID_STATE if the specified railHandle is not the current RAIL handle in use. RAIL_STATUS_INVALID_STATE is only used in the multiprotocol version of RAIL.
This function walks the channelConfigEntry list and applies the configuration associated with the specified channel. This function manually changes channels without starting a TX or RX operation.
When successful, the radio is idled. When unsuccessful, the radio state will not be altered.
◆ RAIL_SetFixedLength()
uint16_t RAIL_SetFixedLength | ( | RAIL_Handle_t |
railHandle,
|
uint16_t |
length
|
||
) |
Modify the currently configured fixed frame length in bytes.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] length
The expected fixed frame length. A value of 0 is infinite. A value of RAIL_SETFIXEDLENGTH_INVALID restores the frame's length back to the length specified by the default frame type configuration.
- Returns
- Length configured; The new frame length configured into the hardware for use. 0 if in infinite mode, or RAIL_SETFIXEDLENGTH_INVALID if the frame length has not yet been overridden by a valid value.
Sets the fixed-length configuration for transmit and receive. Be careful when using this function in receive and transmit as this function changes the default frame configuration and remains in force until it is called again with an input value of RAIL_SETFIXEDLENGTH_INVALID. This function will override any fixed or variable length settings from a radio configuration.
◆ RAIL_SetPaCTune()
RAIL_Status_t RAIL_SetPaCTune | ( | RAIL_Handle_t |
railHandle,
|
uint8_t |
txPaCtuneValue,
|
||
uint8_t |
rxPaCtuneValue
|
||
) |
Set the PA capacitor tune value for transmit and receive.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] txPaCtuneValue
PA Ctune value for TX mode. [in] rxPaCtuneValue
PA Ctune value for RX mode.
- Returns
- Status code indicating success of the function call.
Tunes the impedance of the transmit and receive modes by changing the amount of capacitance at the PA output.