RAIL_SyncWordConfig_t Struct Reference

RAIL sync words and length configuration.

#include < rail_types.h >

Data Fields

uint8_t syncWordBits
Sync word length in bits, between 2 and 32, inclusive.
uint32_t syncWord1
Sync Word1.
uint32_t syncWord2
Sync Word2.

RAIL sync words and length configuration.

Definition at line 2253 of file rail_types.h .

Field Documentation

◆ syncWordBits

uint8_t RAIL_SyncWordConfig_t::syncWordBits

Sync word length in bits, between 2 and 32, inclusive.

Definition at line 2255 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h