State Transitions
Data Structures |
|
| struct | RAIL_StateTransitions_t |
|
Used to specify radio states to transition to on success or failure.
|
|
| struct | RAIL_StateTiming_t |
|
A timing configuration structure for the RAIL State Machine.
|
|
Enumerations |
|
| enum |
RAIL_RadioState_t
{
RAIL_RF_STATE_INACTIVE = 0u, RAIL_RF_STATE_ACTIVE = (1u << 0), RAIL_RF_STATE_RX = (1u << 1), RAIL_RF_STATE_TX = (1u << 2), RAIL_RF_STATE_IDLE = (RAIL_RF_STATE_ACTIVE), RAIL_RF_STATE_RX_ACTIVE = (RAIL_RF_STATE_RX | RAIL_RF_STATE_ACTIVE), RAIL_RF_STATE_TX_ACTIVE = (RAIL_RF_STATE_TX | RAIL_RF_STATE_ACTIVE) } |
|
The state of the radio.
|
|
| enum |
RAIL_IdleMode_t
{
RAIL_IDLE , RAIL_IDLE_ABORT , RAIL_IDLE_FORCE_SHUTDOWN , RAIL_IDLE_FORCE_SHUTDOWN_CLEAR_FLAGS } |
|
An enumeration for the different types of supported idle modes.
|
|
Functions |
|
| RAIL_Status_t | RAIL_SetRxTransitions ( RAIL_Handle_t railHandle, const RAIL_StateTransitions_t *transitions) |
|
Configure RAIL automatic state transitions after RX.
|
|
| RAIL_Status_t | RAIL_GetRxTransitions ( RAIL_Handle_t railHandle, RAIL_StateTransitions_t *transitions) |
|
Get the current RAIL automatic state transitions after RX.
|
|
| RAIL_Status_t | RAIL_SetTxTransitions ( RAIL_Handle_t railHandle, const RAIL_StateTransitions_t *transitions) |
|
Configure RAIL automatic state transitions after TX.
|
|
| RAIL_Status_t | RAIL_GetTxTransitions ( RAIL_Handle_t railHandle, RAIL_StateTransitions_t *transitions) |
|
Get the current RAIL automatic state transitions after TX.
|
|
| RAIL_Status_t | RAIL_SetStateTiming ( RAIL_Handle_t railHandle, RAIL_StateTiming_t *timings) |
|
Configure RAIL automatic state transition timing.
|
|
| void | RAIL_Idle ( RAIL_Handle_t railHandle, RAIL_IdleMode_t mode, bool wait) |
|
Place the radio into an idle state.
|
|
| RAIL_RadioState_t | RAIL_GetRadioState ( RAIL_Handle_t railHandle) |
|
Get the current radio state.
|
|
Enumeration Type Documentation
◆ RAIL_IdleMode_t
| enum RAIL_IdleMode_t |
An enumeration for the different types of supported idle modes.
These vary how quickly and destructively they put the radio into idle.
| Enumerator | |
|---|---|
| RAIL_IDLE |
Idle the radio by turning off receive and canceling any future scheduled receive or transmit operations. It does not abort a receive or transmit in progress. |
| RAIL_IDLE_ABORT |
Idle the radio by turning off receive and any scheduled events. It also aborts any receive, transmit, or scheduled events in progress. |
| RAIL_IDLE_FORCE_SHUTDOWN |
Force the radio into a shutdown mode by stopping whatever state is in progress. This is a more destructive shutdown than RAIL_IDLE or RAIL_IDLE_ABORT and can be useful in certain situations when directed by the support team or for debugging. Note that this method may corrupt receive and transmit buffers so it requires a more thorough cleanup and any held packets will be lost. |
| RAIL_IDLE_FORCE_SHUTDOWN_CLEAR_FLAGS |
Similar to the RAIL_IDLE_FORCE_SHUTDOWN command, however, it will also clear any pending RAIL events related to receive and transmit. |
Definition at line
1731
of file
rail_types.h
.
◆ RAIL_RadioState_t
| enum RAIL_RadioState_t |
The state of the radio.
Definition at line
1664
of file
rail_types.h
.
Function Documentation
◆ RAIL_GetRadioState()
| RAIL_RadioState_t RAIL_GetRadioState | ( | RAIL_Handle_t |
railHandle
|
) |
Get the current radio state.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- An enumeration for the current radio state.
Returns the state of the radio as a bitmask containing: RAIL_RF_STATE_IDLE , RAIL_RF_STATE_RX , RAIL_RF_STATE_TX , and RAIL_RF_STATE_ACTIVE . RAIL_RF_STATE_IDLE , RAIL_RF_STATE_RX , and RAIL_RF_STATE_TX bits are mutually exclusive. The radio can transition through intermediate states, which are not reported but are instead considered part of the state most closely associated. For example, when the radio is warming up or shutting down the transmitter or receiver, this function returns RAIL_RF_STATE_TX or RAIL_RF_STATE_RX , respectively. When transitioning directly from RX to TX or vice-versa, this function returns the earlier state.
◆ RAIL_GetRxTransitions()
| RAIL_Status_t RAIL_GetRxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Get the current RAIL automatic state transitions after RX.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] transitionsThe state transitions that apply after receive.
- Returns
- Status code indicating a success of the function call.
Retrieves the current state transitions after RX and stores them in the transitions argument.
◆ RAIL_GetTxTransitions()
| RAIL_Status_t RAIL_GetTxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Get the current RAIL automatic state transitions after TX.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] transitionsThe state transitions that apply after transmission.
- Returns
- Status code indicating a success of the function call.
Retrieves the current state transitions after TX and stores them in the transitions argument.
◆ RAIL_Idle()
| void RAIL_Idle | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_IdleMode_t |
mode,
|
||
| bool |
wait
|
||
| ) |
Place the radio into an idle state.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] modeThe method for shutting down the radio. [in] waitWhether this function should wait for the radio to reach idle before returning.
- Returns
- void.
This function is used to remove the radio from TX and RX states. How these states are left is defined by the mode parameter.
In multiprotocol, this API will also cause the radio to be yielded so that other tasks can be run. See Yielding the radio for more details.
◆ RAIL_SetRxTransitions()
| RAIL_Status_t RAIL_SetRxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Configure RAIL automatic state transitions after RX.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] transitionsThe state transitions to apply after reception.
- Returns
- Status code indicating success of the function call.
This function fails if unsupported transitions are passed in or if the radio is currently in the RX state. Success can transition to TX, RX, or IDLE, while error can transition to RX or IDLE. The timings of state transitions from the RX state are not guaranteed when packets are longer than 16 seconds on-air.
◆ RAIL_SetStateTiming()
| RAIL_Status_t RAIL_SetStateTiming | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_StateTiming_t * |
timings
|
||
| ) |
Configure RAIL automatic state transition timing.
- Parameters
-
[in] railHandleA RAIL instance handle. [in,out] timingsThe timings used to configure the RAIL state machine. This structure is overwritten with the actual times that were set, if an input timing is invalid.
- Returns
- Status code indicating a success of the function call.
The timings given are close to the actual transition time. However, a still uncharacterized software overhead occurs. Also, timings are not always adhered to when using an automatic transition after an error, due to the cleanup required to recover from the error.
◆ RAIL_SetTxTransitions()
| RAIL_Status_t RAIL_SetTxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Configure RAIL automatic state transitions after TX.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] transitionsThe state transitions to apply after transmission.
- Returns
- Status code indicating a success of the function call.
This function fails if unsupported transitions are passed in or if the radio is currently in the TX state. Success and error can each transition to RX or IDLE.