Configuration structure for Z-Wave Long Range Ack.

DeprecatedRAIL 2.x synonym of sl_rail_zwave_lr_ack_data_t.

Public Attributes#

int8_t

Radio noise level measured on the channel the frame is transmitted on.

int8_t

Transmit power used to transmit the ongoing Z-Wave Long Range Ack.

int8_t

Signal strength measured while receiving the Z-Wave Long Range frame.

Public Attribute Documentation#

noiseFloorDbm#

int8_t RAIL_ZWAVE_LrAckData_t::noiseFloorDbm

Radio noise level measured on the channel the frame is transmitted on.

DeprecatedRAIL 2.x synonym of sl_rail_zwave_lr_ack_data_t::noise_floor_dbm.


txPowerDbm#

int8_t RAIL_ZWAVE_LrAckData_t::txPowerDbm

Transmit power used to transmit the ongoing Z-Wave Long Range Ack.

DeprecatedRAIL 2.x synonym of sl_rail_zwave_lr_ack_data_t::transmit_power_dbm.


receiveRssiDbm#

int8_t RAIL_ZWAVE_LrAckData_t::receiveRssiDbm

Signal strength measured while receiving the Z-Wave Long Range frame.

DeprecatedRAIL 2.x synonym of sl_rail_zwave_lr_ack_data_t::receive_rssi_dbm.