Configuration structure for Z-Wave Long Range Ack.
Public Attributes#
int8_t
Radio noise level measured on the channel the frame is transmitted on.
int8_t
Transmit power used to transmit the ongoing Z-Wave Long Range Ack.
int8_t
Signal strength measured while receiving the Z-Wave Long Range frame.
Public Attribute Documentation#
noise_floor_dbm#
int8_t sl_rail_zwave_lr_ack_data_t::noise_floor_dbm
Radio noise level measured on the channel the frame is transmitted on.
transmit_power_dbm#
int8_t sl_rail_zwave_lr_ack_data_t::transmit_power_dbm
Transmit power used to transmit the ongoing Z-Wave Long Range Ack.
receive_rssi_dbm#
int8_t sl_rail_zwave_lr_ack_data_t::receive_rssi_dbm
Signal strength measured while receiving the Z-Wave Long Range frame.