Configuration parameters for thermal protection.

Public Attributes#

bool

Indicates whether the protection is enabled.

uint8_t

Mandatory temperature cool down when the threshold is exceeded, in degrees Kelvin.

uint16_t

Temperature above which transmit is blocked, in degrees Kelvin.

Public Attribute Documentation#

enable#

bool sl_rail_chip_temp_config_t::enable

Indicates whether the protection is enabled.


cool_down_kelvin#

uint8_t sl_rail_chip_temp_config_t::cool_down_kelvin

Mandatory temperature cool down when the threshold is exceeded, in degrees Kelvin.


threshold_kelvin#

uint16_t sl_rail_chip_temp_config_t::threshold_kelvin

Temperature above which transmit is blocked, in degrees Kelvin.