FULL_MAC_DRIVER_API

Functions

sl_status_t wf200_set_mac_address (const wf200_mac_address_t *mac, wf200_interface_t interface)
Set the MAC address used by wf200.
sl_status_t wf200_send_join_command (const uint8_t *ssid, uint32_t ssid_length, uint16_t security_mode, const uint8_t *passkey, uint32_t passkey_length)
As a station, send a command to join a Wi-Fi network.
sl_status_t wf200_send_disconnect_command (void)
As a station, send a disconnection request to the AP.
sl_status_t wf200_start_ap_command (uint32_t channel, uint8_t *ssid, uint32_t ssid_length, WfmSecurityMode security, const uint8_t *passkey, uint8_t passkey_length)
Send a command to start the softap mode.
sl_status_t wf200_update_ap_command (uint16_t beacon_iedata_length, uint16_t proberesp_iedata_length, uint32_t *beacon_iedata, uint32_t *proberesp_iedata)
Update AP settings.
sl_status_t wf200_stop_ap_command (void)
Send a command to stop the softap mode.
sl_status_t wf200_send_ethernet_frame ( wf200_frame_t *frame, uint32_t data_length, wf200_interface_t interface)
Send an Ethernet frame.
sl_status_t wf200_send_scan_command (uint16_t scan_mode, const uint8_t *channel_list, uint16_t channel_list_count, const WfmHiSsidDef_t *ssid_list, uint16_t ssid_list_count, const uint8_t *ie_data, uint16_t ie_data_length)
send a scan command
sl_status_t wf200_send_stop_scan_command (void)
Stop a scan process.
sl_status_t wf200_get_signal_strength (uint32_t *signal_strength)
Get the signal strength of the last packets received.
sl_status_t wf200_disconnect_ap_client_command (const wf200_mac_address_t *client)
In AP mode, disconnect the specified client.
sl_status_t wf200_set_power_mode ( WfmPmMode mode, uint16_t interval)
Set the power mode used as a station.
sl_status_t wf200_add_multicast_address (const wf200_mac_address_t *mac_address, wf200_interface_t interface)
Configure the maximum number of clients supported in softap mode //TODO.
sl_status_t wf200_set_max_ap_client (uint32_t max_clients)
Configure the maximum number of clients supported in softap mode.

Function Documentation

◆ wf200_add_multicast_address()

sl_status_t wf200_add_multicast_address ( const wf200_mac_address_t * mac_address,
wf200_interface_t interface
)

Configure the maximum number of clients supported in softap mode //TODO.

Parameters
mac_address
interface Interface used to send the ethernet frame. wf200_interface_t.
  • WF200_STA_INTERFACE
  • WF200_SOFTAP_INTERFACE
Returns
SL_SUCCESS if the setting is applied correctly, SL_ERROR otherwise

Definition at line 581 of file wf200.c .

References WfmHiAddMulticastAddrReqBody_t::Mac , and WFM_HI_ADD_MULTICAST_ADDR_REQ_ID .

◆ wf200_disconnect_ap_client_command()

sl_status_t wf200_disconnect_ap_client_command ( const wf200_mac_address_t * client )

In AP mode, disconnect the specified client.

Parameters
client the mac address of the client to disconnect
Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 541 of file wf200.c .

References WfmHiDisconnectApClientReqBody_t::Mac , and WFM_HI_DISCONNECT_AP_CLIENT_REQ_ID .

◆ wf200_get_signal_strength()

sl_status_t wf200_get_signal_strength ( uint32_t * signal_strength )

Get the signal strength of the last packets received.

Parameters
signal_strength return the RCPI value averaged on the last packets received. RCPI ranges from 0 - 220 with 220 corresponds to 0dBm and each increment represents an increase of 0.5 dBm
Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 505 of file wf200.c .

◆ wf200_send_disconnect_command()

sl_status_t wf200_send_disconnect_command ( void )

As a station, send a disconnection request to the AP.

Returns
SL_SUCCESS if the command has been sent correctly, SL_ERROR otherwise

Definition at line 279 of file wf200.c .

References WFM_HI_DISCONNECT_REQ_ID .

◆ wf200_send_ethernet_frame()

sl_status_t wf200_send_ethernet_frame ( wf200_frame_t * frame,
uint32_t data_length,
wf200_interface_t interface
)

Send an Ethernet frame.

Parameters
frame Ethernet frame to be sent
data_length Size of the frame
interface Interface used to send the ethernet frame.
  • WF200_STA_INTERFACE
  • WF200_SOFTAP_INTERFACE
Returns
SL_SUCCESS if the command has been sent correctly, SL_ERROR otherwise

Definition at line 379 of file wf200.c .

◆ wf200_send_join_command()

sl_status_t wf200_send_join_command ( const uint8_t * ssid,
uint32_t ssid_length,
uint16_t security_mode,
const uint8_t * passkey,
uint32_t passkey_length
)

As a station, send a command to join a Wi-Fi network.

Note
The PDS file contains the WF200 settings
Parameters
ssid Name of the AP to connect to
ssid_length Size of the SSID name
security_mode Security mode of the AP
  • WFM_SECURITY_MODE_OPEN
  • WFM_SECURITY_MODE_WEP
  • WFM_SECURITY_MODE_WPA2_WPA1_PSK
  • WFM_SECURITY_MODE_WPA2_PSK
passkey Passkey of the AP
passkey_length Size of the passkey
Returns
SL_SUCCESS if the command has been sent correctly, SL_ERROR otherwise

Definition at line 224 of file wf200.c .

◆ wf200_send_scan_command()

sl_status_t wf200_send_scan_command ( uint16_t scan_mode,
const uint8_t * channel_list,
uint16_t channel_list_count,
const WfmHiSsidDef_t * ssid_list,
uint16_t ssid_list_count,
const uint8_t * ie_data,
uint16_t ie_data_length
)

send a scan command

Parameters
scan_mode Mode used for scanning
  • WFM_SCAN_MODE_PASSIVE
  • WFM_SCAN_MODE_ACTIVE
channel_list Channels to be scanned [1;13]
channel_list_count Number of channels to be scanned. If 0 the scan will be performed on every channel.
ssid_list Specify SSID names to look for. WF200 will send information only the specified SSID. Null to request information for every AP found.
ssid_list_count The number of SSID specified [0;2]
ie_data NA
ie_data_length NA
Returns
SL_SUCCESS if the command has been sent correctly, SL_ERROR otherwise

Definition at line 419 of file wf200.c .

◆ wf200_send_stop_scan_command()

sl_status_t wf200_send_stop_scan_command ( void )

Stop a scan process.

Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 494 of file wf200.c .

References WFM_HI_STOP_SCAN_REQ_ID .

◆ wf200_set_mac_address()

sl_status_t wf200_set_mac_address ( const wf200_mac_address_t * mac,
wf200_interface_t interface
)

Set the MAC address used by wf200.

Parameters
mac MAC address of the interface
interface Interface to be configured. wf200_interface_t.
  • WF200_STA_INTERFACE
  • WF200_SOFTAP_INTERFACE
Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 202 of file wf200.c .

References WfmHiSetMacAddressReqBody_t::MacAddr , and WFM_HI_SET_MAC_ADDRESS_REQ_ID .

◆ wf200_set_max_ap_client()

sl_status_t wf200_set_max_ap_client ( uint32_t max_clients )

Configure the maximum number of clients supported in softap mode.

Note
wf200_set_max_ap_client() has to be called after wf200_start_ap_command() . If the softap is stopped or wf200 resets, the command has to be issued again.
Parameters
max_clients Maximum number of clients supported in softap.
Returns
SL_SUCCESS if the setting is applied correctly, SL_ERROR otherwise

Definition at line 597 of file wf200.c .

References WfmHiSetMaxApClientCountReqBody_t::Count , and WFM_HI_SET_MAX_AP_CLIENT_COUNT_REQ_ID .

◆ wf200_set_power_mode()

sl_status_t wf200_set_power_mode ( WfmPmMode mode,
uint16_t interval
)

Set the power mode used as a station.

Note
the power mode has to be set once the connection with the AP is established
Parameters
mode Power mode to be used by the connection
  • WFM_PM_MODE_ACTIVE
  • WFM_PM_MODE_PS
  • WFM_PM_MODE_AUTO
interval interval of sleep in seconds
Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 561 of file wf200.c .

References WfmHiSetPmModeReqBody_t::PowerMode , and WFM_HI_SET_PM_MODE_REQ_ID .

◆ wf200_start_ap_command()

sl_status_t wf200_start_ap_command ( uint32_t channel,
uint8_t * ssid,
uint32_t ssid_length,
WfmSecurityMode security,
const uint8_t * passkey,
uint8_t passkey_length
)

Send a command to start the softap mode.

Parameters
channel channel used by the softap
ssid SSID name used by the softap
ssid_length SSID name length
security Security level used by the AP
  • WFM_SECURITY_MODE_OPEN
  • WFM_SECURITY_MODE_WEP
  • WFM_SECURITY_MODE_WPA2_WPA1_PSK
  • WFM_SECURITY_MODE_WPA2_PSK
passkey Passkey used by the softap if security level is different to WFM_SECURITY_MODE_OPEN
passkey_length Passkey length, [8;64]
Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 299 of file wf200.c .

References WfmHiStartApReqBody_t::Channel , WfmHiStartApReqBody_t::Password , WfmHiStartApReqBody_t::PasswordLength , WfmHiSsidDef_t::Ssid , WfmHiStartApReqBody_t::SsidDef , WFM_API_PASSWORD_SIZE , WFM_HI_START_AP_REQ_ID , and WFM_SECURITY_MODE_OPEN .

◆ wf200_stop_ap_command()

sl_status_t wf200_stop_ap_command ( void )

Send a command to stop the softap mode.

Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 364 of file wf200.c .

References WFM_HI_STOP_AP_REQ_ID .

◆ wf200_update_ap_command()

sl_status_t wf200_update_ap_command ( uint16_t beacon_iedata_length,
uint16_t proberesp_iedata_length,
uint32_t * beacon_iedata,
uint32_t * proberesp_iedata
)

Update AP settings.

Parameters
beacon_iedata_length length of Beacon IE data
proberesp_iedata_length length of probe response IE data
beacon_iedata Beacon IE data
proberesp_iedata probe response IE data
Returns
SL_SUCCESS if the request has been sent correctly, SL_ERROR otherwise

Definition at line 345 of file wf200.c .

References WfmHiUpdateApReqBody_t::BeaconIeDataLength , and WFM_HI_UPDATE_AP_REQ_ID .