API messagesFULL_MAC_API

WFM API messages.

Data Structures

struct WfmHiSetMacAddressReqBody_t
Request message body for WfmHiSetMacAddressReq_t .
struct WfmHiSetMacAddressReq_t
Request message to set MAC address of the interface.
struct WfmHiSetMacAddressCnfBody_t
Confirmation message body for WfmHiSetMacAddressCnf_t .
struct WfmHiSetMacAddressCnf_t
Confirmation message for WfmHiSetMacAddressReq_t .
struct WfmHiConnectReqBody_t
Request message body for WfmHiConnectReq_t .
struct WfmHiConnectReq_t
Request message for connecting to a Wi-Fi network.
struct WfmHiConnectCnfBody_t
Confirmation message body for WfmHiConnectCnf_t .
struct WfmHiConnectCnf_t
Confirmation message for WfmHiConnectReq_t .
struct WfmHiConnectIndBody_t
Indication message body for WfmHiConnectInd_t .
struct WfmHiConnectInd_t
Indication message used to signal the completion of a connection operation.
struct WfmHiDisconnectCnfBody_t
Confirmation message body for WfmHiDisconnectCnf_t .
struct WfmHiDisconnectCnf_t
Confirmation message for WfmHiDisconnectReq_t .
struct WfmHiDisconnectIndBody_t
Indication message body for WfmHiDisconnectInd_t .
struct WfmHiDisconnectInd_t
Indication message used to signal the completion of a disconnection operation.
struct WfmHiGetSignalStrengthCnfBody_t
Confirmation message body for WfmHiGetSignalStrengthCnf_t .
struct WfmHiGetSignalStrengthCnf_t
Confirmation message for WfmHiGetSignalStrengthReq_t .
struct WfmHiSetPmModeReqBody_t
Request message body for WfmHiSetPmModeReq_t .
struct WfmHiSetPmModeReq_t
Request message for setting the power management mode of the device.
struct WfmHiSetPmModeCnfBody_t
Confirmation message body for WfmHiSetPmModeCnf_t .
struct WfmHiSetPmModeCnf_t
Confirmation message for WfmHiSetPmModeReq_t .
struct WfmHiStartApReqBody_t
Request message body for WfmHiStartApReq_t .
struct WfmHiStartApReq_t
Request message for starting a Wi-Fi network.
struct WfmHiStartApCnfBody_t
Confirmation message body for WfmHiStartApCnf_t .
struct WfmHiStartApCnf_t
Confirmation message for WfmHiStartApReq_t .
struct WfmHiStartApIndBody_t
Indication message body for WfmHiStartApInd_t .
struct WfmHiStartApInd_t
Indication message used to signal the completion of a start request.
struct WfmHiUpdateApReqBody_t
Request message body for WfmHiUpdateApReq_t .
struct WfmHiUpdateApReq_t
Request message for updating parameters of the started Wi-Fi network.
struct WfmHiUpdateApCnfBody_t
Confirmation message body for WfmHiUpdateApCnf_t .
struct WfmHiUpdateApCnf_t
Confirmation message for WfmHiUpdateApReq_t .
struct WfmHiStopApCnfBody_t
Confirmation message body for WfmHiStopApCnf_t .
struct WfmHiStopApCnf_t
Confirmation message for WfmHiStopApReq_t .
struct WfmHiApClientConnectedIndBody_t
Indication message body for WfmHiApClientConnectedInd_t .
struct WfmHiApClientConnectedInd_t
Indication message used to signal a connected station.
struct WfmHiApClientRejectedIndBody_t
Indication message body for WfmHiApClientRejectedInd_t .
struct WfmHiApClientRejectedInd_t
Indication message used to signal a rejected connection attempt from a station.
struct WfmHiDisconnectApClientReqBody_t
Request message body for WfmHiDisconnectApClientReq_t .
struct WfmHiDisconnectApClientReq_t
Request message for disconnecting a client from the started Wi-Fi network.
struct WfmHiDisconnectApClientCnfBody_t
Confirmation message body for WfmHiDisconnectApClientCnf_t .
struct WfmHiDisconnectApClientCnf_t
Confirmation message for WfmHiDisconnectApClientReq_t .
struct WfmHiApClientDisconnectedIndBody_t
Indication message body for WfmHiApClientDisconnectedInd_t .
struct WfmHiApClientDisconnectedInd_t
Indication message used to signal a disconnected station.
struct WfmHiSendFrameReqBody_t
Request message body for WfmHiSendFrameReq_t .
struct WfmHiSendFrameReq_t
Request message for sending a packet to the network.
struct WfmHiSendFrameCnfBody_t
Confirmation message body for WfmHiSendFrameCnf_t .
struct WfmHiSendFrameCnf_t
Confirmation message for WfmHiSendFrameReq_t .
struct WfmHiReceivedIndBody_t
Indication message body for WfmHiReceivedInd_t .
struct WfmHiReceivedInd_t
Indication message used to signal a received packet.
struct WfmHiStartScanReqBody_t
Request message body for WfmHiStartScanReq_t .
struct WfmHiStartScanReq_t
Request message for starting a scan to detect near-by access points.
struct WfmHiStartScanCnfBody_t
Confirmation message body for WfmHiStartScanCnf_t .
struct WfmHiStartScanCnf_t
Confirmation message for WfmHiStartScanReq_t .
struct WfmHiStopScanCnfBody_t
Confirmation message body for WfmHiStopScanCnf_t .
struct WfmHiStopScanCnf_t
Confirmation message for WfmHiStopScanReq_t .
struct WfmHiScanResultIndBody_t
Indication message body for WfmHiScanResultInd_t .
struct WfmHiScanResultInd_t
Indication message used to signal an access point has been detected.
struct WfmHiScanCompleteIndBody_t
Indication message body for WfmHiScanCompleteInd_t .
struct WfmHiScanCompleteInd_t
Indication message used to signal a scan was completed.
struct WfmHiJoinIbssReqBody_t
Request message body for WfmHiJoinIbssReq_t .
struct WfmHiJoinIbssReq_t
Request message for connecting to or starting an IBSS network.
struct WfmHiJoinIbssCnfBody_t
Confirmation message body for WfmHiJoinIbssCnf_t .
struct WfmHiJoinIbssCnf_t
Confirmation message for WfmHiJoinIbssReq_t .
struct WfmHiJoinIbssIndBody_t
Indication message body for WfmHiJoinIbssInd_t .
struct WfmHiJoinIbssInd_t
Indication message used to signal the completion of a join request.
struct WfmHiLeaveIbssCnfBody_t
Confirmation message body for WfmHiLeaveIbssCnf_t .
struct WfmHiLeaveIbssCnf_t
Confirmation message for WfmHiLeaveIbssReq_t .
struct WfmHiAddMulticastAddrReqBody_t
Request message body for WfmHiAddMulticastAddrReq_t .
struct WfmHiAddMulticastAddrReq_t
Request message for adding a multicast address to the multicast filter whitelist.
struct WfmHiAddMulticastAddrCnfBody_t
Confirmation message body for WfmHiAddMulticastAddrCnf_t .
struct WfmHiAddMulticastAddrCnf_t
Confirmation message for WfmHiAddMulticastAddrReq_t .
struct WfmHiRemoveMulticastAddrReqBody_t
Request message body for WfmHiRemoveMulticastAddrReq_t .
struct WfmHiRemoveMulticastAddrReq_t
Request message for removing a multicast address from the multicast filter whitelist.
struct WfmHiRemoveMulticastAddrCnfBody_t
Confirmation message body for WfmHiRemoveMulticastAddrCnf_t .
struct WfmHiRemoveMulticastAddrCnf_t
Confirmation message for WfmHiRemoveMulticastAddrReq_t .
struct WfmHiSetMaxApClientCountReqBody_t
Request message body for WfmHiSetMaxApClientCountReq_t .
struct WfmHiSetMaxApClientCountReq_t
Request message for setting the maximum number of connected clients.
struct WfmHiSetMaxApClientCountCnfBody_t
Confirmation message body for WfmHiSetMaxApClientCountCnf_t .
struct WfmHiSetMaxApClientCountCnf_t
Confirmation message for WfmHiSetMaxApClientCountReq_t .
struct WfmHiSetMaxApClientInactivityReqBody_t
Request message body for WfmHiSetMaxApClientInactivityReq_t .
struct WfmHiSetMaxApClientInactivityReq_t
Request message for setting the maximum number of connected clients.
struct WfmHiSetMaxApClientInactivityCnfBody_t
Confirmation message body for WfmHiSetMaxApClientCountCnf_t .
struct WfmHiSetMaxApClientInactivityCnf_t
Confirmation message for WfmHiSetMaxApClientInactivityReq_t .
struct WfmHiSetRoamParametersReqBody_t
Request message body for WfmHiSetRoamParametersReq_t .
struct WfmHiSetRoamParametersReq_t
Request message for setting the roaming parameters.
struct WfmHiSetRoamParametersCnfBody_t
Confirmation message body for WfmHiSetRoamParametersCnf_t .
struct WfmHiSetRoamParametersCnf_t
Confirmation message for WfmHiSetRoamParametersReq_t .
struct WfmHiSetTxRateParametersReqBody_t
Request message body for WfmHiSetTxRateParametersReq_t .
struct WfmHiSetTxRateParametersReq_t
Request message for setting the TX rate set parameters.
struct WfmHiSetTxRateParametersCnfBody_t
Confirmation message body for WfmHiSetTxRateParametersCnf_t .
struct WfmHiSetTxRateParametersCnf_t
Confirmation message for WfmHiSetTxRateParametersReq_t .
struct WfmHiSetArpIpAddressReqBody_t
Request message body for WfmHiSetArpIpAddressReq_t .
struct WfmHiSetArpIpAddressReq_t
Request message for setting the Address Resolution Protocol (ARP) offloading state.
struct WfmHiSetArpIpAddressCnfBody_t
Confirmation message body for WfmHiSetArpIpAddressCnf_t .
struct WfmHiSetArpIpAddressCnf_t
Confirmation message for WfmHiSetArpIpAddressReq_t .
struct WfmHiSetNsIpAddressReqBody_t
Request message body for WfmHiSetNsIpAddressReq_t .
struct WfmHiSetNsIpAddressReq_t
Request message for setting the Neighbor Discovery Protocol (NDP) offloading state.
struct WfmHiSetNsIpAddressCnfBody_t
Confirmation message body for WfmHiSetNsIpAddressCnf_t .
struct WfmHiSetNsIpAddressCnf_t
Confirmation message for WfmHiSetNsIpAddressReq_t .
struct WfmHiSetBroadcastFilterReqBody_t
Request message body for WfmHiSetBroadcastFilterReq_t .
struct WfmHiSetBroadcastFilterReq_t
Request message for setting broadcast filter state.
struct WfmHiSetBroadcastFilterCnfBody_t
Confirmation message body for WfmHiSetBroadcastFilterCnf_t .
struct WfmHiSetBroadcastFilterCnf_t
Confirmation message for WfmHiSetBroadcastFilterReq_t .
struct WfmHiSetScanParametersReqBody_t
Request message body for WfmHiSetScanParametersReq_t .
struct WfmHiSetScanParametersReq_t
Request message for setting scan parameters.
struct WfmHiSetScanParametersCnfBody_t
Confirmation message body for WfmHiSetScanParametersCnf_t .
struct WfmHiSetScanParametersCnf_t
Confirmation message for WfmHiSetScanParametersReq_t .
struct WfmHiDisconnectReq_t
Request message for disconnecting from a Wi-Fi network.
struct WfmHiGetSignalStrengthReq_t
Request message for retrieving the signal strength of connection.
struct WfmHiStopApReq_t
Request message for stopping the started Wi-Fi network.
struct WfmHiStopApInd_t
Indication message used to signal the completion of a stop operation.
struct WfmHiStopScanReq_t
Request message for stopping an ongoing scan.
struct WfmHiLeaveIbssReq_t
Request message for disconnecting from an IBSS network.
struct WfmHiLeaveIbssInd_t
Indication message used to signal the completion of a disconnect operation.

Detailed Description

WFM API messages.


Data Structure Documentation

◆ WfmHiSetMacAddressReqBody_t

struct WfmHiSetMacAddressReqBody_t

Request message body for WfmHiSetMacAddressReq_t .

Definition at line 636 of file wfm_cmd_api.h .

Data Fields
uint8_t MacAddr[6] MAC address of the interface.
uint16_t Reserved Reserved, set to zero.

◆ WfmHiSetMacAddressReq_t

struct WfmHiSetMacAddressReq_t

Request message to set MAC address of the interface.

The host can use this request to set the MAC address an interface. If not set, the device will use a built-in MAC address. Note that if multiple interfaces are used, the MAC address MUST be different on each interface.

Definition at line 651 of file wfm_cmd_api.h .

Data Fields
WfmHiSetMacAddressReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetMacAddressCnfBody_t

struct WfmHiSetMacAddressCnfBody_t

Confirmation message body for WfmHiSetMacAddressCnf_t .

Definition at line 661 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetMacAddressCnf_t

struct WfmHiSetMacAddressCnf_t

Confirmation message for WfmHiSetMacAddressReq_t .

Definition at line 675 of file wfm_cmd_api.h .

Data Fields
WfmHiSetMacAddressCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiConnectReqBody_t

struct WfmHiConnectReqBody_t

Request message body for WfmHiConnectReq_t .

Definition at line 685 of file wfm_cmd_api.h .

Data Fields
uint8_t BSSID[6] Basic Service Set Identifier (BSSID) of the access point.

broadcast address : The device will connect to any matching access point.
unicast address : The device will only connect to the given access point.
See Basic Service Set Identifier for further details.

uint16_t Channel Channel of the access point.

0 : The device will connect to a matching access point on any channel.
1 - 13 : The device will only connect to a matching access point on the given channel.

uint16_t IeDataLength Length of vendor-specific Information Element (IE) data.

0 - 255 : The amount of bytes.

uint16_t MgmtFrameProtection Protected Management Frames (PMF) mode.

WFM_MGMT_FRAME_PROTECTION_DISABLED : The device will not use PMF even if supported by the access point.
WFM_MGMT_FRAME_PROTECTION_OPTIONAL : The device will use PMF if supported by the access point.
WFM_MGMT_FRAME_PROTECTION_MANDATORY : The device will only connect to an access point supporting PMF.
See WfmMgmtFrameProtection for enumeration values.

uint8_t Password[64] Password of the network.

64-bit WEP key : 5 bytes in ASCII format or 10 bytes in HEX format.
128-bit WEP key : 13 bytes in ASCII format or 26 bytes in HEX format.
WPA passphrase : 8 - 63 bytes in ASCII format.
WPA-PSK (hashed passphrase) : 64 bytes in HEX format.
See Passwords and passphrases for further details.

uint16_t PasswordLength Length of the network password.

0 - 64 : The amount of bytes.

uint8_t PreventRoaming Boolean option to prevent roaming between access points.

0 : The device may roam to any matching access point within the same network.
1 : The device will not roam to any other access point.

uint8_t SecurityMode Security mode of the network.

WFM_SECURITY_MODE_OPEN : The device will only connect to an unsecured access point.
WFM_SECURITY_MODE_WEP : The device will only connect to a WEP access point.
WFM_SECURITY_MODE_WPA2_WPA1_PSK : The device will only connect to a WPA-Personal or a WPA2-Personal access point.
WFM_SECURITY_MODE_WPA2_PSK : The device will only connect to a WPA2-Personal access point.
See WfmSecurityMode for enumeration values.

WfmHiSsidDef_t SsidDef Service Set Identifier (SSID) of the network.

◆ WfmHiConnectReq_t

struct WfmHiConnectReq_t

Request message for connecting to a Wi-Fi network.

The host can use this request to iniate a connection to a Wi-Fi network.

Successful connection request moves the interface to Wi-Fi client state .

Definition at line 760 of file wfm_cmd_api.h .

Data Fields
WfmHiConnectReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiConnectCnfBody_t

struct WfmHiConnectCnfBody_t

Confirmation message body for WfmHiConnectCnf_t .

Definition at line 770 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the connection request.

WFM_STATUS_SUCCESS : the connection request was accepted. It will be completed by WfmHiConnectInd_t .
any other value : the connection request failed.
See WfmStatus for enumeration values.

◆ WfmHiConnectCnf_t

struct WfmHiConnectCnf_t

Confirmation message for WfmHiConnectReq_t .

Definition at line 784 of file wfm_cmd_api.h .

Data Fields
WfmHiConnectCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiConnectIndBody_t

struct WfmHiConnectIndBody_t

Indication message body for WfmHiConnectInd_t .

Definition at line 794 of file wfm_cmd_api.h .

Data Fields
uint8_t BeaconInterval Beacon Interval of the connected access point.
uint16_t Channel Channel of the connected access point.

1 - 13 : Channel number.

uint8_t DtimPeriod DTIM period of the connected access point.

1 - 255 : DTIM period.

uint8_t Mac[6] MAC address of the connected access point.
uint16_t MaxPhyRate Maximum PHY data rate supported by the connection.

See WfmMaxPhyRate for enumeration values.

uint32_t Status Status of the connection request.

WFM_STATUS_SUCCESS : the connection request was completed successfully.
any other value : the connection request failed.
See WfmStatus for enumeration values.

◆ WfmHiConnectInd_t

struct WfmHiConnectInd_t

Indication message used to signal the completion of a connection operation.

The device will send this indication to signal the connection request initiated with WfmHiConnectReq_t has been completed. The indication is also sent when the device autonomously roams to another access point.

Definition at line 834 of file wfm_cmd_api.h .

Data Fields
WfmHiConnectIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiDisconnectCnfBody_t

struct WfmHiDisconnectCnfBody_t

Confirmation message body for WfmHiDisconnectCnf_t .

Definition at line 853 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the disconnection request.

WFM_STATUS_SUCCESS : the disconnection request was accepted. It will be completed by WfmHiDisconnectInd_t .
any other value : the disconnection request failed.
See WfmStatus for enumeration values.

◆ WfmHiDisconnectCnf_t

struct WfmHiDisconnectCnf_t

Confirmation message for WfmHiDisconnectReq_t .

Definition at line 867 of file wfm_cmd_api.h .

Data Fields
WfmHiDisconnectCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiDisconnectIndBody_t

struct WfmHiDisconnectIndBody_t

Indication message body for WfmHiDisconnectInd_t .

Definition at line 877 of file wfm_cmd_api.h .

Data Fields
uint8_t Mac[6] MAC address of the access point.
uint16_t Reason Reason for disconnection.

WFM_REASON_UNSPECIFIED : The device was disconnected or it disconnected on its own.
See WfmReason for enumeration values.

◆ WfmHiDisconnectInd_t

struct WfmHiDisconnectInd_t

Indication message used to signal the completion of a disconnection operation.

The device will send this indication to signal the disconnection request initiated with WfmHiDisconnectReq_t has been completed. The indication is also sent when the device has lost the connection to an access point and has been unable to regain it.

Definition at line 897 of file wfm_cmd_api.h .

Data Fields
WfmHiDisconnectIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiGetSignalStrengthCnfBody_t

struct WfmHiGetSignalStrengthCnfBody_t

Confirmation message body for WfmHiGetSignalStrengthCnf_t .

Definition at line 915 of file wfm_cmd_api.h .

Data Fields
uint32_t Rcpi Received Channel Power Indicator (RCPI) of the connection.

See Received Channel Power Indicator for further details.

uint32_t Status Status of the get request.

WFM_STATUS_SUCCESS : the get request was completed.
any other value : the get request failed.
See WfmStatus for enumeration values.

◆ WfmHiGetSignalStrengthCnf_t

struct WfmHiGetSignalStrengthCnf_t

Confirmation message for WfmHiGetSignalStrengthReq_t .

Definition at line 934 of file wfm_cmd_api.h .

Data Fields
WfmHiGetSignalStrengthCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetPmModeReqBody_t

struct WfmHiSetPmModeReqBody_t

Request message body for WfmHiSetPmModeReq_t .

Definition at line 944 of file wfm_cmd_api.h .

Data Fields
uint16_t ListenInterval Number of beacons/DTIMs to skip while sleeping.

0 : wake-up on every beacon/DTIM.
1 - 600: the number of beacon/DTIMs to skip.
See Power management for further details.

uint16_t PowerMode Power management mode.

WFM_PM_MODE_ACTIVE : the device will not use Wi-Fi power management mechanisms.
WFM_PM_MODE_BEACON : the device will wake-up on beacons.
WFM_PM_MODE_DTIM : the device will wake-up on DTIMs.
See WfmPmMode for enumeration values.

◆ WfmHiSetPmModeReq_t

struct WfmHiSetPmModeReq_t

Request message for setting the power management mode of the device.

The host can use this request to enable or disable Wi-Fi power management mechanisms.

Definition at line 967 of file wfm_cmd_api.h .

Data Fields
WfmHiSetPmModeReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetPmModeCnfBody_t

struct WfmHiSetPmModeCnfBody_t

Confirmation message body for WfmHiSetPmModeCnf_t .

Definition at line 977 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the power management request.

WFM_STATUS_SUCCESS : the power management request was completed.
any other value : the power management request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetPmModeCnf_t

struct WfmHiSetPmModeCnf_t

Confirmation message for WfmHiSetPmModeReq_t .

Definition at line 991 of file wfm_cmd_api.h .

Data Fields
WfmHiSetPmModeCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiStartApReqBody_t

struct WfmHiStartApReqBody_t

Request message body for WfmHiStartApReq_t .

Definition at line 1001 of file wfm_cmd_api.h .

Data Fields
uint16_t BeaconIeDataLength Length of vendor-specific Information Element (IE) data in 802.11 Beacon frames.

0 - 255 : The amount of bytes.

uint16_t Channel Channel of the access point.

1 - 13 : The device will create the access point on the given channel.

uint8_t ClientIsolation Boolean option to isolate connected clients from each other.

0 : The device will allow connected clients to communicate with each other.
1 : The device will prevent multiple connected clients from communicating.
Regardless of the value, the connected stations will always be able to communicate with the device.
See Client isolation for further details.

uint8_t HiddenSsid Boolean option to hide the network.

0 : The device will advertise the SSID of the network to any near-by stations.
1 : The device will hide the SSID of the network and will only respond to stations that specify the SSID.
See Hidden network for further details.

uint8_t MgmtFrameProtection Protected Management Frames (PMF) mode.

WFM_MGMT_FRAME_PROTECTION_DISABLED : The device will not use PMF even if supported by the connecting station.
WFM_MGMT_FRAME_PROTECTION_OPTIONAL : The device will use PMF if supported by the connecting station.
WFM_MGMT_FRAME_PROTECTION_MANDATORY : The device will only allow connecting stations that support PMF.
See WfmMgmtFrameProtection for enumeration values.

uint8_t Password[64] Password of the network.

64-bit WEP key : 5 bytes in ASCII format or 10 bytes in HEX format.
128-bit WEP key : 13 bytes in ASCII format or 26 bytes in HEX format.
WPA passphrase : 8 - 63 bytes in ASCII format.
WPA-PSK (hashed passphrase) : 64 bytes in HEX format.
See Passwords and passphrases for further details.

uint16_t PasswordLength Length of the network password.

0 - 64 : The amount of bytes.

uint16_t ProbeRespIeDataLength Length of vendor-specific Information Element (IE) data in 802.11 Probe Response frames.

0 - 255 : The amount of bytes.

uint8_t SecurityMode Security mode of the access point.

WFM_SECURITY_MODE_OPEN : The device will only allow unsecured connections.
WFM_SECURITY_MODE_WEP : The device will only allow WEP connections.
WFM_SECURITY_MODE_WPA2_WPA1_PSK : The device will only allow WPA-Personal and WPA2-Personal connections.
WFM_SECURITY_MODE_WPA2_PSK : The device will only allow WPA2-Personal connections.
See WfmSecurityMode for enumeration values.

WfmHiSsidDef_t SsidDef Service Set Identifier (SSID) of the network.

◆ WfmHiStartApReq_t

struct WfmHiStartApReq_t

Request message for starting a Wi-Fi network.

The host can use this request to iniate a Wi-Fi network.

Successful start request moves the interface to Wi-Fi access point state .

Definition at line 1090 of file wfm_cmd_api.h .

Data Fields
WfmHiStartApReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiStartApCnfBody_t

struct WfmHiStartApCnfBody_t

Confirmation message body for WfmHiStartApCnf_t .

Definition at line 1100 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the start request.

WFM_STATUS_SUCCESS : the start request was accepted. It will be completed by WfmHiStartApInd_t .
any other value : the start request failed.
See WfmStatus for enumeration values.

◆ WfmHiStartApCnf_t

struct WfmHiStartApCnf_t

Confirmation message for WfmHiStartApReq_t .

Definition at line 1114 of file wfm_cmd_api.h .

Data Fields
WfmHiStartApCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiStartApIndBody_t

struct WfmHiStartApIndBody_t

Indication message body for WfmHiStartApInd_t .

Definition at line 1124 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the start request.

WFM_STATUS_SUCCESS : the start request was completed successfully.
any other value : the start request failed.
See WfmStatus for enumeration values.

◆ WfmHiStartApInd_t

struct WfmHiStartApInd_t

Indication message used to signal the completion of a start request.

The device will send this indication to signal the start request initiated with WfmHiStartApReq_t has been completed.

Definition at line 1140 of file wfm_cmd_api.h .

Data Fields
WfmHiStartApIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiUpdateApReqBody_t

struct WfmHiUpdateApReqBody_t

Request message body for WfmHiUpdateApReq_t .

Definition at line 1150 of file wfm_cmd_api.h .

Data Fields
uint16_t BeaconIeDataLength Length of vendor-specific Information Element (IE) data in 802.11 Beacon frames.

0 - 255 : The amount of bytes.

uint16_t ProbeRespIeDataLength Length of vendor-specific Information Element (IE) data in 802.11 Probe Response frames.

0 - 255 : The amount of bytes.

◆ WfmHiUpdateApReq_t

struct WfmHiUpdateApReq_t

Request message for updating parameters of the started Wi-Fi network.

The host can use this request to update parameters of the started Wi-Fi network.

Definition at line 1182 of file wfm_cmd_api.h .

Data Fields
WfmHiUpdateApReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiUpdateApCnfBody_t

struct WfmHiUpdateApCnfBody_t

Confirmation message body for WfmHiUpdateApCnf_t .

Definition at line 1192 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the update request.

WFM_STATUS_SUCCESS : the update request was completed.
any other value : the update request failed.
See WfmStatus for enumeration values.

◆ WfmHiUpdateApCnf_t

struct WfmHiUpdateApCnf_t

Confirmation message for WfmHiUpdateApReq_t .

Definition at line 1206 of file wfm_cmd_api.h .

Data Fields
WfmHiUpdateApCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiStopApCnfBody_t

struct WfmHiStopApCnfBody_t

Confirmation message body for WfmHiStopApCnf_t .

Definition at line 1225 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the stop request.

WFM_STATUS_SUCCESS : the stop request was accepted. It will be completed by WfmHiStopApInd_t .
any other value : the stop request failed.
See WfmStatus for enumeration values.

◆ WfmHiStopApCnf_t

struct WfmHiStopApCnf_t

Confirmation message for WfmHiStopApReq_t .

Definition at line 1239 of file wfm_cmd_api.h .

Data Fields
WfmHiStopApCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiApClientConnectedIndBody_t

struct WfmHiApClientConnectedIndBody_t

Indication message body for WfmHiApClientConnectedInd_t .

Definition at line 1259 of file wfm_cmd_api.h .

Data Fields
uint8_t Mac[6] MAC address of the station.

◆ WfmHiApClientConnectedInd_t

struct WfmHiApClientConnectedInd_t

Indication message used to signal a connected station.

The device will send this indication to signal a station has connected to the started network.

Definition at line 1272 of file wfm_cmd_api.h .

Data Fields
WfmHiApClientConnectedIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiApClientRejectedIndBody_t

struct WfmHiApClientRejectedIndBody_t

Indication message body for WfmHiApClientRejectedInd_t .

Definition at line 1282 of file wfm_cmd_api.h .

Data Fields
uint8_t Mac[6] MAC address of the station.
uint16_t Reason Reason for rejection.

WFM_REASON_TIMEOUT : A timeout occurred during a station connection attempt.
WFM_REASON_UNKNOWN_STA : The device received data from a non-connected station.
WFM_REASON_AP_FULL : The device was not able to accommodate any more stations.
See WfmReason for enumeration values.

◆ WfmHiApClientRejectedInd_t

struct WfmHiApClientRejectedInd_t

Indication message used to signal a rejected connection attempt from a station.

The device will send this indication to signal a station has attempted connection to the started network and was rejected by the device.

Definition at line 1303 of file wfm_cmd_api.h .

Data Fields
WfmHiApClientRejectedIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiDisconnectApClientReqBody_t

struct WfmHiDisconnectApClientReqBody_t

Request message body for WfmHiDisconnectApClientReq_t .

Definition at line 1313 of file wfm_cmd_api.h .

Data Fields
uint8_t Mac[6] MAC address of the station.

◆ WfmHiDisconnectApClientReq_t

struct WfmHiDisconnectApClientReq_t

Request message for disconnecting a client from the started Wi-Fi network.

The host can use this request to disconnect a client from the started Wi-Fi network.

Definition at line 1325 of file wfm_cmd_api.h .

Data Fields
WfmHiDisconnectApClientReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiDisconnectApClientCnfBody_t

struct WfmHiDisconnectApClientCnfBody_t

Confirmation message body for WfmHiDisconnectApClientCnf_t .

Definition at line 1335 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the disconnect request.

WFM_STATUS_SUCCESS : the disconnect request was completed.
any other value : the disconnect request failed.
See WfmStatus for enumeration values.

◆ WfmHiDisconnectApClientCnf_t

struct WfmHiDisconnectApClientCnf_t

Confirmation message for WfmHiDisconnectApClientReq_t .

Definition at line 1349 of file wfm_cmd_api.h .

Data Fields
WfmHiDisconnectApClientCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiApClientDisconnectedIndBody_t

struct WfmHiApClientDisconnectedIndBody_t

Indication message body for WfmHiApClientDisconnectedInd_t .

Definition at line 1359 of file wfm_cmd_api.h .

Data Fields
uint8_t Mac[6] MAC address of the station.
uint16_t Reason Reason for disconnection.

WFM_REASON_LEAVING_BSS : The station was disconnected or it disconnected on its own.
See WfmReason for enumeration values.

◆ WfmHiApClientDisconnectedInd_t

struct WfmHiApClientDisconnectedInd_t

Indication message used to signal a disconnected station.

The device will send this indication to signal a station has left the started network.

Definition at line 1378 of file wfm_cmd_api.h .

Data Fields
WfmHiApClientDisconnectedIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSendFrameReqBody_t

struct WfmHiSendFrameReqBody_t

Request message body for WfmHiSendFrameReq_t .

Definition at line 1388 of file wfm_cmd_api.h .

Data Fields
uint8_t FrameType Type of the packet.

0 : Data packet with Ethernet II frame header.

uint32_t PacketDataLength Length of packet data.

1 - 1604 : The amount of bytes.

uint16_t PacketId Packet ID number.

0 - 65535 : Host-assigned unique number for the packet.
The number is returned in the corresponding confirmation message.

uint8_t Priority User Priority level.

0 - 7 : 802.1D Priority field value.

◆ WfmHiSendFrameReq_t

struct WfmHiSendFrameReq_t

Request message for sending a packet to the network.

The host can use this request to send a packet to the network.

Definition at line 1424 of file wfm_cmd_api.h .

Data Fields
WfmHiSendFrameReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSendFrameCnfBody_t

struct WfmHiSendFrameCnfBody_t

Confirmation message body for WfmHiSendFrameCnf_t .

Definition at line 1434 of file wfm_cmd_api.h .

Data Fields
uint16_t PacketId Packet ID number from the corresponding request.
uint16_t Reserved Reserved.
uint32_t Status Status of the send request.

WFM_STATUS_SUCCESS : the send request was completed.
any other value : the send request failed.
See WfmStatus for enumeration values.

◆ WfmHiSendFrameCnf_t

struct WfmHiSendFrameCnf_t

Confirmation message for WfmHiSendFrameReq_t .

Definition at line 1458 of file wfm_cmd_api.h .

Data Fields
WfmHiSendFrameCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiReceivedIndBody_t

struct WfmHiReceivedIndBody_t

Indication message body for WfmHiReceivedInd_t .

Definition at line 1468 of file wfm_cmd_api.h .

Data Fields
uint16_t FrameLength Length of packet data excluding the padding bytes.

1 - 2310 : The amount of bytes.

uint8_t FramePadding The amount of padding bytes before the packet data.

0 - 3 : The amount of bytes.

uint8_t FrameType Type of the packet.

0 : Data packet with Ethernet II frame header.

◆ WfmHiReceivedInd_t

struct WfmHiReceivedInd_t

Indication message used to signal a received packet.

The device will send this indication to signal a packet has been received.

Definition at line 1503 of file wfm_cmd_api.h .

Data Fields
WfmHiReceivedIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiStartScanReqBody_t

struct WfmHiStartScanReqBody_t

Request message body for WfmHiStartScanReq_t .

Definition at line 1513 of file wfm_cmd_api.h .

Data Fields
uint16_t ChannelListCount The amount of specific channels to scan.

0 : The device will scan all channels
1 - 13 : The amount of specific channels to scan.

uint16_t IeDataLength Length of vendor-specific Information Element (IE) data in 802.11 Probe Request frames.

0 - 255 : The amount of bytes.

uint16_t ScanMode Scan mode.

WFM_SCAN_MODE_PASSIVE : The device will perform a passive scan.
WFM_SCAN_MODE_ACTIVE : The device will perform an active scan.
See WfmScanMode for enumeration values.
See Scanning for further details.

uint16_t SsidListCount The amount of specific SSIDs to scan.

0 : The device will perform a broadcast scan
1 - 2 : The amount of specific SSIDs to scan.

◆ WfmHiStartScanReq_t

struct WfmHiStartScanReq_t

Request message for starting a scan to detect near-by access points.

The host can use this request to start a scan operation to detect near-by access points.

Definition at line 1567 of file wfm_cmd_api.h .

Data Fields
WfmHiStartScanReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiStartScanCnfBody_t

struct WfmHiStartScanCnfBody_t

Confirmation message body for WfmHiStartScanCnf_t .

Definition at line 1577 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the scan request.

WFM_STATUS_SUCCESS : the scan request was accepted. It will be completed by WfmHiScanCompleteInd_t .
any other value : the scan request failed.
See WfmStatus for enumeration values.

◆ WfmHiStartScanCnf_t

struct WfmHiStartScanCnf_t

Confirmation message for WfmHiStartScanReq_t .

Definition at line 1592 of file wfm_cmd_api.h .

Data Fields
WfmHiStartScanCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiStopScanCnfBody_t

struct WfmHiStopScanCnfBody_t

Confirmation message body for WfmHiStopScanCnf_t .

Definition at line 1611 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the stop request.

WFM_STATUS_SUCCESS : the stop request was accepted. It will be completed by WfmHiScanResultInd_t .
any other value : the stop request failed.
See WfmStatus for enumeration values.

◆ WfmHiStopScanCnf_t

struct WfmHiStopScanCnf_t

Confirmation message for WfmHiStopScanReq_t .

Definition at line 1626 of file wfm_cmd_api.h .

Data Fields
WfmHiStopScanCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiScanResultIndBody_t

struct WfmHiScanResultIndBody_t

Indication message body for WfmHiScanResultInd_t .

Definition at line 1636 of file wfm_cmd_api.h .

Data Fields
uint16_t Channel Channel of the access point.

1 - 13 : Channel number.

uint16_t IeDataLength Length of access point Information Element (IE) data in bytes.
uint8_t Mac[6] MAC address of the access point.
uint16_t Rcpi Received Channel Power Indicator (RCPI) of the access point.

See Received Channel Power Indicator for further details.

uint32_t Reserved Reserved.
WfmHiSsidDef_t SsidDef Service Set Identifier (SSID) of the network.

◆ WfmHiScanResultInd_t

struct WfmHiScanResultInd_t

Indication message used to signal an access point has been detected.

The device will send this indication to signal an access point has has been detected during the scan operation.

Definition at line 1676 of file wfm_cmd_api.h .

Data Fields
WfmHiScanResultIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiScanCompleteIndBody_t

struct WfmHiScanCompleteIndBody_t

Indication message body for WfmHiScanCompleteInd_t .

Definition at line 1686 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the scan request.

WFM_STATUS_SUCCESS : the scan request was completed.
any other value : the scan request failed.
See WfmStatus for enumeration values.

◆ WfmHiScanCompleteInd_t

struct WfmHiScanCompleteInd_t

Indication message used to signal a scan was completed.

The device will send this indication to signal a scan operation has been completed.

Definition at line 1703 of file wfm_cmd_api.h .

Data Fields
WfmHiScanCompleteIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiJoinIbssReqBody_t

struct WfmHiJoinIbssReqBody_t

Request message body for WfmHiJoinIbssReq_t .

Definition at line 1713 of file wfm_cmd_api.h .

Data Fields
uint32_t Channel Channel of the network.

0 : The device will connect to a matching network on any channel.
1 - 13 : The device will only connect to a matching network on the given channel.

uint8_t Password[64] Password of the network.

64-bit WEP key : 5 bytes in ASCII format or 10 bytes in HEX format.
128-bit WEP key : 13 bytes in ASCII format or 26 bytes in HEX format.
See Passwords and passphrases for further details.

uint16_t PasswordLength Length of the network password.

0 - 26 : The amount of bytes.

uint16_t SecurityMode Security mode of the network.

WFM_SECURITY_MODE_OPEN : The device will only use unsecured connections.
WFM_SECURITY_MODE_WEP : The device will only use WEP connections.
See WfmSecurityMode for enumeration values.

WfmHiSsidDef_t SsidDef Service Set Identifier (SSID) of the network.

◆ WfmHiJoinIbssReq_t

struct WfmHiJoinIbssReq_t

Request message for connecting to or starting an IBSS network.

The host can use this request to connect to an IBSS network. If no existing network is found, the device will start a new network.

Successful join request moves the interface to IBSS station state .

Definition at line 1752 of file wfm_cmd_api.h .

Data Fields
WfmHiJoinIbssReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiJoinIbssCnfBody_t

struct WfmHiJoinIbssCnfBody_t

Confirmation message body for WfmHiJoinIbssCnf_t .

Definition at line 1762 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the join request.

WFM_STATUS_SUCCESS : the join request was accepted. It will be completed by WfmHiJoinIbssInd_t .
any other value : the join request failed.
See WfmStatus for enumeration values.

◆ WfmHiJoinIbssCnf_t

struct WfmHiJoinIbssCnf_t

Confirmation message for WfmHiJoinIbssReq_t .

Definition at line 1776 of file wfm_cmd_api.h .

Data Fields
WfmHiJoinIbssCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiJoinIbssIndBody_t

struct WfmHiJoinIbssIndBody_t

Indication message body for WfmHiJoinIbssInd_t .

Definition at line 1786 of file wfm_cmd_api.h .

Data Fields
uint8_t Bssid[6] Basic Service Set Identifier (BSSID) of the network.


See Basic Service Set Identifier for further details.

uint16_t Reserved Reserved.
uint32_t Status Status of the join request.

WFM_STATUS_SUCCESS : the join request was completed successfully.
any other value : the join request failed.
See WfmStatus for enumeration values.

◆ WfmHiJoinIbssInd_t

struct WfmHiJoinIbssInd_t

Indication message used to signal the completion of a join request.

The device will send this indication to signal the join request initiated with WfmHiJoinIbssReq_t has been completed.

Definition at line 1811 of file wfm_cmd_api.h .

Data Fields
WfmHiJoinIbssIndBody_t Body Indication message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiLeaveIbssCnfBody_t

struct WfmHiLeaveIbssCnfBody_t

Confirmation message body for WfmHiLeaveIbssCnf_t .

Definition at line 1830 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the disconnect request.

WFM_STATUS_SUCCESS : the disconnect request was accepted. It will be completed by WfmHiLeaveIbssInd_t .
any other value : the disconnect request failed.
See WfmStatus for enumeration values.

◆ WfmHiLeaveIbssCnf_t

struct WfmHiLeaveIbssCnf_t

Confirmation message for WfmHiLeaveIbssReq_t .

Definition at line 1844 of file wfm_cmd_api.h .

Data Fields
WfmHiLeaveIbssCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiAddMulticastAddrReqBody_t

struct WfmHiAddMulticastAddrReqBody_t

Request message body for WfmHiAddMulticastAddrReq_t .

Definition at line 1864 of file wfm_cmd_api.h .

Data Fields
uint8_t Mac[6] MAC address to add.

broadcast address : The device will empty the whitelist and allow all multicast addresses.
zero address : The device will empty the whitelist and deny all multicast addresses.
unicast address : The device will add the given address to the whitelist.
See Basic Service Set Identifier for further details.

◆ WfmHiAddMulticastAddrReq_t

struct WfmHiAddMulticastAddrReq_t

Request message for adding a multicast address to the multicast filter whitelist.

The host can use this request to add a multicast address to the multicast filter whitelist. When the first address is added the whitelist, the device will discard all multicast frames whose destination address does not match any of the addresses on the list. The default state is to allow all multicast addresses.
See Filtering for further details.

Definition at line 1885 of file wfm_cmd_api.h .

Data Fields
WfmHiAddMulticastAddrReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiAddMulticastAddrCnfBody_t

struct WfmHiAddMulticastAddrCnfBody_t

Confirmation message body for WfmHiAddMulticastAddrCnf_t .

Definition at line 1895 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the add request.

WFM_STATUS_SUCCESS : the add request was completed successfully.
any other value : the add request failed.
See WfmStatus for enumeration values.

◆ WfmHiAddMulticastAddrCnf_t

struct WfmHiAddMulticastAddrCnf_t

Confirmation message for WfmHiAddMulticastAddrReq_t .

Definition at line 1910 of file wfm_cmd_api.h .

Data Fields
WfmHiAddMulticastAddrCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiRemoveMulticastAddrReqBody_t

struct WfmHiRemoveMulticastAddrReqBody_t

Request message body for WfmHiRemoveMulticastAddrReq_t .

Definition at line 1920 of file wfm_cmd_api.h .

Data Fields
uint8_t Mac[6] MAC address to remove.

unicast address : The device will remove the given address from the whitelist.
See Basic Service Set Identifier for further details.

◆ WfmHiRemoveMulticastAddrReq_t

struct WfmHiRemoveMulticastAddrReq_t

Request message for removing a multicast address from the multicast filter whitelist.

The host can use this request to remove a multicast address from the multicast filter whitelist.

Definition at line 1936 of file wfm_cmd_api.h .

Data Fields
WfmHiRemoveMulticastAddrReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiRemoveMulticastAddrCnfBody_t

struct WfmHiRemoveMulticastAddrCnfBody_t

Confirmation message body for WfmHiRemoveMulticastAddrCnf_t .

Definition at line 1946 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the remove request.

WFM_STATUS_SUCCESS : the remove request was completed successfully.
any other value : the remove request failed.
See WfmStatus for enumeration values.

◆ WfmHiRemoveMulticastAddrCnf_t

struct WfmHiRemoveMulticastAddrCnf_t

Confirmation message for WfmHiRemoveMulticastAddrReq_t .

Definition at line 1961 of file wfm_cmd_api.h .

Data Fields
WfmHiRemoveMulticastAddrCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetMaxApClientCountReqBody_t

struct WfmHiSetMaxApClientCountReqBody_t

Request message body for WfmHiSetMaxApClientCountReq_t .

Definition at line 1971 of file wfm_cmd_api.h .

Data Fields
uint32_t Count Maximum number of connected clients.

0 : The device will set the limit value to the firmware default.
1 - 8 : The maximum number of connected clients.

◆ WfmHiSetMaxApClientCountReq_t

struct WfmHiSetMaxApClientCountReq_t

Request message for setting the maximum number of connected clients.

The host can use this request to limit the number of stations that can connect the started Wi-Fi network.

Definition at line 1986 of file wfm_cmd_api.h .

Data Fields
WfmHiSetMaxApClientCountReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetMaxApClientCountCnfBody_t

struct WfmHiSetMaxApClientCountCnfBody_t

Confirmation message body for WfmHiSetMaxApClientCountCnf_t .

Definition at line 1996 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetMaxApClientCountCnf_t

struct WfmHiSetMaxApClientCountCnf_t

Confirmation message for WfmHiSetMaxApClientCountReq_t .

Definition at line 2010 of file wfm_cmd_api.h .

Data Fields
WfmHiSetMaxApClientCountCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetMaxApClientInactivityReqBody_t

struct WfmHiSetMaxApClientInactivityReqBody_t

Request message body for WfmHiSetMaxApClientInactivityReq_t .

Definition at line 2020 of file wfm_cmd_api.h .

Data Fields
uint32_t InactivityTimeout Maximum amount of client idle time.

0 : The device will set the limit value to the firmware default.
1 - 240 : The maximum number of seconds.

◆ WfmHiSetMaxApClientInactivityReq_t

struct WfmHiSetMaxApClientInactivityReq_t

Request message for setting the maximum number of connected clients.

The host can use this request to limit the number of stations that can connect the started Wi-Fi network.

Definition at line 2035 of file wfm_cmd_api.h .

Data Fields
WfmHiSetMaxApClientInactivityReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetMaxApClientInactivityCnfBody_t

struct WfmHiSetMaxApClientInactivityCnfBody_t

Confirmation message body for WfmHiSetMaxApClientCountCnf_t .

Definition at line 2045 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetMaxApClientInactivityCnf_t

struct WfmHiSetMaxApClientInactivityCnf_t

Confirmation message for WfmHiSetMaxApClientInactivityReq_t .

Definition at line 2059 of file wfm_cmd_api.h .

Data Fields
WfmHiSetMaxApClientInactivityCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetRoamParametersReqBody_t

struct WfmHiSetRoamParametersReqBody_t

Request message body for WfmHiSetRoamParametersReq_t .

Definition at line 2069 of file wfm_cmd_api.h .

Data Fields
uint8_t BeaconLostCount Beacon loss limit for a roaming attempt.

0 : The device will set the limit value to the firmware default.
1 - 255: Beacon loss limit for a roaming attempt.

uint8_t ChannelListCount The amount of specific channels to scan.

0 : The device will scan all channels.
1 - 13 : The amount of specific channels to scan.

uint8_t RcpiHysteresis Upper RCPI limit that must be attained before triggering roaming again.

0 : The device will set the limit value to the firmware default.
1 - 220: RCPI limit to re-enable automatic roaming based on RCPI. This value is used to prevent automatic roaming from triggering again and again while the signal strength stays close to the RcpiThreshold value. RcpiHysteresis should be set to a value grater than RcpiThreshold.
See Received Channel Power Indicator for further details.

uint8_t RcpiThreshold Received Channel Power Indicator (RCPI) limit for a roaming attempt.

0 : The device will set the limit value to the firmware default.
1 - 220: RCPI limit for a roaming attempt.
See Received Channel Power Indicator for further details.

◆ WfmHiSetRoamParametersReq_t

struct WfmHiSetRoamParametersReq_t

Request message for setting the roaming parameters.

The host can use this request to configure the roaming parameters of the device.
See Roaming for further details.

Definition at line 2116 of file wfm_cmd_api.h .

Data Fields
WfmHiSetRoamParametersReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetRoamParametersCnfBody_t

struct WfmHiSetRoamParametersCnfBody_t

Confirmation message body for WfmHiSetRoamParametersCnf_t .

Definition at line 2126 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetRoamParametersCnf_t

struct WfmHiSetRoamParametersCnf_t

Confirmation message for WfmHiSetRoamParametersReq_t .

Definition at line 2141 of file wfm_cmd_api.h .

Data Fields
WfmHiSetRoamParametersCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetTxRateParametersReqBody_t

struct WfmHiSetTxRateParametersReqBody_t

Request message body for WfmHiSetTxRateParametersReq_t .

Definition at line 2151 of file wfm_cmd_api.h .

Data Fields
WfmHiRateSetBitmask_t RateSetBitmask TX rate set parameters.
uint32_t Reserved Reserved, set to zero.

◆ WfmHiSetTxRateParametersReq_t

struct WfmHiSetTxRateParametersReq_t

Request message for setting the TX rate set parameters.

The host can use this request to configure the TX rate set parameters of the device. The rate set determines what data rates will be used by the device to transmit data frames.

Definition at line 2171 of file wfm_cmd_api.h .

Data Fields
WfmHiSetTxRateParametersReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetTxRateParametersCnfBody_t

struct WfmHiSetTxRateParametersCnfBody_t

Confirmation message body for WfmHiSetTxRateParametersCnf_t .

Definition at line 2181 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetTxRateParametersCnf_t

struct WfmHiSetTxRateParametersCnf_t

Confirmation message for WfmHiSetTxRateParametersReq_t .

Definition at line 2196 of file wfm_cmd_api.h .

Data Fields
WfmHiSetTxRateParametersCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetArpIpAddressReqBody_t

struct WfmHiSetArpIpAddressReqBody_t

Request message body for WfmHiSetArpIpAddressReq_t .

Definition at line 2206 of file wfm_cmd_api.h .

Data Fields
uint32_t ArpIpAddr[2] List of offloaded ARP IP addresses.

The device will automatically reply to an ARP request that matches one the addresses on the list. Note that addresses not in use must be set to zero. Offloading is disabled by setting all addresses to zero.
See Offloading for further details.

◆ WfmHiSetArpIpAddressReq_t

struct WfmHiSetArpIpAddressReq_t

Request message for setting the Address Resolution Protocol (ARP) offloading state.

The host can use this request to offload handling of ARP requests to the device. When offloading is enabled, the device will automatically respond to ARP requests with an ARP reply.
See Offloading for further details.

Definition at line 2226 of file wfm_cmd_api.h .

Data Fields
WfmHiSetArpIpAddressReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetArpIpAddressCnfBody_t

struct WfmHiSetArpIpAddressCnfBody_t

Confirmation message body for WfmHiSetArpIpAddressCnf_t .

Definition at line 2236 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetArpIpAddressCnf_t

struct WfmHiSetArpIpAddressCnf_t

Confirmation message for WfmHiSetArpIpAddressReq_t .

Definition at line 2250 of file wfm_cmd_api.h .

Data Fields
WfmHiSetArpIpAddressCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetNsIpAddressReqBody_t

struct WfmHiSetNsIpAddressReqBody_t

Request message body for WfmHiSetNsIpAddressReq_t .

Definition at line 2260 of file wfm_cmd_api.h .

Data Fields
WfmHiNsIpAddr_t NsIpAddr[2] List of offloaded NS IP addresses.

The device will automatically reply to a NS that matches one the addresses on the list. Note that addresses not in use must be set to zero. Offloading is disabled by setting all addresses to zero.
See Offloading for further details.

◆ WfmHiSetNsIpAddressReq_t

struct WfmHiSetNsIpAddressReq_t

Request message for setting the Neighbor Discovery Protocol (NDP) offloading state.

The host can use this request to offload handling of IPv6 Neighbor Solicitations to the device. When offloading is enabled, the device will automatically respond to a solicitation with a Neighbor Advertisement.
See Offloading for further details.

Definition at line 2279 of file wfm_cmd_api.h .

Data Fields
WfmHiSetNsIpAddressReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetNsIpAddressCnfBody_t

struct WfmHiSetNsIpAddressCnfBody_t

Confirmation message body for WfmHiSetNsIpAddressCnf_t .

Definition at line 2289 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetNsIpAddressCnf_t

struct WfmHiSetNsIpAddressCnf_t

Confirmation message for WfmHiSetNsIpAddressReq_t .

Definition at line 2303 of file wfm_cmd_api.h .

Data Fields
WfmHiSetNsIpAddressCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetBroadcastFilterReqBody_t

struct WfmHiSetBroadcastFilterReqBody_t

Request message body for WfmHiSetBroadcastFilterReq_t .

Definition at line 2313 of file wfm_cmd_api.h .

Data Fields
uint32_t Filter Boolean option for broadcast filtering.

0 : The device will forward all received broadcast frames to the host.
1 : The device will only forward ARP and DHCP frames to the host, other broadcast frames are discarded.
See Filtering for further details.

◆ WfmHiSetBroadcastFilterReq_t

struct WfmHiSetBroadcastFilterReq_t

Request message for setting broadcast filter state.

The host can use this request to configure the state of the broadcast filter. When enabled, the device will only forward certain broadcast frames to the host and automatically discard the rest. The default state is to allow all broadcast traffic.
See Filtering for further details.

Definition at line 2333 of file wfm_cmd_api.h .

Data Fields
WfmHiSetBroadcastFilterReqBody_t Body Request message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetBroadcastFilterCnfBody_t

struct WfmHiSetBroadcastFilterCnfBody_t

Confirmation message body for WfmHiSetBroadcastFilterCnf_t .

Definition at line 2343 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetBroadcastFilterCnf_t

struct WfmHiSetBroadcastFilterCnf_t

Confirmation message for WfmHiSetBroadcastFilterReq_t .

Definition at line 2357 of file wfm_cmd_api.h .

Data Fields
WfmHiSetBroadcastFilterCnfBody_t Body Confirmation message body.
HiMsgHdr_t Header Common message header.

◆ WfmHiSetScanParametersReqBody_t

struct WfmHiSetScanParametersReqBody_t

Request message body for WfmHiSetScanParametersReq_t .

Definition at line 2367 of file wfm_cmd_api.h .

Data Fields
uint16_t ActiveChannelTime Set to 0 for FW default, 1 - 550 TUs.
uint16_t NumOfProbeRequests Set to 0 for FW default, 1 - 2.
uint16_t PassiveChannelTime Set to 0 for FW default, 1 - 550 TUs.
uint16_t Reserved Reserved, set to zero.

◆ WfmHiSetScanParametersReq_t

struct WfmHiSetScanParametersReq_t

Request message for setting scan parameters.

The host can use this request to configure scans.

Definition at line 2391 of file wfm_cmd_api.h .

◆ WfmHiSetScanParametersCnfBody_t

struct WfmHiSetScanParametersCnfBody_t

Confirmation message body for WfmHiSetScanParametersCnf_t .

Definition at line 2399 of file wfm_cmd_api.h .

Data Fields
uint32_t Status Status of the set request.

WFM_STATUS_SUCCESS : the set request was completed successfully.
any other value : the set request failed.
See WfmStatus for enumeration values.

◆ WfmHiSetScanParametersCnf_t

struct WfmHiSetScanParametersCnf_t

Confirmation message for WfmHiSetScanParametersReq_t .

Definition at line 2413 of file wfm_cmd_api.h .

◆ WfmHiDisconnectReq_t

struct WfmHiDisconnectReq_t

Request message for disconnecting from a Wi-Fi network.

The host can use this request to iniate a disconnection from a Wi-Fi network.

Successful disconnection request moves the interface to Idle state .

◆ WfmHiGetSignalStrengthReq_t

struct WfmHiGetSignalStrengthReq_t

Request message for retrieving the signal strength of connection.

The host can use this request to retrieve the signal strength of the connection.

◆ WfmHiStopApReq_t

struct WfmHiStopApReq_t

Request message for stopping the started Wi-Fi network.

The host can use this request to stop the started Wi-Fi network.

Successful stop request moves the interface to Idle state .

◆ WfmHiStopApInd_t

struct WfmHiStopApInd_t

Indication message used to signal the completion of a stop operation.

The device will send this indication to signal the stop request initiated with WfmHiStopApReq_t has been completed. The indication is also sent when the started network has encountered a fatal error.

◆ WfmHiStopScanReq_t

struct WfmHiStopScanReq_t

Request message for stopping an ongoing scan.

The host can use this request to stop an ongoing scan operation.

◆ WfmHiLeaveIbssReq_t

struct WfmHiLeaveIbssReq_t

Request message for disconnecting from an IBSS network.

The host can use this request to disconnect from an IBSS network.

Successful disconnect request moves the interface to Idle state .

◆ WfmHiLeaveIbssInd_t

struct WfmHiLeaveIbssInd_t

Indication message used to signal the completion of a disconnect operation.

The device will send this indication to signal the disconnect request initiated with WfmHiLeaveIbssReq_t has been completed. The indication is also sent when the network has encountered a fatal error.