GENERAL_DRIVER_API

Functions

sl_status_t wf200_send_configuration (const char *pds_data, uint32_t pds_data_length)
Function to send PDS chunks.
sl_status_t wf200_shutdown (void)
Shutdown wf200.

Function Documentation

◆ wf200_send_configuration()

sl_status_t wf200_send_configuration ( const char * pds_data,
uint32_t pds_data_length
)

Function to send PDS chunks.

Note
The PDS file contains the WF200 settings (refer to wf200_pds.h )
Parameters
pds_data Data to be sent in the compressed PDS format
pds_data_length Size of the data to be sent
Returns
SL_SUCCESS if the configuration has been sent correctly, SL_ERROR otherwise

Definition at line 620 of file wf200.c .

◆ wf200_shutdown()

sl_status_t wf200_shutdown ( void )

Shutdown wf200.

Note
Send the shutdown command and clear GPIO WUP to enable wf200 to go to sleep
Returns
SL_SUCCESS if the wf200 has been shutdown correctly, SL_ERROR otherwise

Definition at line 664 of file wf200.c .