FULL_MAC_DRIVER_API

Functions

sl_status_t sl_wfx_set_mac_address (const sl_wfx_mac_address_t *mac, sl_wfx_interface_t interface)
Brief Set the MAC address used by Wi-Fi chip.
sl_status_t sl_wfx_send_join_command (const uint8_t *ssid, uint32_t ssid_length, const sl_wfx_mac_address_t *bssid, uint16_t channel, sl_wfx_security_mode_t security_mode, uint8_t prevent_roaming, uint16_t management_frame_protection, const uint8_t *passkey, uint16_t passkey_length, const uint8_t *ie_data, uint16_t ie_data_length)
As a station, send a command to join a Wi-Fi network.
sl_status_t sl_wfx_send_disconnect_command (void)
Connected as a station, send a disconnection request to the AP.
sl_status_t sl_wfx_start_ap_command (uint16_t channel, uint8_t *ssid, uint32_t ssid_length, uint8_t hidden_ssid, uint8_t client_isolation, sl_wfx_security_mode_t security_mode, uint8_t management_frame_protection, const uint8_t *passkey, uint16_t passkey_length, const uint8_t *beacon_ie_data, uint16_t beacon_ie_data_length, const uint8_t *probe_response_ie_data, uint16_t probe_response_ie_data_length)
Send a command to start the softap mode.
sl_status_t sl_wfx_update_ap_command (uint16_t beacon_ie_data_length, uint16_t probe_response_ie_data_length, uint32_t *beacon_ie_data, uint32_t *probe_response_ie_data)
Update the softap settings.
sl_status_t sl_wfx_stop_ap_command (void)
Send a command to stop the softap mode.
sl_status_t sl_wfx_send_ethernet_frame ( sl_wfx_send_frame_req_t *frame, uint32_t data_length, sl_wfx_interface_t interface, uint8_t priority)
Send an Ethernet frame.
sl_status_t sl_wfx_send_scan_command (uint16_t scan_mode, const uint8_t *channel_list, uint16_t channel_list_count, const sl_wfx_ssid_def_t *ssid_list, uint16_t ssid_list_count, const uint8_t *ie_data, uint16_t ie_data_length, const uint8_t *bssid)
Send a scan command.
sl_status_t sl_wfx_send_stop_scan_command (void)
Stop an ongoing scan process.
sl_status_t sl_wfx_get_signal_strength (uint32_t *signal_strength)
Get the signal strength of the last packets received.
sl_status_t sl_wfx_disconnect_ap_client_command (const sl_wfx_mac_address_t *client)
In AP mode, disconnect the specified client.
sl_status_t sl_wfx_set_power_mode ( sl_wfx_pm_mode_t mode, sl_wfx_pm_poll_t strategy, uint16_t interval)
Set the power mode used as a station.
sl_status_t sl_wfx_add_multicast_address (const sl_wfx_mac_address_t *mac_address, sl_wfx_interface_t interface)
Add a multicast address to the multicast filter whitelist.
sl_status_t sl_wfx_remove_multicast_address (const sl_wfx_mac_address_t *mac_address, sl_wfx_interface_t interface)
Remove a multicast address from the multicast filter whitelist.
sl_status_t sl_wfx_set_arp_ip_address (uint32_t *arp_ip_addr, uint8_t num_arp_ip_addr)
Set the ARP offloading state.
sl_status_t sl_wfx_set_ns_ip_address (uint8_t *ns_ip_addr, uint8_t num_ns_ip_addr)
Set the NS offloading state.
sl_status_t sl_wfx_set_broadcast_filter (uint32_t filter)
Set the broadcast filter state.
sl_status_t sl_wfx_set_unicast_filter (uint32_t filter)
Set the unicast filter state.
sl_status_t sl_wfx_add_whitelist_address (const sl_wfx_mac_address_t *mac_address)
Add a mac address to the device whitelist.
sl_status_t sl_wfx_add_blacklist_address (const sl_wfx_mac_address_t *mac_address)
Add a mac address to the device blacklist.
sl_status_t sl_wfx_set_max_ap_client (uint32_t max_clients)
Configure the maximum number of clients supported in softap mode.
sl_status_t sl_wfx_set_max_ap_client_inactivity (uint32_t inactivity_timeout)
Configure the maximum client idle time.
sl_status_t sl_wfx_set_scan_parameters (uint16_t active_channel_time, uint16_t passive_channel_time, uint16_t num_probe_requests)
Configure scan parameters.
sl_status_t sl_wfx_set_roam_parameters (uint8_t rcpi_threshold, uint8_t rcpi_hysteresis, uint8_t beacon_lost_count, const uint8_t *channel_list, uint8_t channel_list_count)
Configure the roaming behavior in station mode.
sl_status_t sl_wfx_set_tx_rate_parameters ( sl_wfx_rate_set_bitmask_t rate_set_bitmask, uint8_t use_minstrel)
Set the rate mode allowed by the station once connected.
sl_status_t sl_wfx_set_max_tx_power (int32_t max_tx_power, sl_wfx_interface_t interface)
Set maximum transmit power.
sl_status_t sl_wfx_get_max_tx_power (int32_t *max_tx_power_rf_port_1, int32_t *max_tx_power_rf_port_2, sl_wfx_interface_t interface)
Set maximum transmit power.
sl_status_t sl_wfx_get_pmk ( sl_wfx_password_t *password, uint32_t *password_length, sl_wfx_interface_t interface)
Get the PMK used to connect to the current secure network.
sl_status_t sl_wfx_get_ap_client_signal_strength (const sl_wfx_mac_address_t *client, uint32_t *signal_strength)
Get the signal strength of the last packets received from an AP client.
sl_status_t sl_wfx_ext_auth ( sl_wfx_ext_auth_data_type_t auth_data_type, uint16_t auth_data_length, const uint8_t *auth_data)
Send a WPA3 Auth packet.

Function Documentation

◆ sl_wfx_add_blacklist_address()

sl_status_t sl_wfx_add_blacklist_address ( const sl_wfx_mac_address_t * mac_address )

Add a mac address to the device blacklist.

Parameters
mac_address is the MAC address to add. Broadcast address denies all MAC addresses.
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 905 of file sl_wfx.c .

References sl_wfx_add_blacklist_addr_req_body_t::mac , sl_wfx_mac_address_t::octet , SL_WFX_ADD_BLACKLIST_ADDR_REQ_ID , sl_wfx_send_command() , and SL_WFX_SOFTAP_INTERFACE .

◆ sl_wfx_add_multicast_address()

sl_status_t sl_wfx_add_multicast_address ( const sl_wfx_mac_address_t * mac_address,
sl_wfx_interface_t interface
)

Add a multicast address to the multicast filter whitelist.

Parameters
mac_address is the MAC address to add
interface is the interface where to apply the change
  • SL_WFX_STA_INTERFACE
  • SL_WFX_SOFTAP_INTERFACE
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 783 of file sl_wfx.c .

References sl_wfx_add_multicast_addr_req_body_t::mac , sl_wfx_mac_address_t::octet , SL_WFX_ADD_MULTICAST_ADDR_REQ_ID , and sl_wfx_send_command() .

◆ sl_wfx_add_whitelist_address()

sl_status_t sl_wfx_add_whitelist_address ( const sl_wfx_mac_address_t * mac_address )

Add a mac address to the device whitelist.

Parameters
mac_address is the MAC address to add. Broadcast address allows all MAC addresses.
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 889 of file sl_wfx.c .

References sl_wfx_add_whitelist_addr_req_body_t::mac , sl_wfx_mac_address_t::octet , SL_WFX_ADD_WHITELIST_ADDR_REQ_ID , sl_wfx_send_command() , and SL_WFX_SOFTAP_INTERFACE .

◆ sl_wfx_disconnect_ap_client_command()

sl_status_t sl_wfx_disconnect_ap_client_command ( const sl_wfx_mac_address_t * client )

In AP mode, disconnect the specified client.

Parameters
client is the mac address of the client to disconnect
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 739 of file sl_wfx.c .

References sl_wfx_disconnect_ap_client_req_body_t::mac , sl_wfx_mac_address_t::octet , SL_WFX_DISCONNECT_AP_CLIENT_REQ_ID , sl_wfx_send_command() , and SL_WFX_SOFTAP_INTERFACE .

◆ sl_wfx_ext_auth()

sl_status_t sl_wfx_ext_auth ( sl_wfx_ext_auth_data_type_t auth_data_type,
uint16_t auth_data_length,
const uint8_t * auth_data
)

Send a WPA3 Auth packet.

Parameters
auth_data_type is the type of the packet to send.
  • WFM_EXT_AUTH_DATA_TYPE_SAE_START
  • WFM_EXT_AUTH_DATA_TYPE_SAE_COMMIT
  • WFM_EXT_AUTH_DATA_TYPE_SAE_CONFIRM
  • WFM_EXT_AUTH_DATA_TYPE_MSK
auth_data_length is the length of the data to be sent.
auth_data is the data.
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 1196 of file sl_wfx.c .

References sl_wfx_allocate_command_buffer() , and SL_WFX_EXT_AUTH_REQ_ID .

◆ sl_wfx_get_ap_client_signal_strength()

sl_status_t sl_wfx_get_ap_client_signal_strength ( const sl_wfx_mac_address_t * client,
uint32_t * signal_strength
)

Get the signal strength of the last packets received from an AP client.

Parameters
client is the mac address of the client
signal_strength returns the RCPI value averaged on the last packets received. RCPI ranges from 0 - 220 with 220 corresponds to 0 dBm and each increment represents an increase of 0.5 dBm.
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 1159 of file sl_wfx.c .

References sl_wfx_get_ap_client_signal_strength_cnf_t::body , sl_wfx_get_ap_client_signal_strength_req_body_t::mac , sl_wfx_mac_address_t::octet , sl_wfx_get_ap_client_signal_strength_cnf_body_t::rcpi , SL_WFX_GET_AP_CLIENT_SIGNAL_STRENGTH_REQ_ID , sl_wfx_get_status_code() , sl_wfx_send_command() , SL_WFX_SOFTAP_INTERFACE , and sl_wfx_get_ap_client_signal_strength_cnf_body_t::status .

◆ sl_wfx_get_max_tx_power()

sl_status_t sl_wfx_get_max_tx_power ( int32_t * max_tx_power_rf_port_1,
int32_t * max_tx_power_rf_port_2,
sl_wfx_interface_t interface
)

Set maximum transmit power.

Parameters
max_tx_power_rf_port_1 returns the maximum transmit power in units of 0.1d_bm, on RF port 1.
max_tx_power_rf_port_2 returns the maximum transmit power in units of 0.1d_bm, on RF port 2.
interface is the interface used to send the request.
  • SL_WFX_STA_INTERFACE
  • SL_WFX_SOFTAP_INTERFACE
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 1091 of file sl_wfx.c .

References sl_wfx_get_max_tx_power_cnf_t::body , sl_wfx_get_max_tx_power_cnf_body_t::max_tx_power_rf_port1 , sl_wfx_get_max_tx_power_cnf_body_t::max_tx_power_rf_port2 , SL_WFX_GET_MAX_TX_POWER_REQ_ID , sl_wfx_get_status_code() , sl_wfx_send_command() , and sl_wfx_get_max_tx_power_cnf_body_t::status .

◆ sl_wfx_get_pmk()

sl_status_t sl_wfx_get_pmk ( sl_wfx_password_t * password,
uint32_t * password_length,
sl_wfx_interface_t interface
)

Get the PMK used to connect to the current secure network.

Parameters
password is the current Pairwise Master Key
password_length is its length in bytes
interface is the interface used to send the request.
  • SL_WFX_STA_INTERFACE
  • SL_WFX_SOFTAP_INTERFACE
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_WOULD_OVERFLOW if the password would overflow, SL_STATUS_FAIL otherwise

Definition at line 1123 of file sl_wfx.c .

References sl_wfx_get_pmk_cnf_t::body , sl_wfx_get_pmk_cnf_body_t::password , sl_wfx_get_pmk_cnf_body_t::password_length , SL_WFX_GET_PMK_REQ_ID , sl_wfx_get_status_code() , SL_WFX_PASSWORD_SIZE , sl_wfx_send_command() , and sl_wfx_get_pmk_cnf_body_t::status .

◆ sl_wfx_get_signal_strength()

sl_status_t sl_wfx_get_signal_strength ( uint32_t * signal_strength )

Get the signal strength of the last packets received.

Parameters
signal_strength returns the RCPI value averaged on the last packets received. RCPI ranges from 0 - 220 with 220 corresponds to 0 dBm and each increment represents an increase of 0.5 dBm.
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 711 of file sl_wfx.c .

References sl_wfx_get_signal_strength_cnf_t::body , sl_wfx_get_signal_strength_cnf_body_t::rcpi , SL_WFX_GET_SIGNAL_STRENGTH_REQ_ID , sl_wfx_get_status_code() , sl_wfx_send_command() , SL_WFX_STA_INTERFACE , and sl_wfx_get_signal_strength_cnf_body_t::status .

◆ sl_wfx_remove_multicast_address()

sl_status_t sl_wfx_remove_multicast_address ( const sl_wfx_mac_address_t * mac_address,
sl_wfx_interface_t interface
)

Remove a multicast address from the multicast filter whitelist.

Parameters
mac_address is the MAC address to remove
interface is the interface where to apply the change
  • SL_WFX_STA_INTERFACE
  • SL_WFX_SOFTAP_INTERFACE
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 801 of file sl_wfx.c .

References sl_wfx_remove_multicast_addr_req_body_t::mac , sl_wfx_mac_address_t::octet , SL_WFX_REMOVE_MULTICAST_ADDR_REQ_ID , and sl_wfx_send_command() .

◆ sl_wfx_send_disconnect_command()

sl_status_t sl_wfx_send_disconnect_command ( void )

Connected as a station, send a disconnection request to the AP.

Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 398 of file sl_wfx.c .

References SL_WFX_DISCONNECT_REQ_ID , sl_wfx_send_command() , and SL_WFX_STA_INTERFACE .

◆ sl_wfx_send_ethernet_frame()

sl_status_t sl_wfx_send_ethernet_frame ( sl_wfx_send_frame_req_t * frame,
uint32_t data_length,
sl_wfx_interface_t interface,
uint8_t priority
)

Send an Ethernet frame.

Parameters
frame contains the Ethernet frame to be sent
data_length is the length of the Ethernet frame
interface is the interface used to send the ethernet frame.
  • SL_WFX_STA_INTERFACE
  • SL_WFX_SOFTAP_INTERFACE
priority is the priority level used to send the Ethernet frame.
Returns
SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 567 of file sl_wfx.c .

References sl_wfx_send_frame_req_t::body , sl_wfx_context_t::data_frame_id , sl_wfx_send_frame_req_body_t::frame_type , sl_wfx_send_frame_req_t::header , sl_wfx_header_t::id , sl_wfx_header_t::info , sl_wfx_header_t::length , sl_wfx_send_frame_req_body_t::packet_data_length , sl_wfx_send_frame_req_body_t::packet_id , sl_wfx_send_frame_req_body_t::priority , SL_WFX_SEND_FRAME_REQ_ID , sl_wfx_send_request() , and WFM_FRAME_TYPE_DATA .

◆ sl_wfx_send_join_command()

sl_status_t sl_wfx_send_join_command ( const uint8_t * ssid,
uint32_t ssid_length,
const sl_wfx_mac_address_t * bssid,
uint16_t channel,
sl_wfx_security_mode_t security_mode,
uint8_t prevent_roaming,
uint16_t management_frame_protection,
const uint8_t * passkey,
uint16_t passkey_length,
const uint8_t * ie_data,
uint16_t ie_data_length
)

As a station, send a command to join a Wi-Fi network.

Parameters
ssid is the name of the AP to connect to
ssid_length is the length of the SSID name
bssid is the address of the AP to connect to (optional)
channel is the channel used by AP. Set at 0 if the channel is unknown
security_mode is the security used by the AP
  • WFM_SECURITY_MODE_OPEN
  • WFM_SECURITY_MODE_WEP
  • WFM_SECURITY_MODE_WPA2_WPA1_PSK
  • WFM_SECURITY_MODE_WPA2_PSK
  • WFM_SECURITY_MODE_WPA3_SAE
prevent_roaming is equal to 1 to prevent automatic roaming between APs
management_frame_protection is equal to 1 to enable PMF mode
passkey is the passkey used by the AP. Can be the WPA hash key to improve connection speed
passkey_length is the length of the passkey
ie_data are the Vendor-specific IEs to be added to the probe request
ie_data_length is the length of the IEs
Returns
Returns SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 328 of file sl_wfx.c .

References sl_wfx_allocate_command_buffer() , and SL_WFX_CONNECT_REQ_ID .

◆ sl_wfx_send_scan_command()

sl_status_t sl_wfx_send_scan_command ( uint16_t scan_mode,
const uint8_t * channel_list,
uint16_t channel_list_count,
const sl_wfx_ssid_def_t * ssid_list,
uint16_t ssid_list_count,
const uint8_t * ie_data,
uint16_t ie_data_length,
const uint8_t * bssid
)

Send a scan command.

Parameters
scan_mode is the mode used during the scan phase
  • WFM_SCAN_MODE_PASSIVE
  • WFM_SCAN_MODE_ACTIVE
channel_list is the list of channels to be scanned. Suitable values goes from 1 to 13.
channel_list_count is the number of channels to be scanned. If 0 the scan will be performed on every channel.
ssid_list is the list of SSID names to look for. The Wi-Fi chip will only send scan results for the specified SSIDs. If Null, every scan result will be passed on to the host.
ssid_list_count is the number of SSID specified (from 0 up to 2)
ie_data is the Vendor-specific IE data to be added to probe requests
ie_data_length is the length of the probe request IEs
bssid is optional and triggers a unicast scan if the scan mode used is WFM_SCAN_MODE_ACTIVE.
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 611 of file sl_wfx.c .

References sl_wfx_allocate_command_buffer() , and SL_WFX_START_SCAN_REQ_ID .

◆ sl_wfx_send_stop_scan_command()

sl_status_t sl_wfx_send_stop_scan_command ( void )

Stop an ongoing scan process.

Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 697 of file sl_wfx.c .

References sl_wfx_send_command() , SL_WFX_STA_INTERFACE , and SL_WFX_STOP_SCAN_REQ_ID .

◆ sl_wfx_set_arp_ip_address()

sl_status_t sl_wfx_set_arp_ip_address ( uint32_t * arp_ip_addr,
uint8_t num_arp_ip_addr
)

Set the ARP offloading state.

Parameters
arp_ip_addr is the pointer to ARP IP address list to offload
num_arp_ip_addr is the number of addresses in the list (0 - 2)
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 817 of file sl_wfx.c .

References sl_wfx_set_arp_ip_address_req_body_t::arp_ip_addr , sl_wfx_send_command() , SL_WFX_SET_ARP_IP_ADDRESS_REQ_ID , and SL_WFX_STA_INTERFACE .

◆ sl_wfx_set_broadcast_filter()

sl_status_t sl_wfx_set_broadcast_filter ( uint32_t filter )

Set the broadcast filter state.

Parameters
filter is equal to 1 to enable broadcast filtering.
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 858 of file sl_wfx.c .

References sl_wfx_set_broadcast_filter_req_body_t::filter , sl_wfx_send_command() , SL_WFX_SET_BROADCAST_FILTER_REQ_ID , and SL_WFX_STA_INTERFACE .

◆ sl_wfx_set_mac_address()

sl_status_t sl_wfx_set_mac_address ( const sl_wfx_mac_address_t * mac,
sl_wfx_interface_t interface
)

Brief Set the MAC address used by Wi-Fi chip.

Parameters
mac is the MAC address to be set on the specified the interface
interface is the interface to be configured. see sl_wfx_interface_t.
  • SL_WFX_STA_INTERFACE
  • SL_WFX_SOFTAP_INTERFACE
Returns
Returns SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 282 of file sl_wfx.c .

References sl_wfx_set_mac_address_req_body_t::mac_addr , sl_wfx_context_t::mac_addr_0 , sl_wfx_context_t::mac_addr_1 , sl_wfx_mac_address_t::octet , sl_wfx_send_command() , SL_WFX_SET_MAC_ADDRESS_REQ_ID , SL_WFX_SOFTAP_INTERFACE , and SL_WFX_STA_INTERFACE .

◆ sl_wfx_set_max_ap_client()

sl_status_t sl_wfx_set_max_ap_client ( uint32_t max_clients )

Configure the maximum number of clients supported in softap mode.

Parameters
max_clients is the maximum number of clients supported in softap. Broadcast address denies all MAC addresses.
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Note
sl_wfx_set_max_ap_client() has to be called after sl_wfx_start_ap_command() . If the softap is stopped or the Wi-Fi chip resets, the command has to be issued again.

Definition at line 925 of file sl_wfx.c .

References sl_wfx_set_max_ap_client_count_req_body_t::count , sl_wfx_send_command() , SL_WFX_SET_MAX_AP_CLIENT_COUNT_REQ_ID , and SL_WFX_SOFTAP_INTERFACE .

◆ sl_wfx_set_max_ap_client_inactivity()

sl_status_t sl_wfx_set_max_ap_client_inactivity ( uint32_t inactivity_timeout )

Configure the maximum client idle time.

Parameters
inactivity_timeout is the maximum client idle time in seconds.
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Note
sl_wfx_set_max_ap_client() has to be called after sl_wfx_start_ap_command() . If the softap is stopped or the Wi-Fi chip resets, the command has to be issued again.

Definition at line 944 of file sl_wfx.c .

References sl_wfx_set_max_ap_client_inactivity_req_body_t::inactivity_timeout , sl_wfx_send_command() , SL_WFX_SET_MAX_AP_CLIENT_INACTIVITY_REQ_ID , and SL_WFX_SOFTAP_INTERFACE .

◆ sl_wfx_set_max_tx_power()

sl_status_t sl_wfx_set_max_tx_power ( int32_t max_tx_power,
sl_wfx_interface_t interface
)

Set maximum transmit power.

Parameters
max_tx_power is the maximum transmit power in units of 0.1d_bm.
interface is the interface used to send the request.
  • SL_WFX_STA_INTERFACE
  • SL_WFX_SOFTAP_INTERFACE
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 1070 of file sl_wfx.c .

References sl_wfx_set_max_tx_power_req_body_t::max_tx_power , sl_wfx_send_command() , and SL_WFX_SET_MAX_TX_POWER_REQ_ID .

◆ sl_wfx_set_ns_ip_address()

sl_status_t sl_wfx_set_ns_ip_address ( uint8_t * ns_ip_addr,
uint8_t num_ns_ip_addr
)

Set the NS offloading state.

Parameters
ns_ip_addr is the pointer to NS IP address list to offload
num_ns_ip_addr is the number of addresses in the list (0 - 2)
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 838 of file sl_wfx.c .

References sl_wfx_set_ns_ip_address_req_body_t::ns_ip_addr , sl_wfx_send_command() , SL_WFX_SET_NS_IP_ADDRESS_REQ_ID , and SL_WFX_STA_INTERFACE .

◆ sl_wfx_set_power_mode()

sl_status_t sl_wfx_set_power_mode ( sl_wfx_pm_mode_t mode,
sl_wfx_pm_poll_t strategy,
uint16_t interval
)

Set the power mode used as a station.

The Wi-Fi chip will enable the Wi-Fi power mode feature.

Parameters
mode is the power mode to be used by the connection
  • WFM_PM_MODE_ACTIVE
  • WFM_PM_MODE_BEACON
  • WFM_PM_MODE_DTIM
interval is the number of beacons/DTIMs to skip while sleeping
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise
Note
the power mode has to be set once the connection with the AP is established

Definition at line 763 of file sl_wfx.c .

References sl_wfx_set_pm_mode_req_body_t::listen_interval , sl_wfx_set_pm_mode_req_body_t::polling_strategy , sl_wfx_set_pm_mode_req_body_t::power_mode , sl_wfx_send_command() , SL_WFX_SET_PM_MODE_REQ_ID , and SL_WFX_STA_INTERFACE .

◆ sl_wfx_set_roam_parameters()

sl_status_t sl_wfx_set_roam_parameters ( uint8_t rcpi_threshold,
uint8_t rcpi_hysteresis,
uint8_t beacon_lost_count,
const uint8_t * channel_list,
uint8_t channel_list_count
)

Configure the roaming behavior in station mode.

Parameters
rcpi_threshold is the lower RCPI limit trigerring a roaming attempt
rcpi_hysteresis is the High RCPI limit that must be attain before a roaming attempt can be triggered again
beacon_lost_count is the beacon loss limit for a roaming attempt
channel_list is the list of specific channels to scan
channel_list_count is the amount of specific channels to scan
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Note
Parameters set by sl_wfx_set_roam_parameters() take effect at the next connection. Calling it while connected has no immediate effect.

Definition at line 995 of file sl_wfx.c .

References sl_wfx_allocate_command_buffer() , and SL_WFX_SET_ROAM_PARAMETERS_REQ_ID .

◆ sl_wfx_set_scan_parameters()

sl_status_t sl_wfx_set_scan_parameters ( uint16_t active_channel_time,
uint16_t passive_channel_time,
uint16_t num_probe_requests
)

Configure scan parameters.

Parameters
active_channel_time is the time spent on each channel during active scan. Set to 0 for FW default, 1 - 550 TUs (1 TU = 1.024 ms).
passive_channel_time Time spent on each channel during passive scan. Set to 0 for FW default, 1 - 550 TUs (1 TU = 1.024 ms).
num_probe_requests is the number of probe requests to send. Set to 0 for FW default, 1 - 2
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Note
Parameters set with sl_wfx_set_scan_parameters() will apply for every future scan

Definition at line 967 of file sl_wfx.c .

References sl_wfx_set_scan_parameters_req_body_t::active_channel_time , sl_wfx_set_scan_parameters_req_body_t::num_of_probe_requests , sl_wfx_set_scan_parameters_req_body_t::passive_channel_time , sl_wfx_set_scan_parameters_req_body_t::reserved , sl_wfx_send_command() , SL_WFX_SET_SCAN_PARAMETERS_REQ_ID , and SL_WFX_STA_INTERFACE .

◆ sl_wfx_set_tx_rate_parameters()

sl_status_t sl_wfx_set_tx_rate_parameters ( sl_wfx_rate_set_bitmask_t rate_set_bitmask,
uint8_t use_minstrel
)

Set the rate mode allowed by the station once connected.

Parameters
rate_set_bitmask is the list of rates that will be used in STA mode.
use_minstrel is equal to 1 to use the Minstrel rate algorithm.
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Note
Parameters set by sl_wfx_set_tx_rate_parameters() take effect at the next connection. Calling it while connected has no immediate effect.

Definition at line 1050 of file sl_wfx.c .

References sl_wfx_set_tx_rate_parameters_req_body_t::rate_set_bitmask , sl_wfx_set_tx_rate_parameters_req_body_t::reserved , sl_wfx_send_command() , SL_WFX_SET_TX_RATE_PARAMETERS_REQ_ID , SL_WFX_STA_INTERFACE , and sl_wfx_set_tx_rate_parameters_req_body_t::use_minstrel .

◆ sl_wfx_set_unicast_filter()

sl_status_t sl_wfx_set_unicast_filter ( uint32_t filter )

Set the unicast filter state.

Parameters
filter is equal to 1 to enable unicast filtering.
Returns
SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise

Definition at line 873 of file sl_wfx.c .

References sl_wfx_set_unicast_filter_req_body_t::filter , sl_wfx_send_command() , SL_WFX_SET_UNICAST_FILTER_REQ_ID , and SL_WFX_SOFTAP_INTERFACE .

◆ sl_wfx_start_ap_command()

sl_status_t sl_wfx_start_ap_command ( uint16_t channel,
uint8_t * ssid,
uint32_t ssid_length,
uint8_t hidden_ssid,
uint8_t client_isolation,
sl_wfx_security_mode_t security_mode,
uint8_t management_frame_protection,
const uint8_t * passkey,
uint16_t passkey_length,
const uint8_t * beacon_ie_data,
uint16_t beacon_ie_data_length,
const uint8_t * probe_response_ie_data,
uint16_t probe_response_ie_data_length
)

Send a command to start the softap mode.

Parameters
channel is the channel used by AP. Between 1 and 14
ssid is the SSID name used by the softap
ssid_length is the SSID name length
hidden_ssid is equal to 1 to hide the network
client_isolation is equal to 1 isolate clients from each other
security_mode is the security level used by the softap
  • WFM_SECURITY_MODE_OPEN
  • WFM_SECURITY_MODE_WEP
  • WFM_SECURITY_MODE_WPA2_WPA1_PSK
  • WFM_SECURITY_MODE_WPA2_PSK
  • WFM_SECURITY_MODE_WPA3_SAE
management_frame_protection is equal to 1 to enable PMF mode
passkey is the passkey used by the softap. Only applicable in security modes different from WFM_SECURITY_MODE_OPEN.
passkey_length is the length of the passkey
beacon_ie_data is the Vendor-specific IE data to be added to beacons
beacon_ie_data_length is the length of the beacon IEs
probe_response_ie_data is the Vendor-specific IE data to be added to probe responses
probe_response_ie_data_length is the length of the probe response IEs
Returns
Returns SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 429 of file sl_wfx.c .

References sl_wfx_allocate_command_buffer() , and SL_WFX_START_AP_REQ_ID .

◆ sl_wfx_stop_ap_command()

sl_status_t sl_wfx_stop_ap_command ( void )

Send a command to stop the softap mode.

Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 550 of file sl_wfx.c .

References sl_wfx_send_command() , SL_WFX_SOFTAP_INTERFACE , and SL_WFX_STOP_AP_REQ_ID .

◆ sl_wfx_update_ap_command()

sl_status_t sl_wfx_update_ap_command ( uint16_t beacon_ie_data_length,
uint16_t probe_response_ie_data_length,
uint32_t * beacon_ie_data,
uint32_t * probe_response_ie_data
)

Update the softap settings.

Parameters
beacon_ie_data_length is the length of the beacon IEs
probe_response_ie_data_length is the length of the probe response IEs
beacon_ie_data is the Vendor-specific IE data to be added to beacons
probe_response_ie_data is the Vendor-specific IE data to be added to probe responses
Returns
SL_STATUS_OK if the command has been sent correctly, SL_STATUS_FAIL otherwise

Definition at line 502 of file sl_wfx.c .

References sl_wfx_allocate_command_buffer() , and SL_WFX_UPDATE_AP_REQ_ID .