GENERAL_DRIVER_API
Functions |
|
| sl_status_t | sl_wfx_secure_link_set_mac_key (const uint8_t *sl_mac_key, sl_wfx_securelink_mac_key_dest_t destination) |
|
SecureLink Set MAC Key.
|
|
| sl_status_t | sl_wfx_secure_link_exchange_keys (const uint8_t *sl_mac_key, uint8_t *sl_host_pub_key) |
|
Exchange SecureLink public keys.
|
|
| sl_status_t | sl_wfx_secure_link_renegotiate_session_key (void) |
|
Renegotiate session key request.
|
|
| sl_status_t | sl_wfx_secure_link_configure (const uint8_t *encryption_bitmap, uint8_t disable_session_key_protection) |
|
Modify SecureLink configuration.
|
|
| sl_status_t | sl_wfx_send_configuration (const char *pds_data, uint32_t pds_data_length) |
|
Function to send PDS chunks.
|
|
| sl_status_t | sl_wfx_control_gpio (uint8_t gpio_label, uint8_t gpio_mode, uint32_t *value) |
|
Send a request to read or write a GPIO.
|
|
| sl_status_t | sl_wfx_pta_settings (uint8_t pta_mode, uint8_t request_signal_active_level, uint8_t priority_signal_active_level, uint8_t freq_signal_active_level, uint8_t grant_signal_active_level, uint8_t coex_type, uint8_t default_grant_state, uint8_t simultaneous_rx_access, uint8_t priority_sampling_time, uint8_t tx_rx_sampling_time, uint8_t freq_sampling_time, uint8_t grant_valid_time, uint8_t fem_control_time, uint8_t first_slot_time, uint16_t periodic_tx_rx_sampling_time, uint16_t coex_quota, uint16_t wlan_quota) |
|
Send a request to set the PTA mode, the active levels on signals, the Coex type, to define the timings, quotas, combined mode and default grant state.
|
|
| sl_status_t | sl_wfx_pta_priority (uint32_t priority) |
|
Send a request to define the level of priority used to arbitrate concurrent Coex and Wlan requests.
|
|
| sl_status_t | sl_wfx_pta_state (uint32_t pta_state) |
|
Send a request to start or stop the PTA.
|
|
| sl_status_t | sl_wfx_set_cca_config (uint8_t cca_thr_mode) |
|
Send a request to configure the CCA mode.
|
|
| sl_status_t | sl_wfx_prevent_rollback (uint32_t magic_word) |
|
Prevent Rollback request.
|
|
| sl_status_t | sl_wfx_shutdown (void) |
|
Shutdown the Wi-Fi chip.
|
|
Function Documentation
◆ sl_wfx_control_gpio()
| sl_status_t sl_wfx_control_gpio | ( | uint8_t |
gpio_label,
|
| uint8_t |
gpio_mode,
|
||
| uint32_t * |
value
|
||
| ) |
Send a request to read or write a GPIO.
- Parameters
-
gpio_labelis the GPIO label to control (defined in the PDS) gpio_modedefines how to read or set the GPIO valuereturns the read value or the detailed error cause
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line
1302
of file
sl_wfx.c
.
References
sl_wfx_control_gpio_req_body_t::gpio_label
,
sl_wfx_control_gpio_req_body_t::gpio_mode
,
SL_WFX_CONTROL_GPIO_REQ_ID
,
sl_wfx_get_status_code()
,
sl_wfx_send_command()
, and
SL_WFX_STA_INTERFACE
.
◆ sl_wfx_prevent_rollback()
| sl_status_t sl_wfx_prevent_rollback | ( | uint32_t |
magic_word
|
) |
Prevent Rollback request.
- Parameters
-
magic_wordUsed to prevent mistakenly sent request from burning the OTP
- Returns
- SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Definition at line
1475
of file
sl_wfx.c
.
References
sl_wfx_prevent_rollback_req_body_t::magic_word
,
SL_WFX_PREVENT_ROLLBACK_REQ_ID
,
sl_wfx_send_command()
, and
SL_WFX_STA_INTERFACE
.
◆ sl_wfx_pta_priority()
| sl_status_t sl_wfx_pta_priority | ( | uint32_t |
priority
|
) |
Send a request to define the level of priority used to arbitrate concurrent Coex and Wlan requests.
- Parameters
-
prioritydefines the priority levels for concurrent Coex and WLAN request arbitration - SL_WFX_PTA_PRIORITY_COEX_MAXIMIZED
- SL_WFX_PTA_PRIORITY_COEX_HIGH
- SL_WFX_PTA_PRIORITY_BALANCED
- SL_WFX_PTA_PRIORITY_WLAN_HIGH
- SL_WFX_PTA_PRIORITY_WLAN_MAXIMIZED
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line
1412
of file
sl_wfx.c
.
References
sl_wfx_pta_priority_req_body_t::priority
,
SL_WFX_PTA_PRIORITY_REQ_ID
,
sl_wfx_send_command()
, and
SL_WFX_STA_INTERFACE
.
◆ sl_wfx_pta_settings()
| sl_status_t sl_wfx_pta_settings | ( | uint8_t |
pta_mode,
|
| uint8_t |
request_signal_active_level,
|
||
| uint8_t |
priority_signal_active_level,
|
||
| uint8_t |
freq_signal_active_level,
|
||
| uint8_t |
grant_signal_active_level,
|
||
| uint8_t |
coex_type,
|
||
| uint8_t |
default_grant_state,
|
||
| uint8_t |
simultaneous_rx_access,
|
||
| uint8_t |
priority_sampling_time,
|
||
| uint8_t |
tx_rx_sampling_time,
|
||
| uint8_t |
freq_sampling_time,
|
||
| uint8_t |
grant_valid_time,
|
||
| uint8_t |
fem_control_time,
|
||
| uint8_t |
first_slot_time,
|
||
| uint16_t |
periodic_tx_rx_sampling_time,
|
||
| uint16_t |
coex_quota,
|
||
| uint16_t |
wlan_quota
|
||
| ) |
Send a request to set the PTA mode, the active levels on signals, the Coex type, to define the timings, quotas, combined mode and default grant state.
- Parameters
-
pta_modedefines the mode to use - SL_WFX_PTA_1W_WLAN_MASTER
- SL_WFX_PTA_1W_COEX_MASTER
- SL_WFX_PTA_2W
- SL_WFX_PTA_3W
- SL_WFX_PTA_4W
request_signal_active_levelis the active level on REQUEST signal (PTA_RF_ACT pin) priority_signal_active_levelis the active level on PRIORITY signal (PTA_STATUS pin) freq_signal_active_levelis the active level on FREQ signal (PTA_FREQ pin) grant_signal_active_levelis the active level on GRANT signal (PTA_TX_CONF pin) - SL_WFX_SIGNAL_LOW
- SL_WFX_SIGNAL_HIGH
coex_type- SL_WFX_COEX_TYPE_GENERIC
- SL_WFX_COEX_TYPE_BLE
default_grant_stateis the state of the GRANT signal before arbitration at grant_valid_time - SL_WFX_NO_GRANT
- SL_WFX_GRANT
simultaneous_rx_accessis a boolean to allow both Coex and Wlan to receive concurrently, also named combined mode priority_sampling_timeis the time (in microseconds) from the Coex request to the sampling of the priority on PRIORITY signal (1 to 31) tx_rx_sampling_timeis the time (in microseconds) from the Coex request to the sampling of the directionality on PRIORITY signal (priority_sampling_time to 63) freq_sampling_timeis the time (in microseconds) from the Coex request to the sampling of freq-match information on FREQ signal (1 to 127) grant_valid_timeis the time (in microseconds) from Coex request to the GRANT signal assertion (MAX(tx_rx_sampling_time, freq_sampling_time) to 255) fem_control_timeis the time (in microseconds) from Coex request to the control of FEM (grant_valid_time to 255) first_slot_timeis the time (in microseconds) from the Coex request to the beginning of reception or transmission (grant_valid_time to 255) periodic_tx_rx_sampling_timeis the period (in microseconds) from first_slot_time of following samplings of the directionality on PRIORITY signal (1 to 1023) coex_quotais the duration (in microseconds) for which RF is granted to Coex before it is moved to Wlan wlan_quotais the duration (in microseconds) for which RF is granted to Wlan before it is moved to Coex
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line
1356
of file
sl_wfx.c
.
References
sl_wfx_pta_settings_req_body_t::coex_quota
,
sl_wfx_pta_settings_req_body_t::coex_type
,
sl_wfx_pta_settings_req_body_t::default_grant_state
,
sl_wfx_pta_settings_req_body_t::fem_control_time
,
sl_wfx_pta_settings_req_body_t::first_slot_time
,
sl_wfx_pta_settings_req_body_t::freq_sampling_time
,
sl_wfx_pta_settings_req_body_t::freq_signal_active_level
,
sl_wfx_pta_settings_req_body_t::grant_signal_active_level
,
sl_wfx_pta_settings_req_body_t::grant_valid_time
,
sl_wfx_pta_settings_req_body_t::periodic_tx_rx_sampling_time
,
sl_wfx_pta_settings_req_body_t::priority_sampling_time
,
sl_wfx_pta_settings_req_body_t::priority_signal_active_level
,
sl_wfx_pta_settings_req_body_t::pta_mode
,
sl_wfx_pta_settings_req_body_t::request_signal_active_level
,
sl_wfx_pta_settings_req_body_t::simultaneous_rx_access
,
SL_WFX_PTA_SETTINGS_REQ_ID
,
sl_wfx_send_command()
,
SL_WFX_STA_INTERFACE
,
sl_wfx_pta_settings_req_body_t::tx_rx_sampling_time
, and
sl_wfx_pta_settings_req_body_t::wlan_quota
.
◆ sl_wfx_pta_state()
| sl_status_t sl_wfx_pta_state | ( | uint32_t |
pta_state
|
) |
Send a request to start or stop the PTA.
- Parameters
-
pta_statedefines the requested state of the PTA - SL_WFX_PTA_OFF
- SL_WFX_PTA_ON
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line
1433
of file
sl_wfx.c
.
References
sl_wfx_pta_state_req_body_t::pta_state
,
SL_WFX_PTA_STATE_REQ_ID
,
sl_wfx_send_command()
, and
SL_WFX_STA_INTERFACE
.
◆ sl_wfx_secure_link_configure()
| sl_status_t sl_wfx_secure_link_configure | ( | const uint8_t * |
encryption_bitmap,
|
| uint8_t |
disable_session_key_protection
|
||
| ) |
Modify SecureLink configuration.
- Parameters
-
encryption_bitmapEncryption bitmap that must be written to wf200 disable_session_key_protectionForce the firmware to authorize the use of the same session key during a complete power cycle, even very long.
- Note
- Disabling the session key protection downgrades the link security and is NOT RECOMMENDED.
- The magic word SL_WFX_SESSION_KEY_PROTECTION_DISABLE_MAGIC is used to disable this protection.
- Returns
- Returns SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
- Note
- The bitmap used as a parameter will be copied to the context bitmap if the setting completed successfully.
Definition at line
247
of file
sl_wfx_secure_link.c
.
References
sl_wfx_securelink_configure_req_body_t::encr_bmp
.
◆ sl_wfx_secure_link_exchange_keys()
| sl_status_t sl_wfx_secure_link_exchange_keys | ( | const uint8_t * |
sl_mac_key,
|
| uint8_t * |
sl_host_pub_key
|
||
| ) |
Exchange SecureLink public keys.
- Parameters
-
sl_mac_keyMAC key to be used sl_host_pub_keypublic key of the host
- Returns
- Returns SL_STATUS_OK if the request has been sent correctly, SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED otherwise
Definition at line
139
of file
sl_wfx_secure_link.c
.
References
sl_wfx_allocate_command_buffer()
, and
SL_WFX_SECURELINK_EXCHANGE_PUB_KEYS_REQ_ID
.
◆ sl_wfx_secure_link_renegotiate_session_key()
| sl_status_t sl_wfx_secure_link_renegotiate_session_key | ( | void |
|
) |
Renegotiate session key request.
- Returns
- SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
Definition at line
183
of file
sl_wfx_secure_link.c
.
◆ sl_wfx_secure_link_set_mac_key()
| sl_status_t sl_wfx_secure_link_set_mac_key | ( | const uint8_t * |
sl_mac_key,
|
| sl_wfx_securelink_mac_key_dest_t |
destination
|
||
| ) |
SecureLink Set MAC Key.
- Parameters
-
sl_mac_keyMAC key to write on wf200 destinationMemory section where it should be written - SL_MAC_KEY_DEST_OTP
- SL_MAC_KEY_DEST_RAM
- Returns
- Returns SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line
113
of file
sl_wfx_secure_link.c
.
References
sl_wfx_set_securelink_mac_key_req_body_t::key_value
, and
sl_wfx_set_securelink_mac_key_req_body_t::otp_or_ram
.
◆ sl_wfx_send_configuration()
| sl_status_t sl_wfx_send_configuration | ( | const char * |
pds_data,
|
| uint32_t |
pds_data_length
|
||
| ) |
Function to send PDS chunks.
- Parameters
-
pds_dataData to be sent in the compressed PDS format pds_data_lengthSize of the data to be sent
- Returns
- SL_STATUS_OK if the configuration has been sent correctly, SL_STATUS_FAIL otherwise
- Note
- The PDS (Platform Data Set) file contains the WF200 settings
Definition at line
1255
of file
sl_wfx.c
.
References
sl_wfx_allocate_command_buffer()
, and
SL_WFX_CONFIGURATION_REQ_ID
.
Referenced by
sl_wfx_set_antenna_config()
.
◆ sl_wfx_set_cca_config()
| sl_status_t sl_wfx_set_cca_config | ( | uint8_t |
cca_thr_mode
|
) |
Send a request to configure the CCA mode.
- Parameters
-
cca_thr_modedefines the requested mode for CCA - SL_WFX_CCA_THR_MODE_RELATIVE
- SL_WFX_CCA_THR_MODE_ABSOLUTE
- Returns
- SL_STATUS_OK if the request has been sent correctly, SL_STATUS_FAIL otherwise
Definition at line
1454
of file
sl_wfx.c
.
References
sl_wfx_set_cca_config_req_body_t::cca_thr_mode
,
sl_wfx_set_cca_config_req_body_t::reserved
,
sl_wfx_send_command()
,
SL_WFX_SET_CCA_CONFIG_REQ_ID
, and
SL_WFX_STA_INTERFACE
.
◆ sl_wfx_shutdown()
| sl_status_t sl_wfx_shutdown | ( | void |
|
) |
Shutdown the Wi-Fi chip.
- Returns
- SL_STATUS_OK if the Wi-Fi chip has been shutdown correctly, SL_STATUS_FAIL otherwise
- Note
- Send the shutdown command, clear the WUP bit and the GPIO WUP to enable the Wi-Fi chips to go to sleep
Definition at line
1493
of file
sl_wfx.c
.
References
sl_wfx_allocate_command_buffer()
, and
SL_WFX_SHUT_DOWN_REQ_ID
.
Referenced by
sl_wfx_deinit()
.