Prevent_Firmware_Rollback
APIs for preventing Rollback of unsafe firmware images.
Data Structures |
|
| struct | sl_wfx_prevent_rollback_req_body_t |
|
Prevent Rollback request.
|
|
| struct | sl_wfx_prevent_rollback_cnf_body_t |
|
Confirmation of the
Prevent Rollback
request.
|
|
Detailed Description
APIs for preventing Rollback of unsafe firmware images.
By enabling this feature Device can prevent unsafe/outdated firmware from booting.
Each firmware owns its internal rollback revision number which is compared to an equivalent revision number burned in Device OTP memory. Depending on the comparison result, two use cases can occur:
- Firmware revision number is higher or equal to the OTP number -> the firmware is allowed to proceed
- Firmware revision number is lower than the OTP value -> the firmware is not allowed to proceed. An Error indication will be returned to the driver indicating the cause of the error (SL_WFX_ERROR_FIRMWARE_ROLLBACK).
- Note
- The firmware rollback revision number is different that the firmware version . The former is incremented only when some important fixes (i.e., Security patches) are provided by a given version of the firmware,that MUST be applied to Device and should not be reverted. Usually, subsequent firmware versions are supposed to embed the same rollback revision number.
The rollback capability relies on the use of a dedicated API sl_wfx_prevent_rollback_req_body_t .
All Device drivers supporting Rollback Prevention should send this request just after booting a new firmware. This way, any newer rollback revision number included in a firmware will be burned in the OTP.
Data Structure Documentation
◆ sl_wfx_prevent_rollback_req_body_t
| struct sl_wfx_prevent_rollback_req_body_t |
Prevent Rollback request.
Prevent Rollback asks WLAN firmware to burn a new Firmware Rollback value in a dedicated OTP section.
The new value is encoded in the firmware itself. After it is burned, this value will prevent from starting all firmwares whose internal rollback value is lower than the OTP value.
Magic Word is used to prevent mistakenly sent requests from burning the OTP.
Definition at line
746
of file
sl_wfx_general_api.h
.
| Data Fields | ||
|---|---|---|
| uint32_t | magic_word | Magic Word - should be 0x5C8912F3. |