MESSAGE_CONSTRUCTION
interface message formating
Data Structures |
|
| struct | sl_wfx_header_t |
|
General Message header structure.
|
|
| struct | sl_wfx_generic_message_t |
|
Generic message structure for all requests, confirmations and indications.
|
|
| struct | sl_wfx_generic_confirmation_t |
|
Generic confirmation message with the body reduced to the status field.
|
|
Detailed Description
interface message formating
The WLAN API handles 3 types of messages. REQUEST, CONFIRMATION and INDICATION
WLAN can send an INDICATION message to the host at any time.
Host can send REQUEST to the WLAN and the WLAN will always answer to it (either immediately or after a while) with a CONFIRMATION.
A message is composed of a header and a body (see sl_wfx_generic_msg_t). In the rest of the API description, only the body is detailed for each message.
Data Structure Documentation
◆ sl_wfx_header_t
| struct sl_wfx_header_t |
General Message header structure.
Definition at line
113
of file
sl_wfx_general_api.h
.
| Data Fields | ||
|---|---|---|
| uint8_t | id | Contains the message Id indexed by sl_wfx_general_commands_ids_t or sl_wfx_message_ids_t . |
| uint8_t | info | TODO comment missing. |
| uint16_t | length |
Message length in bytes including this uint16_t.
Maximum value is 8188 but maximum Request size is FW dependent and reported in the sl_wfx_startup_ind_body_t::size_inp_ch_buf . |
◆ sl_wfx_generic_message_t
| struct sl_wfx_generic_message_t |
Generic message structure for all requests, confirmations and indications.
Definition at line
124
of file
sl_wfx_general_api.h
.
| Data Fields | ||
|---|---|---|
| uint8_t | body[] | variable size payload of the message |
| sl_wfx_header_t | header | 4 bytes header |
◆ sl_wfx_generic_confirmation_t
| struct sl_wfx_generic_confirmation_t |
Generic confirmation message with the body reduced to the status field.
This structure is not related to a specific confirmation ID.
It is a global simplified structure that can be used to easily access the header and status fields.
All confirmation bodies start with a status word and in a lot of them it is followed by other data (not present in this structure).
Definition at line
137
of file
sl_wfx_general_api.h
.
| Data Fields | ||
|---|---|---|
| sl_wfx_header_t | header | 4 bytes header |
| uint32_t | status | See enum sl_wfx_status_t. |