DRIVER_API
| Modules | |
| GENERAL_DRIVER_API | |
| FULL_MAC_DRIVER_API | |
| Functions | |
| void | sl_wfx_init_secure_link_encryption_bitmap (uint8_t *bitmap) | 
| Initializes the whole SecureLink bitmap to disable encryption for all request IDs. | |
| uint8_t | sl_wfx_secure_link_encryption_required_get (uint8_t request_id) | 
| Get the encryption state of a request ID. | |
| void | sl_wfx_secure_link_bitmap_set_all_encrypted (uint8_t *bitmap) | 
| Quickly set the bitmap to encrypt all requests. | |
| void | sl_wfx_secure_link_bitmap_add_request_id (uint8_t *bitmap, uint8_t request_id) | 
| Add a request ID to the SecureLink bitmap. | |
| void | sl_wfx_secure_link_bitmap_remove_request_id (uint8_t *bitmap, uint8_t request_id) | 
| Remove a request ID to the SecureLink bitmap. | |
| sl_status_t | sl_wfx_init ( sl_wfx_context_t *context) | 
| Init the Wi-Fi chip. | |
| sl_status_t | sl_wfx_deinit (void) | 
| Deinit the Wi-Fi chip. | |
| sl_status_t | sl_wfx_send_command (uint8_t command_id, void *data, uint32_t data_size, sl_wfx_interface_t interface, sl_wfx_generic_confirmation_t **response) | 
| Send a command to WF200. | |
| sl_status_t | sl_wfx_send_request (uint8_t command_id, sl_wfx_generic_message_t *request, uint16_t request_length) | 
| Send a request to the Wi-Fi chip. | |
| sl_status_t | sl_wfx_receive_frame (uint16_t *ctrl_reg) | 
| Receive available frame from the Wi-Fi chip. | |
| sl_status_t | sl_wfx_enable_irq (void) | 
| Enable the Wi-Fi chip irq. | |
| sl_status_t | sl_wfx_disable_irq (void) | 
| Disable the Wi-Fi chip irq. | |
| sl_status_t | sl_wfx_set_access_mode_message (void) | 
| Set access mode message. | |
| sl_status_t | sl_wfx_set_wake_up_bit (uint8_t state) | 
| Set the Wi-Fi chip wake up bit. | |
| sl_status_t | sl_wfx_enable_device_power_save (void) | 
| Active the power save feature in the FMAC driver and let the WFx go in sleep mode. | |
| sl_status_t | sl_wfx_disable_device_power_save (void) | 
| Disable the power save feature in the FMAC driver and prevent the WFx going in sleep mode. | |
| static sl_status_t | sl_wfx_init_chip (void) | 
| Init the Wi-Fi chip. | |
| static sl_status_t | sl_wfx_download_run_bootloader (void) | 
| run the Wi-Fi chip bootloader | |
| static sl_status_t | sl_wfx_download_run_firmware (void) | 
| Download the Wi-Fi chip firmware. | |
| static sl_status_t | sl_wfx_poll_for_value (uint32_t address, uint32_t polled_value, uint32_t max_retries) | 
| Poll a value from the Wi-Fi chip. | |
| static sl_status_t | sl_wfx_compare_keysets (uint8_t chip_keyset, char *firmware_keyset) | 
| Compare the chip keyset and the firmware one to check compatibility. | |
| sl_status_t | sl_wfx_set_antenna_config ( sl_wfx_antenna_config_t config) | 
| Configure the antenna setting (done through the PDS) | |
| sl_status_t | sl_wfx_get_hardware_revision_and_type (uint8_t *revision, uint8_t *type) | 
| Retrieve the hardware version and type. | |
| sl_status_t | sl_wfx_get_opn (uint8_t **opn) | 
| Get the part opn. | |
| sl_status_t | sl_wfx_get_status_code (uint32_t wfx_status, uint8_t command_id) | 
| Extract status code from WFx message. | |
| sl_status_t | sl_wfx_allocate_command_buffer ( sl_wfx_generic_message_t **buffer, uint32_t command_id, sl_wfx_buffer_type_t type, uint32_t buffer_size) | 
| Allocate a buffer for the Wi-Fi driver. | |
| sl_status_t | sl_wfx_free_command_buffer ( sl_wfx_generic_message_t *buffer, uint32_t command_id, sl_wfx_buffer_type_t type) | 
| Free a buffer for the Wi-Fi driver. | |
Function Documentation
◆ sl_wfx_allocate_command_buffer()
| sl_status_t sl_wfx_allocate_command_buffer | ( | sl_wfx_generic_message_t ** | 
            buffer,
            | 
| uint32_t | 
            command_id,
            | ||
| sl_wfx_buffer_type_t | 
            type,
            | ||
| uint32_t | 
            buffer_size
            | ||
| ) | 
Allocate a buffer for the Wi-Fi driver.
- Parameters
- 
         buffercommand_idis the ID of the command to check if encryption is required typeof the buffer to allocate buffer_sizeis the size of the buffer to allocate 
- Returns
- SL_STATUS_OK if the values are retrieved correctly, SL_STATUS_TIMEOUT if the buffer is not allocated in time, SL_STATUS_FAIL otherwise
        Definition at line
        
         2430
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_host_allocate_buffer()
        
        , and
        
         sl_wfx_secure_link_encryption_required_get()
        
        .
       
        Referenced by
        
         sl_wfx_ext_auth()
        
        ,
        
         sl_wfx_secure_link_exchange_keys()
        
        ,
        
         sl_wfx_send_command()
        
        ,
        
         sl_wfx_send_configuration()
        
        ,
        
         sl_wfx_send_join_command()
        
        ,
        
         sl_wfx_send_scan_command()
        
        ,
        
         sl_wfx_set_roam_parameters()
        
        ,
        
         sl_wfx_shutdown()
        
        ,
        
         sl_wfx_start_ap_command()
        
        , and
        
         sl_wfx_update_ap_command()
        
        .
       
◆ sl_wfx_compare_keysets()
| 
 | static | 
Compare the chip keyset and the firmware one to check compatibility.
- Parameters
- 
         chip_keysetis the value retrieved from the Wi-Fi chip firmware_keysetis the 8 first bytes of the firmware 
- Returns
- SL_STATUS_OK if the firmware is compatible with the WF200, SL_STATUS_WIFI_INVALID_KEY otherwise
        Definition at line
        
         2233
        
        of file
        
         sl_wfx.c
        
        .
       
        Referenced by
        
         sl_wfx_download_run_firmware()
        
        .
       
◆ sl_wfx_deinit()
| sl_status_t sl_wfx_deinit | ( | void | 
            | ) | 
Deinit the Wi-Fi chip.
- Returns
- Returns SL_STATUS_OK if the deinitialization is successful, SL_STATUS_FAIL otherwise
        Definition at line
        
         250
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_disable_irq()
        
        , and
        
         sl_wfx_shutdown()
        
        .
       
◆ sl_wfx_disable_device_power_save()
| sl_status_t sl_wfx_disable_device_power_save | ( | void | 
            | ) | 
Disable the power save feature in the FMAC driver and prevent the WFx going in sleep mode.
- Returns
- SL_STATUS_OK if the bit has been set correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         1899
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_context_t::state
        
        .
       
◆ sl_wfx_disable_irq()
| sl_status_t sl_wfx_disable_irq | ( | void | 
            | ) | 
Disable the Wi-Fi chip irq.
- Returns
- SL_STATUS_OK if the irq is disabled correctly, SL_STATUS_FAIL otherwise
- Note
- Disable the host irq and set the Wi-Fi chip register accordingly
        Definition at line
        
         1788
        
        of file
        
         sl_wfx.c
        
        .
       
        Referenced by
        
         sl_wfx_deinit()
        
        .
       
◆ sl_wfx_download_run_bootloader()
| 
 | static | 
run the Wi-Fi chip bootloader
- Returns
- SL_STATUS_OK if the bootloader runs correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         1999
        
        of file
        
         sl_wfx.c
        
        .
       
        Referenced by
        
         sl_wfx_init()
        
        .
       
◆ sl_wfx_download_run_firmware()
| 
 | static | 
Download the Wi-Fi chip firmware.
- Returns
- SL_STATUS_OK if the firmware is downloaded correctly, SL_STATUS_WIFI_INVALID_KEY if the firmware keyset does not match the chip one, SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUT or SL_STATUS_TIMEOUT if the process times out, SL_STATUS_FAIL otherwise
        Definition at line
        
         2038
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_compare_keysets()
        
        ,
        
         sl_wfx_host_get_firmware_data()
        
        ,
        
         sl_wfx_host_get_firmware_size()
        
        ,
        
         sl_wfx_host_init()
        
        ,
        
         sl_wfx_host_log()
        
        , and
        
         sl_wfx_poll_for_value()
        
        .
       
        Referenced by
        
         sl_wfx_init()
        
        .
       
◆ sl_wfx_enable_device_power_save()
| sl_status_t sl_wfx_enable_device_power_save | ( | void | 
            | ) | 
Active the power save feature in the FMAC driver and let the WFx go in sleep mode.
- Returns
- SL_STATUS_OK if the bit has been set correctly, SL_STATUS_FAIL otherwise
- Note
- In connected state, it is required to activate the Wi-Fi power mode using sl_wfx_set_power_mode() to allow the WFx chip to go to sleep.
        Definition at line
        
         1865
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_context_t::state
        
        .
       
◆ sl_wfx_enable_irq()
| sl_status_t sl_wfx_enable_irq | ( | void | 
            | ) | 
Enable the Wi-Fi chip irq.
- Returns
- SL_STATUS_OK if the irq is enabled correctly, SL_STATUS_FAIL otherwise
- Note
- Enable the host irq and set the Wi-Fi chip register accordingly
        Definition at line
        
         1761
        
        of file
        
         sl_wfx.c
        
        .
       
References sl_wfx_host_enable_platform_interrupt() .
        Referenced by
        
         sl_wfx_init()
        
        .
       
◆ sl_wfx_free_command_buffer()
| sl_status_t sl_wfx_free_command_buffer | ( | sl_wfx_generic_message_t * | 
            buffer,
            | 
| uint32_t | 
            command_id,
            | ||
| sl_wfx_buffer_type_t | 
            type
            | ||
| ) | 
Free a buffer for the Wi-Fi driver.
- Parameters
- 
         buffercommand_idis the ID of the command to check if encryption is required typeof the buffer to allocate 
- Returns
- SL_STATUS_OK if the values are retrieved correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         2479
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_host_free_buffer()
        
        , and
        
         sl_wfx_secure_link_encryption_required_get()
        
        .
       
◆ sl_wfx_get_hardware_revision_and_type()
| sl_status_t sl_wfx_get_hardware_revision_and_type | ( | uint8_t * | 
            revision,
            | 
| uint8_t * | 
            type
            | ||
| ) | 
Retrieve the hardware version and type.
- Parameters
- 
         revisionis the pointer to retrieve the revision version typeis the pointer to retrieve the type 
- Returns
- SL_STATUS_OK if the values are retrieved correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         2292
        
        of file
        
         sl_wfx.c
        
        .
       
◆ sl_wfx_get_opn()
| sl_status_t sl_wfx_get_opn | ( | uint8_t ** | 
            opn
            | ) | 
Get the part opn.
- Parameters
- 
         opn
- Returns
- SL_STATUS_OK if the values are retrieved correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         2313
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_context_t::wfx_opn
        
        .
       
◆ sl_wfx_get_status_code()
| sl_status_t sl_wfx_get_status_code | ( | uint32_t | 
            wfx_status,
            | 
| uint8_t | 
            command_id
            | ||
| ) | 
Extract status code from WFx message.
- Parameters
- 
         wfx_statusis the status returned by the WFx command_idis the ID of the command 
- Returns
- corresponding driver status code enumerated in sl_status_t
        Definition at line
        
         2332
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         SL_WFX_ERROR_UNSUPPORTED_MSG_ID
        
        ,
        
         sl_wfx_host_log()
        
        ,
        
         SL_WFX_INVALID_PARAMETER
        
        ,
        
         SL_WFX_MAC_KEY_STATUS_FAILED_KEY_ALREADY_BURNED
        
        ,
        
         SL_WFX_MAC_KEY_STATUS_FAILED_RAM_MODE_NOT_ALLOWED
        
        ,
        
         SL_WFX_MAC_KEY_STATUS_FAILED_UNKNOWN_MODE
        
        ,
        
         SL_WFX_MAC_KEY_STATUS_SUCCESS
        
        ,
        
         SL_WFX_PREVENT_ROLLBACK_CNF_SUCCESS
        
        ,
        
         SL_WFX_PREVENT_ROLLBACK_CNF_WRONG_MAGIC_WORD
        
        ,
        
         SL_WFX_PUB_KEY_EXCHANGE_STATUS_FAILED
        
        ,
        
         SL_WFX_PUB_KEY_EXCHANGE_STATUS_SUCCESS
        
        ,
        
         SL_WFX_STATUS_FAILURE
        
        ,
        
         SL_WFX_STATUS_GPIO_WARNING
        
        ,
        
         SL_WFX_STATUS_SUCCESS
        
        ,
        
         WFM_STATUS_CHANNEL_NOT_ALLOWED
        
        ,
        
         WFM_STATUS_CONNECTION_ABORTED
        
        ,
        
         WFM_STATUS_CONNECTION_AUTH_FAILURE
        
        ,
        
         WFM_STATUS_CONNECTION_REJECTED_BY_AP
        
        ,
        
         WFM_STATUS_CONNECTION_TIMEOUT
        
        ,
        
         WFM_STATUS_GENERAL_FAILURE
        
        ,
        
         WFM_STATUS_INVALID_PARAMETER
        
        ,
        
         WFM_STATUS_NO_MATCHING_AP
        
        ,
        
         WFM_STATUS_RETRY_EXCEEDED
        
        ,
        
         WFM_STATUS_SUCCESS
        
        ,
        
         WFM_STATUS_TX_LIFETIME_EXCEEDED
        
        ,
        
         WFM_STATUS_WARNING
        
        , and
        
         WFM_STATUS_WRONG_STATE
        
        .
       
        Referenced by
        
         sl_wfx_control_gpio()
        
        ,
        
         sl_wfx_get_ap_client_signal_strength()
        
        ,
        
         sl_wfx_get_max_tx_power()
        
        ,
        
         sl_wfx_get_pmk()
        
        , and
        
         sl_wfx_get_signal_strength()
        
        .
       
◆ sl_wfx_init()
| sl_status_t sl_wfx_init | ( | sl_wfx_context_t * | 
            context
            | ) | 
Init the Wi-Fi chip.
- Parameters
- 
         contextmaintain the Wi-Fi chip information 
- Returns
- Returns SL_STATUS_OK if the initialization is successful, SL_STATUS_FAIL otherwise
- Note
- Actions performed by sl_wfx_init() : Reset -> load firmware -> send PDS
        Definition at line
        
         83
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_context_t::firmware_build
        
        ,
        
         sl_wfx_context_t::firmware_major
        
        ,
        
         sl_wfx_context_t::firmware_minor
        
        ,
        
         sl_wfx_context_t::mac_addr_0
        
        ,
        
         sl_wfx_context_t::mac_addr_1
        
        ,
        
         sl_wfx_mac_address_t::octet
        
        ,
        
         sl_wfx_download_run_bootloader()
        
        ,
        
         sl_wfx_download_run_firmware()
        
        ,
        
         sl_wfx_enable_irq()
        
        ,
        
         sl_wfx_host_log()
        
        ,
        
         sl_wfx_host_setup_waited_event()
        
        ,
        
         sl_wfx_host_wait_for_confirmation()
        
        ,
        
         sl_wfx_init_chip()
        
        ,
        
         sl_wfx_set_access_mode_message()
        
        ,
        
         SL_WFX_STARTUP_IND_ID
        
        ,
        
         sl_wfx_context_t::used_buffers
        
        , and
        
         sl_wfx_context_t::wfx_opn
        
        .
       
◆ sl_wfx_init_chip()
| 
 | static | 
Init the Wi-Fi chip.
- Returns
- SL_STATUS_OK if the initialization is successful, SL_STATUS_FAIL otherwise
        Definition at line
        
         1937
        
        of file
        
         sl_wfx.c
        
        .
       
        Referenced by
        
         sl_wfx_init()
        
        .
       
◆ sl_wfx_init_secure_link_encryption_bitmap()
| void sl_wfx_init_secure_link_encryption_bitmap | ( | uint8_t * | 
            bitmap
            | ) | 
Initializes the whole SecureLink bitmap to disable encryption for all request IDs.
Copyright 2018, Silicon Laboratories Inc.
- Parameters
- 
         bitmapis the bitmap that must be updated 
- Note
- It is advised to apply these changes to a transitory bitmap. Its data will be copied to the sl_wfx_context bitmap once the sl_wfx_send_secure_link_encryption_bitmap() has completed successfully.
        Definition at line
        
         73
        
        of file
        
         sl_wfx_secure_link.c
        
        .
       
◆ sl_wfx_poll_for_value()
| 
 | static | 
Poll a value from the Wi-Fi chip.
- Parameters
- 
         addressis the address of the value to be polled polled_valuewaiting for the value to be equal to polled_value max_retriesis the number of polling to be done before returning SL_STATUS_TIMEOUT 
- Returns
- SL_STATUS_OK if the value is received correctly, SL_STATUS_TIMEOUT if the value is not found in time, SL_STATUS_FAIL if not able to poll the value from the Wi-Fi chip
        Definition at line
        
         2203
        
        of file
        
         sl_wfx.c
        
        .
       
References sl_wfx_host_wait() .
        Referenced by
        
         sl_wfx_download_run_firmware()
        
        .
       
◆ sl_wfx_receive_frame()
| sl_status_t sl_wfx_receive_frame | ( | uint16_t * | 
            ctrl_reg
            | ) | 
Receive available frame from the Wi-Fi chip.
- Parameters
- 
         ctrl_regis the control register value of the last call of sl_wfx_receive_frame() . If equal to 0, the driver will read the control register. 
- Returns
- SL_STATUS_OK if the frame has been received correctly, SL_STATUS_WIFI_NO_PACKET_TO_RECEIVE if no frame are pending inside the Wi-Fi chip SL_STATUS_FAIL otherwise
        Definition at line
        
         1659
        
        of file
        
         sl_wfx.c
        
        .
       
◆ sl_wfx_secure_link_bitmap_add_request_id()
| void sl_wfx_secure_link_bitmap_add_request_id | ( | uint8_t * | 
            bitmap,
            | 
| uint8_t | 
            request_id
            | ||
| ) | 
Add a request ID to the SecureLink bitmap.
- Parameters
- 
         bitmapis the bitmap that must be updated request_idis id to add to the bitmap 
- Note
- It is advised to apply these changes to a transitory bitmap. Its data will be copied to the sl_wfx_context bitmap once the sl_wfx_send_secure_link_encryption_bitmap() has completed successfully.
        Definition at line
        
         443
        
        of file
        
         sl_wfx_secure_link.c
        
        .
       
◆ sl_wfx_secure_link_bitmap_remove_request_id()
| void sl_wfx_secure_link_bitmap_remove_request_id | ( | uint8_t * | 
            bitmap,
            | 
| uint8_t | 
            request_id
            | ||
| ) | 
Remove a request ID to the SecureLink bitmap.
- Parameters
- 
         bitmapis the bitmap that must be updated request_idis id to remove from the bitmap 
- Note
- It is advised to apply these changes to a transitory bitmap. Its data will be copied to the sl_wfx_context bitmap once the sl_wfx_send_secure_link_encryption_bitmap() has completed successfully.
        Definition at line
        
         458
        
        of file
        
         sl_wfx_secure_link.c
        
        .
       
◆ sl_wfx_secure_link_bitmap_set_all_encrypted()
| void sl_wfx_secure_link_bitmap_set_all_encrypted | ( | uint8_t * | 
            bitmap
            | ) | 
Quickly set the bitmap to encrypt all requests.
- Parameters
- 
         bitmapis the bitmap that must be updated 
- Note
- WFX firmware automatically adjusts for commands that should never or always be encrypted
        Definition at line
        
         428
        
        of file
        
         sl_wfx_secure_link.c
        
        .
       
◆ sl_wfx_secure_link_encryption_required_get()
| uint8_t sl_wfx_secure_link_encryption_required_get | ( | uint8_t | 
            request_id
            | ) | 
Get the encryption state of a request ID.
- Parameters
- 
         request_idto check in the bitmap 
- Returns
- Returns SL_WFX_SECURE_LINK_ENCRYPTION_REQUIRED if the request should be encrypted, SL_WFX_SECURE_LINK_ENCRYPTION_NOT_REQUIRED otherwise
        Definition at line
        
         85
        
        of file
        
         sl_wfx_secure_link.c
        
        .
       
        Referenced by
        
         sl_wfx_allocate_command_buffer()
        
        , and
        
         sl_wfx_free_command_buffer()
        
        .
       
◆ sl_wfx_send_command()
| sl_status_t sl_wfx_send_command | ( | uint8_t | 
            command_id,
            | 
| void * | 
            data,
            | ||
| uint32_t | 
            data_size,
            | ||
| sl_wfx_interface_t | 
            interface,
            | ||
| sl_wfx_generic_confirmation_t ** | 
            response
            | ||
| ) | 
Send a command to WF200.
- Parameters
- 
         command_idis the ID of the command to be sent (cf. sl_wfx_cmd_api.h)datais the pointer to the data to be sent by the command data_sizeis the size of the data to be sent interfaceis the interface affected by the command responseis a pointer to the response retrieved - SL_WFX_STA_INTERFACE
- SL_WFX_SOFTAP_INTERFACE
 
- Returns
- SL_STATUS_OK if the command is sent correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         1541
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_allocate_command_buffer()
        
        .
       
        Referenced by
        
         sl_wfx_add_blacklist_address()
        
        ,
        
         sl_wfx_add_multicast_address()
        
        ,
        
         sl_wfx_add_whitelist_address()
        
        ,
        
         sl_wfx_control_gpio()
        
        ,
        
         sl_wfx_disconnect_ap_client_command()
        
        ,
        
         sl_wfx_get_ap_client_signal_strength()
        
        ,
        
         sl_wfx_get_max_tx_power()
        
        ,
        
         sl_wfx_get_pmk()
        
        ,
        
         sl_wfx_get_signal_strength()
        
        ,
        
         sl_wfx_prevent_rollback()
        
        ,
        
         sl_wfx_pta_priority()
        
        ,
        
         sl_wfx_pta_settings()
        
        ,
        
         sl_wfx_pta_state()
        
        ,
        
         sl_wfx_remove_multicast_address()
        
        ,
        
         sl_wfx_send_disconnect_command()
        
        ,
        
         sl_wfx_send_stop_scan_command()
        
        ,
        
         sl_wfx_set_arp_ip_address()
        
        ,
        
         sl_wfx_set_broadcast_filter()
        
        ,
        
         sl_wfx_set_cca_config()
        
        ,
        
         sl_wfx_set_mac_address()
        
        ,
        
         sl_wfx_set_max_ap_client()
        
        ,
        
         sl_wfx_set_max_ap_client_inactivity()
        
        ,
        
         sl_wfx_set_max_tx_power()
        
        ,
        
         sl_wfx_set_ns_ip_address()
        
        ,
        
         sl_wfx_set_power_mode()
        
        ,
        
         sl_wfx_set_scan_parameters()
        
        ,
        
         sl_wfx_set_tx_rate_parameters()
        
        ,
        
         sl_wfx_set_unicast_filter()
        
        , and
        
         sl_wfx_stop_ap_command()
        
        .
       
◆ sl_wfx_send_request()
| sl_status_t sl_wfx_send_request | ( | uint8_t | 
            command_id,
            | 
| sl_wfx_generic_message_t * | 
            request,
            | ||
| uint16_t | 
            request_length
            | ||
| ) | 
Send a request to the Wi-Fi chip.
- Parameters
- 
         command_idis the ID of the command to be sent (cf. sl_wfx_cmd_api.h)requestis the pointer to the request to be sent request_lengthis the size of the request to be sent 
- Returns
- SL_STATUS_OK if the command is sent correctly, SL_STATUS_WOULD_OVERFLOW if the HIF queue is full, SL_STATUS_FAIL otherwise
        Definition at line
        
         1595
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         sl_wfx_generic_message_t::header
        
        ,
        
         sl_wfx_header_t::id
        
        ,
        
         sl_wfx_header_t::length
        
        ,
        
         sl_wfx_host_lock()
        
        ,
        
         sl_wfx_host_log()
        
        , and
        
         sl_wfx_context_t::used_buffers
        
        .
       
        Referenced by
        
         sl_wfx_send_ethernet_frame()
        
        .
       
◆ sl_wfx_set_access_mode_message()
| sl_status_t sl_wfx_set_access_mode_message | ( | void | 
            | ) | 
Set access mode message.
- Returns
- SL_STATUS_OK if the message mode is enabled correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         1814
        
        of file
        
         sl_wfx.c
        
        .
       
        Referenced by
        
         sl_wfx_init()
        
        .
       
◆ sl_wfx_set_antenna_config()
| sl_status_t sl_wfx_set_antenna_config | ( | sl_wfx_antenna_config_t | 
            config
            | ) | 
Configure the antenna setting (done through the PDS)
- Parameters
- 
         configis the antenna configuration to be used. - SL_WFX_ANTENNA_1_ONLY
- SL_WFX_ANTENNA_2_ONLY
- SL_WFX_ANTENNA_TX1_RX2
- SL_WFX_ANTENNA_TX2_RX1
- SL_WFX_ANTENNA_DIVERSITY
 
- Returns
- SL_STATUS_OK if the setting is applied correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         2263
        
        of file
        
         sl_wfx.c
        
        .
       
        References
        
         SL_WFX_ANTENNA_DIVERSITY
        
        , and
        
         sl_wfx_send_configuration()
        
        .
       
◆ sl_wfx_set_wake_up_bit()
| sl_status_t sl_wfx_set_wake_up_bit | ( | uint8_t | 
            state
            | ) | 
Set the Wi-Fi chip wake up bit.
- Parameters
- 
         stateis the state of the wake up bit to configure 
- Returns
- SL_STATUS_OK if the bit has been set correctly, SL_STATUS_FAIL otherwise
        Definition at line
        
         1836
        
        of file
        
         sl_wfx.c
        
        .