ENUM
| Enumerations | |
| enum | sl_wfx_register_address_t | 
| Enum listing the registers of the WFx solution. | |
| enum | sl_wfx_state_t | 
| Enum listing the different state of the WFx chip. | |
| enum | sl_wfx_interface_t
         
         { SL_WFX_STA_INTERFACE = 0x00 , SL_WFX_SOFTAP_INTERFACE = 0x01 } | 
| Enum listing available interfaces in WFx Wi-Fi solution. | |
| enum | sl_wfx_antenna_config_t
         
         { SL_WFX_ANTENNA_1_ONLY = 0 , SL_WFX_ANTENNA_2_ONLY , SL_WFX_ANTENNA_TX1_RX2 , SL_WFX_ANTENNA_TX2_RX1 , SL_WFX_ANTENNA_DIVERSITY } | 
| Enum listing the different antenna configurations. | |
| enum | sl_wfx_received_message_type_t
         
         { SL_WFX_CONFIRMATION_MESSAGE = 0 , SL_WFX_INDICATION_MESSAGE = 1 , SL_WFX_MANAGEMENT_MESSAGE = 2 , SL_WFX_ETHERNET_DATA_MESSAGE = 3 } | 
| Enum listing different message types received from WFx. | |
| enum | sl_wfx_buffer_type_t | 
| Enumerates the different types of buffer. | |
| enum | sl_wfx_host_bus_transfer_type_t | 
| Enumerates the different types of bus transfers. | |
| enum | sl_wfx_secure_link_mode_t | 
| Enum listing the different secure link mode of a part. | |
| enum | sl_wfx_securelink_renegotiation_state_t | 
| Enumerates the states of the secure link key renegotiation. | |
Enumeration Type Documentation
◆ sl_wfx_antenna_config_t
Enum listing the different antenna configurations.
        Definition at line
        
         289
        
        of file
        
         sl_wfx_constants.h
        
        .
       
◆ sl_wfx_interface_t
| enum sl_wfx_interface_t | 
Enum listing available interfaces in WFx Wi-Fi solution.
For convenience, interface 0 is associated with the station interface and interface 1 is associated with the softap interface.
| Enumerator | |
|---|---|
| SL_WFX_STA_INTERFACE | Interface 0, linked to the station. | 
| SL_WFX_SOFTAP_INTERFACE | Interface 1, linked to the softap. | 
        Definition at line
        
         280
        
        of file
        
         sl_wfx_constants.h
        
        .
       
◆ sl_wfx_received_message_type_t
Enum listing different message types received from WFx.
The information is found in the control register using SL_WFX_CONT_FRAME_TYPE_INFO mask.
        Definition at line
        
         303
        
        of file
        
         sl_wfx_constants.h
        
        .