ERROR_IDS
| Enumerations | |
| enum | sl_wfx_error_t
         
         { SL_WFX_ERROR_FIRMWARE_ROLLBACK = 0x0 , SL_WFX_ERROR_DEPRECATED_0 = 0x1 , SL_WFX_ERROR_DEPRECATED_1 = 0x2 , SL_WFX_ERROR_INVALID_SESSION_KEY = 0x3 , SL_WFX_ERROR_OOR_VOLTAGE = 0x4 , SL_WFX_ERROR_PDS_VERSION = 0x5 , SL_WFX_ERROR_OOR_TEMPERATURE = 0x6 , SL_WFX_ERROR_REQ_DURING_KEY_EXCHANGE = 0x7 , SL_WFX_ERROR_DEPRECATED_2 = 0x8 , SL_WFX_ERROR_DEPRECATED_3 = 0x9 , SL_WFX_ERROR_SECURELINK_DECRYPTION = 0xa , SL_WFX_ERROR_SECURELINK_WRONG_ENCRYPTION_STATE = 0xb , SL_WFX_SPI_OR_SDIO_FREQ_TOO_LOW = 0xc , SL_WFX_ERROR_DEPRECATED_4 = 0xd , SL_WFX_ERROR_DEPRECATED_5 = 0xe , SL_WFX_HIF_BUS_ERROR = 0xf , SL_WFX_PDS_TESTFEATURE_MODE_ERROR = 0x10 , SL_WFX_ERROR_SECURELINK_EXPECTED_BITMAP = 0x11 } | 
| specifies the type of error reported by the indication message
         
          sl_wfx_error_ind_body_t | |
Enumeration Type Documentation
◆ sl_wfx_error_t
| enum sl_wfx_error_t | 
specifies the type of error reported by the indication message sl_wfx_error_ind_body_t
        Definition at line
        
         36
        
        of file
        
         sl_wfx_general_error_api.h
        
        .