sl_wfx_nonce_t Struct Reference
Structure to maintain secure link counters.
| Data Fields | |
| uint32_t | hp_packet_count | 
| High priority packet counter. | |
| uint32_t | rx_packet_count | 
| Received packet counter. | |
| uint32_t | tx_packet_count | 
| Sent packet counter. | |
Structure to maintain secure link counters.
       Definition at line
       
        379
       
       of file
       
        sl_wfx_constants.h
       
       .
      
Field Documentation
◆ hp_packet_count
| uint32_t sl_wfx_nonce_t::hp_packet_count | 
High priority packet counter.
        Definition at line
        
         380
        
        of file
        
         sl_wfx_constants.h
        
        .
       
◆ rx_packet_count
| uint32_t sl_wfx_nonce_t::rx_packet_count | 
Received packet counter.
        Definition at line
        
         381
        
        of file
        
         sl_wfx_constants.h
        
        .
       
◆ tx_packet_count
| uint32_t sl_wfx_nonce_t::tx_packet_count | 
Sent packet counter.
        Definition at line
        
         382
        
        of file
        
         sl_wfx_constants.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       sl_wfx_constants.h