sl_wfx_mac_address_t Struct Reference
Structure to handle MAC address format.
| Data Fields | |
| uint8_t | octet [6] | 
| Table to store a MAC address. | |
Structure to handle MAC address format.
       Definition at line
       
        363
       
       of file
       
        sl_wfx_constants.h
       
       .
      
Field Documentation
◆ octet
| uint8_t sl_wfx_mac_address_t::octet[6] | 
Table to store a MAC address.
        Definition at line
        
         364
        
        of file
        
         sl_wfx_constants.h
        
        .
       
        Referenced by
        
         sl_wfx_add_blacklist_address()
        
        ,
        
         sl_wfx_add_multicast_address()
        
        ,
        
         sl_wfx_add_whitelist_address()
        
        ,
        
         sl_wfx_disconnect_ap_client_command()
        
        ,
        
         sl_wfx_get_ap_client_signal_strength()
        
        ,
        
         sl_wfx_init()
        
        ,
        
         sl_wfx_remove_multicast_address()
        
        , and
        
         sl_wfx_set_mac_address()
        
        .
       
The documentation for this struct was generated from the following file:
- 
       sl_wfx_constants.h