Structure representing the BLE event for CBFC connection request.

This structure is used to define the parameters for a BLE event that involves a Circular Buffer Flow Control (CBFC) connection request from a remote device.

Public Attributes#

uint8_t

Address of the remote device.

uint16_t

Protocol/Service Multiplexer (PSM) value.

uint16_t

Local Channel Identifier (LCID)

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_cbfc_conn_req_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the remote device.


Definition at line 1203 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

psm#

uint16_t rsi_ble_event_cbfc_conn_req_s::psm

Protocol/Service Multiplexer (PSM) value.


Definition at line 1205 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

lcid#

uint16_t rsi_ble_event_cbfc_conn_req_s::lcid

Local Channel Identifier (LCID)


Definition at line 1207 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h