Structure representing the BLE read request.
This structure is used to define the parameters for a BLE read request, including the remote device address, attribute handle, request type, and offset.
Public Attributes#
uint8_t
Remote device address.
uint16_t
Attribute handle.
uint8_t
Request type: 0 - Read request, 1 - Read Blob request.
uint8_t
Reserved for future use.
uint16_t
Offset of attribute value to be read.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_read_req_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address.
Definition at line
1096
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
handle#
uint16_t rsi_ble_read_req_s::handle
Attribute handle.
Definition at line
1098
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
type#
uint8_t rsi_ble_read_req_s::type
Request type: 0 - Read request, 1 - Read Blob request.
Definition at line
1100
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
reserved#
uint8_t rsi_ble_read_req_s::reserved
Reserved for future use.
Definition at line
1102
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
offset#
uint16_t rsi_ble_read_req_s::offset
Offset of attribute value to be read.
Definition at line
1104
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h