Structure representing the connection status event in the BLE module.
Public Attributes#
uint8_t
Address type of the connected device.
uint8_t
Address of the connected device.
uint16_t
Status of the connection - success/failure.
Public Attribute Documentation#
dev_addr_type#
uint8_t rsi_ble_event_conn_status_s::dev_addr_type
Address type of the connected device.
Definition at line
97
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
dev_addr#
uint8_t rsi_ble_event_conn_status_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the connected device.
Definition at line
99
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
status#
uint16_t rsi_ble_event_conn_status_s::status
Status of the connection - success/failure.
Definition at line
101
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h