Structure representing the Bluetooth Low Energy (BLE) event for security keys.

Public Attributes#

uint8_t

BD Address of the remote device.

uint8_t

16 byte irk of the local device

uint8_t

16 byte irk of the remote device

uint16_t

remote device ediv value

uint8_t

remote device rand value

uint8_t

remote device ltk value

uint8_t

Identity address type - public/random

  • 0x00 --> Public Identity Address

  • 0x01 --> Random (static) Identity Address

  • All other values Reserved for future use.

uint8_t

Identity address which is resolved after security keys exchange.

uint8_t

Device address type.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_bt_event_le_security_keys_s::dev_addr[RSI_DEV_ADDR_LEN]

BD Address of the remote device.


Definition at line 176 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

local_irk#

uint8_t rsi_bt_event_le_security_keys_s::local_irk[16]

16 byte irk of the local device


Definition at line 178 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_irk#

uint8_t rsi_bt_event_le_security_keys_s::remote_irk[16]

16 byte irk of the remote device


Definition at line 180 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_ediv#

uint16_t rsi_bt_event_le_security_keys_s::remote_ediv

remote device ediv value


Definition at line 182 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_rand#

uint8_t rsi_bt_event_le_security_keys_s::remote_rand[16]

remote device rand value


Definition at line 184 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_ltk#

uint8_t rsi_bt_event_le_security_keys_s::remote_ltk[16]

remote device ltk value


Definition at line 186 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

Identity_addr_type#

uint8_t rsi_bt_event_le_security_keys_s::Identity_addr_type

Identity address type - public/random

  • 0x00 --> Public Identity Address

  • 0x01 --> Random (static) Identity Address

  • All other values Reserved for future use.


Definition at line 194 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

Identity_addr#

uint8_t rsi_bt_event_le_security_keys_s::Identity_addr[6]

Identity address which is resolved after security keys exchange.


Definition at line 196 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

dev_addr_type#

uint8_t rsi_bt_event_le_security_keys_s::dev_addr_type

Device address type.


Definition at line 198 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h