Structure to hold the MTU exchange information for a BLE event.
Public Attributes#
uint8_t
uint8_t[6], remote device address
uint16_t
uint8_t[2], Remote MTU Size
uint16_t
uint8_t[2], Local MTU Size
uint8_t
uint8_t Initiated role, who initiated MTU exchange
PEER_DEVICE_INITATED_MTU_EXCHANGE 0x01
LOCAL_DEVICE_INITATED_MTU_EXCHANGE 0x02
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_mtu_exchange_information_s::dev_addr[RSI_DEV_ADDR_LEN]
uint8_t[6], remote device address
Definition at line
1128
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
remote_mtu_size#
uint16_t rsi_ble_event_mtu_exchange_information_s::remote_mtu_size
uint8_t[2], Remote MTU Size
Definition at line
1130
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
local_mtu_size#
uint16_t rsi_ble_event_mtu_exchange_information_s::local_mtu_size
uint8_t[2], Local MTU Size
Definition at line
1132
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
initiated_role#
uint8_t rsi_ble_event_mtu_exchange_information_s::initiated_role
uint8_t Initiated role, who initiated MTU exchange
PEER_DEVICE_INITATED_MTU_EXCHANGE 0x01
LOCAL_DEVICE_INITATED_MTU_EXCHANGE 0x02
Definition at line
1138
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h