Structure representing the enhanced connection status event in the module.

Public Attribute Documentation#

dev_addr_type#

uint8_t rsi_ble_event_enhnace_conn_status_s::dev_addr_type

Device address type of the Connected Remote Device


dev_addr#

uint8_t rsi_ble_event_enhnace_conn_status_s::dev_addr[RSI_DEV_ADDR_LEN]

Device address of the remote device.


local_resolvlable_addr#

uint8_t rsi_ble_event_enhnace_conn_status_s::local_resolvlable_addr[RSI_DEV_ADDR_LEN]

Local Device resolvable address


peer_resolvlable_addr#

uint8_t rsi_ble_event_enhnace_conn_status_s::peer_resolvlable_addr[RSI_DEV_ADDR_LEN]

Remote Device resolvable address


role#

uint8_t rsi_ble_event_enhnace_conn_status_s::role

The role of the device - central/ peripheral


conn_interval#

uint16_t rsi_ble_event_enhnace_conn_status_s::conn_interval

Connection interval used on this connection. Range: 0x0006 to 0x0C80


conn_latency#

uint16_t rsi_ble_event_enhnace_conn_status_s::conn_latency

Peripheral latency for the connection in number of connection events. Range: 0x0000 to 0x01F3


supervision_timeout#

uint16_t rsi_ble_event_enhnace_conn_status_s::supervision_timeout

Connection supervision timeout. Range: 0x000A to 0x0C80


master_clock_accuracy#

uint8_t rsi_ble_event_enhnace_conn_status_s::master_clock_accuracy

Only applicable for peripheral, for central this value is set to 0x00


status#

uint16_t rsi_ble_event_enhnace_conn_status_s::status

Status of the Connection - success/failure