Structure representing the BLE read request.

This structure is used to define the parameters for a BLE read request, including the remote device address, attribute handle, request type, and offset.

Public Attributes#

uint8_t
uint16_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_read_req_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


handle#

uint16_t rsi_ble_read_req_s::handle

Attribute handle


type#

uint8_t rsi_ble_read_req_s::type

Request type: 0 - Read request, 1 - Read Blob request


reserved#

uint8_t rsi_ble_read_req_s::reserved

Reserved for future use


offset#

uint16_t rsi_ble_read_req_s::offset

Offset of attribute value to be read