ae periodic sync establishment report event
Public Attribute Documentation#
status#
uint8_t rsi_ble_per_adv_sync_estbl_s::status
uint8_t status , It indicates whether Periodic Advertising is successful or not 0 - Periodic advertising sync successful !0 - Periodic advertising sync failed
sync_handle#
uint16_t rsi_ble_per_adv_sync_estbl_s::sync_handle
uint16_t Sync_Handle, It identifies the periodic Advertising train. Range : 0x0000 to 0x0EFF
adv_sid#
uint8_t rsi_ble_per_adv_sync_estbl_s::adv_sid
uint8_t Advertising_SID, Value of the Advertising SID subfield in the ADI field of the PDU, Range : 0x00 to 0x0F
advertiser_addr_type#
uint8_t rsi_ble_per_adv_sync_estbl_s::advertiser_addr_type
uint8_t Advertiser_Address_Type : Indicates the type of the Address 0x00 - Public Device Address 0x01 - Random Device Address 0x02 - Public Identity Address (corresponds to Resolved Private Address) 0x03 - Random (static) Identity Address (corresponds to Resolved Private Address)
advertiser_addr#
uint8_t rsi_ble_per_adv_sync_estbl_s::advertiser_addr[DEVICE_ADDR_LEN]
uint8[6], Advertiser_Address of the Advertiser type
advertiser_phy#
uint8_t rsi_ble_per_adv_sync_estbl_s::advertiser_phy
uint8_t Advertiser_PHY. This parameter specifies the PHY used for the periodic advertising. 0x01 - Advertiser PHY is LE 1M 0x02 - Advertiser PHY is LE 2M 0x03 - Advertiser PHY is LE Coded
per_adv_interval#
uint16_t rsi_ble_per_adv_sync_estbl_s::per_adv_interval
uint16_t Periodic_Advertising_Interval. This parameter specifies the interval between the periodic advertising events.
advertiser_clock_accuracy#
uint16_t rsi_ble_per_adv_sync_estbl_s::advertiser_clock_accuracy
uint16_t Advertiser_Clock_Accuracy. This parameter specifies the accuracy of the periodic advertiser's clock. 0x00 - 500 ppm 0x01 - 250 ppm 0x02 - 150 ppm 0x03 - 100 ppm 0x04 - 75 ppm 0x05 - 50 ppm 0x06 - 30 ppm 0x07 - 20 ppm