Structure to hold the MTU exchange information event.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_mtu_exchange_information_s::dev_addr[RSI_DEV_ADDR_LEN]
uint8_t[6], remote device address
remote_mtu_size#
uint16_t rsi_ble_event_mtu_exchange_information_s::remote_mtu_size
uint8_t[2], Remote MTU Size
local_mtu_size#
uint16_t rsi_ble_event_mtu_exchange_information_s::local_mtu_size
uint8_t[2], Local MTU Size
initiated_role#
uint8_t rsi_ble_event_mtu_exchange_information_s::initiated_role
uint8_t Initiated role, who initiated MTU exchange
PEER_DEVICE_INITATED_MTU_EXCHANGE 0x01
LOCAL_DEVICE_INITATED_MTU_EXCHANGE 0x02