You are viewing documentation for version:
Structure represents the GATT prepare write event.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_prepare_write_s::dev_addr[RSI_DEV_ADDR_LEN]
remote device address
handle#
uint8_t rsi_ble_event_prepare_write_s::handle[2]
attribute handle
offset#
uint8_t rsi_ble_event_prepare_write_s::offset[2]
attribute value offset
length#
uint16_t rsi_ble_event_prepare_write_s::length
length of attribute value
att_value#
uint8_t rsi_ble_event_prepare_write_s::att_value[RSI_DEV_ATT_LEN]
This contains the attribute value. The maximum value is 240, refer to RSI_DEV_ATT_LEN Macro