Structure to hold the event data for encryption enabled event.
Public Attribute Documentation#
enabled#
uint8_t rsi_bt_event_encryption_enabled_s::enabled
Status of the Encryption
ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC
BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC
BIT(2) --> To indicate or set UnAuthenticated Pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC
BIT(3) --> To indicate or set Authenticated Pairing and Encryption with LE SC
sc_enable#
uint8_t rsi_bt_event_encryption_enabled_s::sc_enable
BLE Secure Connections Enable/Disable indication
0 --> Disable
1 --> Enable