You are viewing documentation for version:
The structure represents security keys event.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_bt_event_le_security_keys_s::dev_addr[RSI_DEV_ADDR_LEN]
BD Address of the remote device
local_irk#
uint8_t rsi_bt_event_le_security_keys_s::local_irk[16]
16 byte irk of the local device
remote_irk#
uint8_t rsi_bt_event_le_security_keys_s::remote_irk[16]
16 byte irk of the remote device
remote_ediv#
uint16_t rsi_bt_event_le_security_keys_s::remote_ediv
remote device ediv value
remote_rand#
uint8_t rsi_bt_event_le_security_keys_s::remote_rand[16]
remote device rand value
remote_ltk#
uint8_t rsi_bt_event_le_security_keys_s::remote_ltk[16]
remote device ltk value
Identity_addr_type#
uint8_t rsi_bt_event_le_security_keys_s::Identity_addr_type
Identity address type - public/random
0x00 --> Public Identity Address
0x01 --> Random (static) Identity Address
All other values Reserved for future use
Identity_addr#
uint8_t rsi_bt_event_le_security_keys_s::Identity_addr[6]
Identity address which is resolved after security keys exchange
dev_addr_type#
uint8_t rsi_bt_event_le_security_keys_s::dev_addr_type
Device address type