ae scan request recvd report event

Public Attributes#

uint8_t

Public Attribute Documentation#

adv_handle#

uint8_t rsi_ble_scan_req_recvd_s::adv_handle

uint8_t Advertising_Handle : Used to identify an Advertising set , Range : 0x00 to 0xEF


scanner_addr_type#

uint8_t rsi_ble_scan_req_recvd_s::scanner_addr_type

uint8_t Scanner_Address_Type : Indicates the type of the Address 0x00 - Public Device Address 0x01 - Random Device Address 0x02 - Public Identity Address (corresponds to Resolved Private Address) 0x03 - Random (static) Identity Address (corresponds to Resolved Private Address)


scanner_addr#

uint8_t rsi_ble_scan_req_recvd_s::scanner_addr[DEVICE_ADDR_LEN]

uint8[6] Scanner_Address : Address of the Advertising Type