Prerequisites#

Hardware Requirements#

  • PTA Main

  • PTA Secondary

    • BLE device supporting Tx and Rx operation

    • Micro USB Cable (For SiWG917 device power)

  • Windows PC

  • Linux PC for running Server

  • Access Point

    • Used only in case of throughput runs on Wi-Fi side (PTA-Main)

  • Saleae Logic Analyzer

    • Used to monitor the Grant, Request, and Priority signals

  • Female-to-female connectors

  • Splitters or Y-connectors

    • Connection between Saleae analyzer & PTA Slave

    • These splitters are connected to the PTA Main to analyze the Grant, Request, and Priority Signals

Software Requirements#

Note: Refer to Update the SiWx91x Connectivity Firmware to load the firmware into the SiWx917 device. The firmware binary is found in the <Release_Package >/connectivity_firmware folder.