Setup Diagram#
In this setup, the SiWG917 operates as the PTA Main (Wi-Fi), with a BLE device connected to it. The SiWG917 throughput application has been executed on a Windows PC to measure Wi-Fi throughput values under various configurations SiWG917 (Config 1, Config 2, and Config 3, Hardware Configurations). To facilitate remote server/client operations, another PC running the iperf application is utilized.