Use Case Scenario#
The current implementation of PTA are suitable for the following scenarios:
Low Wi-Fi usage and low Wi-Fi throughput: In this use case, occasional Wi-Fi disconnects can be tolerated. However, test results do not show any Wi-Fi disconnection unless the REQUEST/PRIORITY frequency increases significantly. All three configurations can be used for this scenario.
Moderate traffic on the BLE Device (BT Classic/BLE) with specific transmit throughput requirements on the Wi-Fi side: Configuration 3 is recommended for this use case.
Moderate traffic on both the BLE device and Wi-Fi.