Predefined FFN parameter sets#

Predefined FFN parameter sets for sl_wisun_set_connection_parameters().

These parameter sets can be used either as-is or used as an initialization value for an application-specific parameter set.

Variables#

Profile for certification testing.

Profile for development (shorter connection time)

Variable Documentation#

SL_WISUN_PARAMS_PROFILE_CERTIF#

const sl_wisun_connection_params_t SL_WISUN_PARAMS_PROFILE_CERTIF

Profile for certification testing.


Definition at line 317 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

SL_WISUN_PARAMS_PROFILE_LARGE#

const sl_wisun_connection_params_t SL_WISUN_PARAMS_PROFILE_LARGE

Profile for a large network.


Definition at line 563 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

SL_WISUN_PARAMS_PROFILE_MEDIUM#

const sl_wisun_connection_params_t SL_WISUN_PARAMS_PROFILE_MEDIUM

Profile for a medium network.


Definition at line 481 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

SL_WISUN_PARAMS_PROFILE_SMALL#

const sl_wisun_connection_params_t SL_WISUN_PARAMS_PROFILE_SMALL

Profile for a small network.


Definition at line 399 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

SL_WISUN_PARAMS_PROFILE_TEST#

const sl_wisun_connection_params_t SL_WISUN_PARAMS_PROFILE_TEST

Profile for development (shorter connection time)


Definition at line 235 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h